[ 116.762765] Power button triggered [ 117.018358] Power button triggered [ 117.553425] PM: suspend entry (deep) [ 117.557050] PM: Syncing filesystems ... done. [ 117.613440] Freezing user space processes ... (elapsed 0.002 seconds) done. [ 117.623784] OOM killer disabled. [ 117.627134] Freezing remaining freezable tasks ... (elapsed 0.001 seconds) done. [ 117.636598] PM: PRCM_CM_WKUP_CLKDIV32K_CLKCTRL = 0x00000100 [ 117.642329] PM: Initiating RTC-Only Mode [ 117.646293] PM: Calling Early Suspend Resume address = 0x8010e62c [ 117.657932] PM: Early Suspend Success [ 117.661751] Suspending console(s) (use no_console_suspend to debug) [ 117.668161] Suspend test start done [ 117.682228] suspending [ 117.686779] tps65218_reg_read Interrupt Mask = 0x37 [ 117.700826] Suspend test finsih done [ 117.714456] Disabling non-boot CPUs ... [ 117.714506] PM: Successfully put all powerdomains to target state [ 117.714506] PM: Wakeup source Tamper RTC [ 117.729882] ==========Resume started ========== error = 0 wakeup = 0x0 state = 3 [ 117.729931] Start Resume [ 117.732715] remoteproc remoteproc0: stopped remote processor wkup_m3 [ 117.732770] remoteproc remoteproc0: powering up wkup_m3 [ 117.732942] remoteproc remoteproc0: Booting fw image am335x-pm-firmware.elf, size 225132 [ 117.734115] remoteproc remoteproc0: remote processor wkup_m3 is now up [ 117.871041] Power button triggered [ 117.875457] tps65218_reg_read Interrupt Mask = 0x37 [ 117.875482] tps65218_regulator_resume Interrupt Mask = 0x37 [ 117.880911] Cannot request GPIO Disp reset [ 117.891203] spidev spi2.3: not using DMA for McSPI (-19) [ 117.897056] spi setup status = 0x0 [ 117.901042] SSD2828: SPI communication failed. [ 117.905653] resuming [ 117.912236] usb usb1: root hub lost power or was reset [ 117.917455] usb usb2: root hub lost power or was reset [ 118.190829] OOM killer enabled. [ 118.194068] Restarting tasks ... done. [ 118.338089] PM: suspend exit [ 118.362021] spidev spi1.0: not using DMA for McSPI (-19) [ 118.414905] spidev spi1.0: not using DMA for McSPI (-19) [ 118.420370] spidev spi1.0: not using DMA for McSPI (-19) [ 118.691562] spidev spi2.3: not using DMA for McSPI (-19) [ 118.719568] spidev spi2.3: not using DMA for McSPI (-19) [ 131.001521] g_multi gadget: high-speed config #2: Multifunction with CDC ECM [ 131.237749] NOHZ: local_softirq_pending 08