U-Boot SPL 2021.01-g8e7635763e-dirty (Jan 06 2022 - 09:34:29 +0800) EEPROM not available at 80, trying to read at 81 Reading on-board EEPROM at 0x51 failed 1 SYSFW ABI: 3.1 (firmware rev 0x0015 '21.5.0--v2021.05 (Terrific Llam') SPL initial stack usage: 13392 bytes Trying to boot from SPI Starting ATF on ARM64 core... NOTICE: BL31: v2.5(release):08.00.00.004-dirty NOTICE: BL31: Built : 14:39:59, Aug 9 2021 U-Boot SPL 2021.01-g8e7635763e-dirty (Jan 06 2022 - 09:35:04 +0800) EEPROM not available at 80, trying to read at 81 Reading on-board EEPROM at 0x51 failed 1 SYSFW ABI: 3.1 (firmware rev 0x0015 '21.5.0--v2021.05 (Terrific Llam') Trying to boot from SPI U-Boot 2021.01-g8e7635763e-dirty (Jan 06 2022 - 09:35:04 +0800) SoC: AM64X SR1.0 P3Y KP Board EEPROM not available at 80, trying to read at 81 Reading on-board EEPROM at 0x51 failed 1 DRAM: 512 MiB Loading Environment from SPIFlash... cadence_spi spi@fc40000: Can't get reset: -2 jedec_spi_nor flash@0: Software reset enable failed: -524 SF: Detected is25lp032 with page size 256 Bytes, erase size 64 KiB, total 4 MiB *** Warning - bad CRC, using default environment In: serial@2800000 Out: serial@2800000 Err: serial@2800000 EEPROM not available at 80, trying to read at 81 Reading on-board EEPROM at 0x51 failed 1 Net: am65_cpsw_nuss_slave ethernet@8000000: K3 CPSW: nuss_ver: 0x6BA00903 cpsw_ver: 0x6BA80903 ale_ver: 0x00294104 Ports:2 mdio_freq:1000000 eth0: ethernet@8000000 Hit any key to stop autoboot: 0 =>