U-Boot SPL 2023.04-g71b8c840ca (Nov 27 2023 - 08:55:35 +0000) SYSFW ABI: 3.1 (firmware rev 0x0009 '9.1.2--v09.01.02 (Kool Koala)') Trying to boot from MMC2 Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Loading Environment from nowhere... OK Starting ATF on ARM64 core... NOTICE: BL31: v2.9(release):v2.9.0-614-gd7a7135d32-dirty NOTICE: BL31: Built : 09:34:15, Aug 24 2023 I/TC: I/TC: OP-TEE version: 4.0.0 (gcc version 11.4.0 (GCC)) #1 Fri Oct 20 18:29:31 UTC 2023 aarch64 I/TC: WARNING: This OP-TEE configuration might be insecure! I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html I/TC: Primary CPU initializing I/TC: SYSFW ABI: 3.1 (firmware rev 0x0009 '9.1.2--v09.01.02 (Kool Koala)') I/TC: HUK Initialized I/TC: Activated SA2UL device I/TC: Fixing SA2UL firewall owner for GP device I/TC: Enabled firewalls for SA2UL TRNG device I/TC: SA2UL TRNG initialized I/TC: SA2UL Drivers initialized I/TC: Primary CPU switching to normal world boot U-Boot SPL 2023.04-g71b8c840ca (Nov 27 2023 - 08:55:35 +0000) SYSFW ABI: 3.1 (firmware rev 0x0009 '9.1.2--v09.01.02 (Kool Koala)') Detected: J7X-BASE-CPB rev E3 Detected: J7X-VSC8514-ETH rev E2 Trying to boot from MMC2 Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted U-Boot 2023.04-g71b8c840ca (Nov 27 2023 - 08:55:35 +0000) SoC: J721E SR1.0 GP Model: Texas Instruments K3 J721E SoC Board: J721EX-PM2-SOM rev E7 DRAM: 4 GiB Core: 126 devices, 35 uclasses, devicetree: separate Flash: 0 Bytes MMC: mmc@4f80000: 0, mmc@4fb0000: 1 Loading Environment from nowhere... OK In: serial@2800000 Out: serial@2800000 Err: serial@2800000 am65_cpsw_nuss ethernet@46000000: K3 CPSW: nuss_ver: 0x6BA00101 cpsw_ver: 0x6BA80100 ale_ver: 0x00293904 Ports:1 mdio_freq:1000000 Detected: J7X-BASE-CPB rev E3 Detected: J7X-VSC8514-ETH rev E2 cdns,sierra serdes@5000000: sierra probed Net: eth0: ethernet@46000000port@1 Hit any key to stop autoboot: 0 switch to partitions #0, OK mmc1 is current device SD/MMC found on device 1 Failed to load 'boot.scr' 723 bytes read in 25 ms (27.3 KiB/s) Loaded env from uEnv.txt Importing environment from mmc1 ... Running uenvcmd ... 1 bytes read in 25 ms (0 Bytes/s) Already setup. gpio: pin gpio@22_17 (gpio 281) value is 1 gpio: pin gpio@22_16 (gpio 280) value is 0 k3_r5f_rproc r5f@41000000: Core 1 is already in use. No rproc commands work Failed to load '/lib/firmware/j7-mcu-r5f0_1-fw' 1310368 bytes read in 53 ms (23.6 MiB/s) Load Remote Processor 2 with data@addr=0x82000000 1310368 bytes: Success! 326836 bytes read in 33 ms (9.4 MiB/s) Load Remote Processor 3 with data@addr=0x82000000 326836 bytes: Success! Failed to load '/lib/firmware/j7-main-r5f1_0-fw' Failed to load '/lib/firmware/j7-main-r5f1_1-fw' 994096 bytes read in 47 ms (20.2 MiB/s) Load Remote Processor 6 with data@addr=0x82000000 994096 bytes: Success! 994096 bytes read in 47 ms (20.2 MiB/s) Load Remote Processor 7 with data@addr=0x82000000 994096 bytes: Success! 13365392 bytes read in 133 ms (95.8 MiB/s) Load Remote Processor 8 with data@addr=0x82000000 13365392 bytes: Success! 20367872 bytes read in 446 ms (43.6 MiB/s) 114792 bytes read in 29 ms (3.8 MiB/s) Working FDT set to 88000000 3589 bytes read in 26 ms (134.8 KiB/s) 11541 bytes read in 27 ms (417 KiB/s) ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Working FDT set to 88000000 ERROR: reserving fdt memory region failed (addr=880000000 size=27000000 flags=4) Loading Device Tree to 000000008fee0000, end 000000008fffffff ... OK Working FDT set to 8fee0000 Starting kernel ...