X.Org X Server 1.18.4 Release Date: 2016-07-19 X Protocol Version 11, Revision 0 Build Operating System: Linux 3.13.0-24-generic x86_64 Current Operating System: Linux omron-nsv3 4.9.41-ge3a80a1c5c #2 PREEMPT Sat Mar 9 18:40:29 JST 2019 armv7l Kernel command line: console=ttyO0,115200n8 root=PARTUUID=5713d26b-02 rw rootfstype=ext4 rootwait Build Date: 17 June 2017 08:20:30PM Current version of pixman: 0.32.8 Before reporting problems, check http://wiki.x.org to make sure that you have the latest version. Markers: (--) probed, (**) from config file, (==) default setting, (++) from command line, (!!) notice, (II) informational, (WW) warning, (EE) error, (NI) not implemented, (??) unknown. (==) Log file: "/usr/local/XSGX/var/log/Xorg.0.log", Time: Thu Mar 14 03:02:06 2019 (++) Using config file: "/usr/local/XSGX/etc/xorg.conf" (==) Using system config directory "/usr/local/XSGX/share/X11/xorg.conf.d" (**) Option "defaultserverlayout" "Server Layout" (**) ServerLayout "Server Layout" (**) |-->Screen "Screen" (0) (**) | |-->Monitor "Monitor" (**) | |-->Device "Video Device" (==) Automatically adding devices (==) Automatically enabling devices (==) Automatically adding GPU devices (==) Max clients allowed: 256, resource mask: 0x1fffff (WW) The directory "/usr/local/XSGX/share/fonts/X11/TTF/" does not exist. Entry deleted from font path. (WW) The directory "/usr/local/XSGX/share/fonts/X11/OTF/" does not exist. Entry deleted from font path. (==) FontPath set to: /usr/local/XSGX/share/fonts/X11/misc/, /usr/local/XSGX/share/fonts/X11/Type1/, /usr/local/XSGX/share/fonts/X11/100dpi/, /usr/local/XSGX/share/fonts/X11/75dpi/ (==) ModulePath set to "/usr/local/XSGX/lib/xorg/modules" (II) The server relies on udev to provide the list of input devices. If no devices become available, reconfigure udev or disable AutoAddDevices. (II) Loader magic: 0x15c8a8 (II) Module ABI versions: X.Org ANSI C Emulation: 0.4 X.Org Video Driver: 20.0 X.Org XInput driver : 22.1 X.Org Server Extension : 9.0 (II) xfree86: Adding drm device (/dev/dri/card0) (II) no primary bus or device found falling back to /sys/devices/platform/ocp/4830e000.lcdc/drm/card0 (WW) "glx" will not be loaded unless you've specified it to be loaded elsewhere. (WW) "pvr" will not be loaded unless you've specified it to be loaded elsewhere. (WW) "modesetting" will not be loaded unless you've specified it to be loaded elsewhere. (II) "glx" will be loaded even though the default is to disable it. (==) Matched modesetting as autoconfigured driver 0 (==) Matched fbdev as autoconfigured driver 1 (==) Assigned the driver to the xf86ConfigLayout (II) LoadModule: "modesetting" (II) Loading /usr/local/XSGX/lib/xorg/modules/drivers/modesetting_drv.so (II) Module modesetting: vendor="X.Org Foundation" compiled for 1.18.4, module version = 1.18.4 Module class: X.Org Video Driver ABI class: X.Org Video Driver, version 20.0 (II) LoadModule: "fbdev" (WW) Warning, couldn't open module fbdev (II) UnloadModule: "fbdev" (II) Unloading fbdev (EE) Failed to load module "fbdev" (module does not exist, 0) (II) modesetting: Driver for Modesetting Kernel Drivers: kms (--) using VT number 2 (II) modeset(0): using drv /dev/dri/card0 (WW) VGA arbiter: cannot open kernel arbiter, no multi-card support (II) modeset(0): Creating default Display subsection in Screen section "Screen" for depth/fbbpp 24/32 (==) modeset(0): Depth 24, (==) framebuffer bpp 32 (==) modeset(0): RGB weight 888 (==) modeset(0): Default visual is TrueColor (II) modeset(0): No glamor support in the X Server (II) modeset(0): ShadowFB: preferred NO, enabled NO (II) modeset(0): Output LVDS-1 using monitor section Monitor (II) modeset(0): Up to 1 crtcs needed for screen. (II) modeset(0): Allocated crtc nr. 0 to this screen. (II) modeset(0): EDID for output LVDS-1 (II) modeset(0): Printing probed modes for output LVDS-1 (II) modeset(0): Modeline "800x600"x60.5 40.00 800 840 904 992 600 639 643 666 +hsync +vsync (40.3 kHz eP) (II) modeset(0): Output LVDS-1 connected (II) modeset(0): Using exact sizes for initial modes (II) modeset(0): Output LVDS-1 using initial mode 800x600 +0+0 (II) modeset(0): Using default gamma of (1.0, 1.0, 1.0) unless otherwise stated. (==) modeset(0): DPI set to (96, 96) (II) Loading sub module "fb" (II) LoadModule: "fb" (II) Loading /usr/local/XSGX/lib/xorg/modules/libfb.so (II) Module fb: vendor="X.Org Foundation" compiled for 1.18.4, module version = 1.0.0 ABI class: X.Org ANSI C Emulation, version 0.4 (==) Depth 24 pixmap format is 32 bpp (==) modeset(0): Backing store enabled (==) modeset(0): Silken mouse enabled (II) modeset(0): RandR 1.2 enabled, ignore the following RandR disabled message. (EE) modeset(0): failed to set mode: Invalid argument (EE) Fatal server error: (EE) AddScreen/ScreenInit failed for driver 0 (EE) (EE) Please consult the The X.Org Foundation support at http://wiki.x.org for help. (EE) Please also check the log file at "/usr/local/XSGX/var/log/Xorg.0.log" for additional information. (EE) (EE) Server terminated with error (1). Closing log file.