**** Build of configuration Debug for project gpioLEDBlink **** "C:\\TI\\ccsv6\\utils\\bin\\gmake" -k -j 8 -s all -O 'Building file: C:/Users/agolestani/workspace_v6_2/AM335X_StarterWare_02_00_01_01/examples/beaglebone/gpio/gpioLEDBlink.c' 'Invoking: ARM Compiler' 'Finished building: C:/Users/agolestani/workspace_v6_2/AM335X_StarterWare_02_00_01_01/examples/beaglebone/gpio/gpioLEDBlink.c' ' ' 'Building target: ../../../../../../../binary/armv7a/cgt_ccs/am335x/beaglebone/gpio/Debug/gpioLEDBlink.out' 'Invoking: ARM Linker' warning #10366-D: automatic library build: using library "C:\TI\ccsv6\tools\compiler\ti-cgt-arm_5.2.5\lib\rtsv7A8_A_le_eabi.lib" for the first time, so it must be built. This may take a few minutes. gmake.exe[1]: warning: -jN forced in submake: disabling jobserver mode. 0 [main] sh 34932 sync_with_child: child 15344(0x1D0) died before initialization with status code 0xC0000142 278430 [main] sh 34932 sync_with_child: *** child state waiting for longjmp /usr/bin/sh: fork: Resource temporarily unavailable gmake.exe[1]: *** [library] Error 128 >> ERROR: mklib: gmake error during rtsv7A8_A_le_eabi.lib build warning #10207-D: automatic RTS selection: resolving index library "libc.a" to "rtsv7A8_A_le_eabi.lib", but "rtsv7A8_A_le_eabi.lib" was not found error #10198-D: no input section is linked in warning #10062-D: entry-point symbol "_c_int00" undefined warning #10202-D: no suitable entry-point found; setting to 0 error #10010: errors encountered during linking; "../../../../../../../binary/armv7a/cgt_ccs/am335x/beaglebone/gpio/Debug/gpi oLEDBlink.out" not built gmake: *** [../../../../../../../binary/armv7a/cgt_ccs/am335x/beaglebone/gpio/Debug/gpioLEDBlink.out] Error 1 Makefile:1937: recipe for target 'library' failed >> Compilation failure makefile:144: recipe for target '../../../../../../../binary/armv7a/cgt_ccs/am335x/beaglebone/gpio/Debug/gpioLEDBlink.out' failed gmake: Target 'all' not remade because of errors. **** Build Finished ****