-Software Package Notice- This is a prerelease version of the control software for TIDA-01606. TI provides this software “as is” and with all faults and disclaims all warranties, express or implied, regarding such software. This software is solely intended for evaluation purposes to assistant users in becoming familiar with the TMS320 device, drivers for TIDA-01606 hardware, and control loop structure. It is not intended to be used in production applications and it does not come with additional usage documentation beyond this document. This release has only been tested with ideal sources and resistive loads in a laboratory environment. The end user is solely responsible for any additional usage and testing. Install Instructions: 1. Download and install the C2000 Digital Power SDK (version 1.03.00.00) from http://www.ti.com/tool/C2000WARE-DIGITALPOWER-SDK to the default directories (c:\ti\c2000\C2000Ware_DigitalPower_SDK_1_03_00_00) 2. Install the TIDA-01606 software release. It will extract the relevant files into the solutions folder that resides in the SDK directory. 3. Using CCS8.3, ensure that the latest C2000 device support packages are installed and avaliable. 4. In the desired workspace, in CCS, use Project>Import CCS Project. 5. Select the location of the projectspec as the search directory (default: C:\ti\c2000\C2000Ware_DigitalPower_SDK_1_03_00_00\solutions\tida_01606\f2837x\ccs). Ensure that Copy Projects Into WOrkspace is selected and import the project.