/****************************************************************************** * * Default Linker Command file for the Texas Instruments LM3S9D92 * * This is part of revision 10114 of the Stellaris Peripheral Driver Library. * *****************************************************************************/ #define APP_BASE 0x00002000 #define RAM_BASE 0x20000000 --retain=g_pfnVectors MEMORY { FLASH1 (RX) : origin = 0x00000000, length = 0x00002000 FLASH (RX) : origin = 0x00002000, length = 0x0007E000 SRAM (RWX) : origin = 0x20000000, length = 0x00018000 } /* The following command line options are set as part of the CCS project. */ /* If you are building using the command line, or for some reason want to */ /* define them here, you can uncomment and modify these lines as needed. */ /* If you are using CCS for building, it is probably better to make any such */ /* modifications in your CCS project and leave this file alone. */ /* */ /* --heap_size=0 */ /* --stack_size=256 */ /* --library=rtsv7M3_T_le_eabi.lib */ /* Section allocation in memory */ SECTIONS { /* .intvecs: > APP_BASE */ .resetVecs: load > APP_BASE .text : > FLASH .const : > FLASH .cinit : > FLASH .pinit : > FLASH .init_array : > FLASH .vtable : > RAM_BASE .data : > SRAM .bss : > SRAM .sysmem : > SRAM .stack : > SRAM } __STACK_TOP = __stack + 512;