//********************************* Headers**************************************** #include #include #include #include #include #include #include //********************************** Global Variables ***************************** #define MCLK_FREQ_MHZ 8 // MCLK = 8MHz volatile unsigned int p=0; volatile unsigned int q=0; volatile unsigned int r=0; volatile unsigned int s=0; volatile unsigned int t=0; volatile unsigned int u=0; volatile unsigned int v=0; volatile unsigned int x=0; volatile unsigned int y=0; volatile unsigned int z=0; volatile unsigned int a=0; volatile unsigned int b=0; int temp, code, counter=0; char done[4] = {'D','O','N','E'}; unsigned char RXData[6]; unsigned char TXData; unsigned int i, flag=0; // to avoid computing code when * or # are pressed //********************************* Global Pointers ******************************** #define FRAM_counter_static 0x1800 // counter to always point at the start of the FRAM address #define FRAM_TEST_START 0x1802 // unsigned int *FRAM_write_ptr; // FRAM pointer to write unsigned int *FRAM_read_ptr; // FRAM pointer to read unsigned int *FRAM_counter_ptr; // counter pointer to read or write codes in to FRAM //********************************** Function Prototype Declarations *************** void Software_Trim(); // to get best possible clock (Helps with UART) void Initialize(void); // to initialize LCD void Display(char); // to display characters to LCD void Init_GPIO(); // to initialize GPIO's void Entercode(); // to enter the new code for the user after pressing * void getKeypad(); // to get the key pressed on the keypad void FRAMWrite(int); // to write the code into FRAM int FRAMRead(int); // to read existing code form FRAM void Init_FRAM(); // to delete all the codes from FRAM except Master code void Codecompare(int); // to compare the code entered with codes in FRAM void Dltcode(); // to delete a certain code int index_read=0; int index_write=0; unsigned int codes[10]; int main(void) { WDTCTL = WDTPW | WDTHOLD; // Stop watchdog timer PM5CTL0 &= ~LOCKLPM5; // Disable the GPIO power-on default high-impedance mode FRAM_counter_ptr = (unsigned int *)FRAM_counter_static; // always pointed to 1800 location. This is where counter is located // ************************************************************************ clock config // comment CLOCK config SPI works and UART doesn't ..... uncomment UART works SPI doesn't __bis_SR_register(SCG0); // disable FLL CSCTL3 |= SELREF__REFOCLK; // Set REFO as FLL reference source CSCTL1 = DCOFTRIMEN|DCOFTRIM0|DCOFTRIM1|DCORSEL_3|DISMOD; // Enable frequency trim | DCOFTRIM=3, DCO Range = 8MHz | modulation disabled CSCTL2 = FLLD_0 + 243; // DCODIV = 8MHz __delay_cycles(3); __bic_SR_register(SCG0); // enable FLL Software_Trim(); // Software Trim to get the best DCOFTRIM value CSCTL4 = SELMS__DCOCLKDIV | SELA__REFOCLK; // set default REFO(~32768Hz) as ACLK source, ACLK = 32768Hz // ********************************************************************************************* P1SEL0 |= BIT4 | BIT5 | BIT6; // set 3-SPI pin as second function UCA0CTLW0 |= UCSWRST; // **Put state machine in reset** UCA0CTLW0 |= UCMST | UCSYNC | UCCKPL | UCMSB | UCMODE_0; // Master Mode | Sync mode | Inactive when CLK High | MSB first | 3-pin, 8-bit SPI master UCA0CTLW0 |= UCSSEL__SMCLK; // SMCLK UCA0BR0 = 0x08; // /2,fBitClock = fBRCLK/(UCBRx+1). UCA0BR1 = 0; UCA0MCTLW = 0; // No modulation UCA0CTLW0 &= ~UCSWRST; // **Initialize USCI state machine** //UCA0IE |= UCRXIE; //**************************************************************************************************** P2SEL0 |= BIT5 | BIT6; // set 2-UART pin as second function UCA1CTLW0 |= UCSWRST; UCA1CTLW0 |= UCSSEL__SMCLK; UCA1BR0 = 52; // 8000000/16/9600 UCA1BR1 = 0x00; UCA1MCTLW = 0x4900 | UCOS16 | UCBRF_1; //UCA1STATW |= 0x0080; UCA1CTLW0 &= ~UCSWRST; UCA1IE |= UCRXIE; // Enable USCI_A0 RX interrupt //__bis_SR_register(LPM0_bits|GIE); // Enter LPM3, interrupts enabled __no_operation(); //************************************************************************************************************** P1DIR &= ~BIT0; // Set P1.0 as input Manually excecute the code pin Init_FRAM(); // Delete all the codes except Master code //FRAMWrite(Master_Code); // Writing the Master code to the FRAM //FRAMWrite(counter); // to keep track of FRAM memory location Init_GPIO(); // Initialize GPIO's Initialize(); //__enable_interrupt(); // enable all interrupts --> GIE = 1 (HIGH) while(1) { P1OUT &= ~BIT2; // clear pin CS2 to select chip P1OUT |= BIT7; // set A0 to enable write data __delay_cycles(10000); // Delay before next transmission Display('C'); Display('O'); Display('D'); Display('E'); Display(' '); Display('I'); Display('N'); Display('?'); P1OUT &= ~BIT2; // clear pin CS2 to select chip P1OUT &= ~BIT7; // clear pin A0 to enter command mode __delay_cycles(4000); // Delay before next transmission UCA0TXBUF = 0xC0; // Setting Address register to Second line while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(1000); // Delay before next transmission P1OUT &= ~BIT7; // clear pin A0 to enter command mode Default P1OUT |= BIT2; // Set the pin CS, Deselecting Chip int f=1000,j; code=0; for(i=0;i<4;i++) { getKeypad(); code = (code+(f*temp)); f = f/10; } Codecompare(code); } } // UART Interrupt *********************************************************** void OTA_code() { int j; for(j=0;j<6;j++) { while (!(UCA1IFG & UCRXIFG)) /*EMPTY*/; RXData[j] = UCA1RXBUF; } __no_operation(); __no_operation(); __no_operation(); __no_operation(); __delay_cycles(10000); __no_operation(); } void Codecompare(int code) { P1OUT &= ~BIT7; // clear pin A0 to enter command mode Default P1OUT |= BIT2; // Set the pin CS, Deselecting Chip P1OUT &= ~BIT2; // clear pin CS2 to select chip P1OUT &= ~BIT7; // clear pin A0 to enter command mode __delay_cycles(10000); // Delay before next transmission UCA0TXBUF = 0x01; // Clear Display while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(10000); // Delay before next transmission if(flag==0) // no comparison when * or # are pressed { int a=FRAMRead(code); if(0!=a) { char codestr[5], *codep; snprintf(codestr, sizeof(codestr), "%d", code); // format as characters for(codep = codestr;*codep != '\0';++codep) // send them one at a time { while(!(UCA1IFG & UCTXIFG)); //while (UCA1STATW & UCBUSY); // byte sent? UCA1TXBUF = (*codep); while (UCA1STATW & UCBUSY); // byte sent? //while(!(UCA1IFG & UCTXIFG)); } while(!(UCA1IFG & UCTXIFG)); UCA1TXBUF = 'X'; // Sending end character while (UCA1STATW & UCBUSY); // byte sent? P1OUT ^= BIT0; // toogle p1.0 __delay_cycles(18000); if(P1IN & BIT0) // is set say open { Display('O'); Display('N'); Display(' '); } else // if clear say close { Display('O'); Display('F'); Display('F'); Display(' '); } } else // incorrect code entered { __delay_cycles(8000); // Delay before next transmission Display('W'); Display('R'); Display('O'); Display('N'); Display('G'); P1OUT &= ~BIT2; // clear pin CS2 to select chip P1OUT &= ~BIT7; // clear pin A0 to enter command mode __delay_cycles(10000); // Delay before next transmission UCA0TXBUF = 0xC0; // Setting Address register to Second line while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(8000); // Delay before next transmission P1OUT &= ~BIT7; // clear pin A0 to enter command mode Default P1OUT |= BIT2; // Set the pin CS, Deselecting Chip } } else flag=0; } void Entercode() { P1OUT &= ~BIT2; // clear pin CS2 to select chip P1OUT &= ~BIT7; // clear pin A0 to enter command mode __delay_cycles(4000); // Delay before next transmission while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? UCA0TXBUF = 0x01; // Clear Display while (UCA0STATW & UCBUSY); // byte sent? __delay_cycles(100); // Delay before next transmission P1OUT |= BIT7; // set A0 to enable write data __delay_cycles(12000); // Delay before next transmission while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? Display('N'); Display('E'); Display('W'); Display(' '); Display('C'); Display('O'); Display('D'); Display('E'); while (UCA0STATW & UCBUSY); // byte sent? P1OUT &= ~BIT2; // clear pin CS2 to select chip P1OUT &= ~BIT7; // clear pin A0 to enter command mode __delay_cycles(4000); // Delay before next transmission UCA0TXBUF = 0xC0; // Setting Address register to Second line while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(100); // Delay before next transmission int f=1000; for(i=0;i<4;i++) { getKeypad(); code = (code+(f*temp)); f = f/10; } int a=FRAMRead(code); P1OUT |= BIT7; // set A0 to enable write data __delay_cycles(12000); // Delay before next transmission if(0==a) // No matching code found { FRAMWrite(code); Display('D'); Display('O'); Display('N'); Display('E'); } else if(0!=a) // code already exists { Display('T'); Display('A'); Display('K'); Display('E'); Display('N'); } P1OUT &= ~BIT7; // clear pin A0 to enter command mode Default P1OUT |= BIT2; // Set the pin CS, Deselecting Chip } void Dltcode() { P1OUT &= ~BIT2; // clear pin CS2 to select chip P1OUT &= ~BIT7; // clear pin A0 to enter command mode __delay_cycles(4000); // Delay before next transmission UCA0TXBUF = 0x01; // Clear Display while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(100); // Delay before next transmission P1OUT |= BIT7; // set A0 to enable write data __delay_cycles(12000); // Delay before next transmission Display('D'); Display('L'); Display('T'); Display(' '); Display('C'); Display('O'); Display('D'); Display('E'); P1OUT &= ~BIT2; // clear pin CS2 to select chip P1OUT &= ~BIT7; // clear pin A0 to enter command mode __delay_cycles(4000); // Delay before next transmission UCA0TXBUF = 0xC0; // Setting Address register to Second line while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(100); // Delay before next transmission int f=1000; for(i=0;i<4;i++) { getKeypad(); code = (code+(f*temp)); f = f/10; } int check=1; check = FRAMRead(code); // index where the dlt code is located, need to delete this location counter = *FRAM_counter_ptr; if(0!=check) // code found { FRAM_read_ptr = (unsigned int *)FRAM_TEST_START; // address to read 1802 FRAM_write_ptr = (unsigned int *)FRAM_TEST_START; // address to write inititially 0x1802 SYSCFG0 = FRWPPW | PFWP; // not protecting the data section so that we can write to the data section while the program section is protected FRAM_read_ptr = FRAM_read_ptr + check; // Reading from the location after delete location FRAM_write_ptr = FRAM_write_ptr + check - 1; // pointing it to write to delete location for(;check <= counter;check++) { *FRAM_write_ptr = *FRAM_read_ptr; // copies data from next location to delete location *FRAM_write_ptr++; // Next location *FRAM_read_ptr++; // Next location } counter = *FRAM_counter_ptr; counter--; *FRAM_counter_ptr = counter; SYSCFG0 = FRWPPW | PFWP | DFWP; // NOW WE ARE PROTECTING THE DATA SECTION AND THE PROGRAM SECTION } } void FRAMWrite(int FRAM_Code) { FRAM_write_ptr = (unsigned int *)FRAM_TEST_START; // address to write inititially 0x1802 SYSCFG0 = FRWPPW | PFWP; // not protecting the data section so that we can write to the data section while the program section is protected counter = *FRAM_counter_ptr; FRAM_write_ptr = FRAM_write_ptr + counter; *FRAM_write_ptr = FRAM_Code; //*FRAM_write_ptr++; counter++; *FRAM_counter_ptr = counter; SYSCFG0 = FRWPPW | PFWP | DFWP; // NOW WE ARE PROTECTING THE DATA SECTION AND THE PROGRAM SECTION } int FRAMRead(int FRAM_Code) { int j,temp=0; FRAM_read_ptr = (unsigned int *)FRAM_TEST_START; // address to read 1802 if(FRAM_Code != 0) { for(j=1;j<10;j++) { if(FRAM_Code == *FRAM_read_ptr++) // comparing codes to FRAM { temp=j; break; } // 0 if there is a match } } return(temp); } void Init_FRAM() // Factory reset FRAM { int i,temp = 0000; // avoid this code all the time FRAM_write_ptr = (unsigned int *)0x1800; // address to write SYSCFG0 = FRWPPW | PFWP; // not protecting the data section so that we can write to the data section while the program section is protected for(i=0;i<12;i++) // 10 code limit { *FRAM_write_ptr = temp; *FRAM_write_ptr++; } SYSCFG0 = FRWPPW | PFWP | DFWP; // Now we are protecting the data section and the program section temp = 7777; FRAMWrite(temp); } void Initialize() { UCA0IE |= UCTXIE; // Enable TX interrupt P1OUT &= ~BIT2; // clear pin CS2 to select chip P1OUT &= ~BIT7; // clear pin A0 to enter command mode __delay_cycles(12000); // Delay before next transmission UCA0TXBUF = 0x38; // Function Set while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? while (UCA0STATW & UCBUSY); // byte sent? __delay_cycles(1000); // Delay before next transmission UCA0TXBUF = 0x0F; // Display ON while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? while (UCA0STATW & UCBUSY); // byte sent? __delay_cycles(1000); // Delay before next transmission UCA0TXBUF = 0x01; // Clear Display while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? while (UCA0STATW & UCBUSY); // byte sent? __delay_cycles(90000); // Delay before next transmission UCA0TXBUF = 0x06; // Entry Mode Set while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? while (UCA0STATW & UCBUSY); // byte sent? __delay_cycles(1000); // Delay before next transmission P1OUT |= BIT2; // Set the pin CS unselect chip P1OUT &= ~BIT7; // Clear pin dafault command mode __delay_cycles(10000); // Delay before next transmission //*************************************************************************************************************************************************** } void Init_GPIO() { P1DIR = 0xFF; P2DIR = 0xFF; P3DIR = 0xFF; P1REN = 0xFF; P2REN = 0xFF; P3REN = 0xFF; P1OUT = 0x00; P2OUT = 0x00; P3OUT = 0x00; P1DIR |= BIT1; // setting p1.1 as output P1OUT &= ~BIT1; // Clearing P1.1 P2DIR |= BIT2; // setting p2.2 as output P2OUT &= ~BIT2; // Clearing P2.2 P3DIR |= BIT2; // setting p3.2 as output P3OUT &= ~BIT2; // Clearing P3.2 P2DIR &= ~BIT7; // Setting p2.7 as input P3DIR &= ~BIT1; // Setting p3.1 as input P2DIR &= ~BIT1; // Setting p2.1 as input P2DIR &= ~BIT0; // Setting p2.0 as input P1DIR |= BIT0; // setting p1.0 as output P1OUT &= ~BIT0; // Clearing P1.0, initially LED OFF // For LCD P1DIR |= BIT7; // Setting it to output direction, A0 of LCD or RS resister Select P1DIR |= BIT2; // Setting it to output direction, CS1 of the LCD, normally High, need to pull low before transferring data P1OUT |= BIT2; // Set the pin CS Deselect LCD } void getKeypad() { int i; P1OUT &= ~BIT1; // Clearing P1.1 P2OUT &= ~BIT2; // Clearing P2.2 P3OUT &= ~BIT2; // Clearing P3.2 while(1) { if(UCA1IFG & UCRXIFG) //(UCA1IV != 0) {OTA_code();} for(i=0;i<10000;i++){;} /*********************** Scanning Column 1 ***********************/ P1OUT |= BIT1; // Setting p1.1 if(P2IN & BIT7) { if(p==0) { Display('1'); // DIsplaying 1 on UART p=1; for(i=0;i<10000;i++){;} temp = 1; break; } } else { p=0; for(i=0;i<10000;i++){;} } if(P3IN & BIT1) { if(q==0) { Display('4'); // DIsplaying 4 on UART q=1; temp = 4; break; } } else q=0; if(P2IN & BIT1) { if(r==0) { Display('7'); // DIsplaying 7 on UART r=1; temp = 7; break; } } else r=0; if(P2IN & BIT0) { if(s==0) { Display('*'); // DIsplaying * on UART s=1; //index_write++; Entercode(); flag=1; i=4; break; } } else s=0; P1OUT &= ~BIT1; // Clearing P1.1 for(i=0;i<10000;i++){;} /*********************** Scanning Column 2 ***********************/ P2OUT |= BIT2; // Setting p2.2 if(P2IN & BIT7) { if(t==0) { Display('2'); // DIsplaying 2 on UART for(i=0;i<10000;i++){;} t=1; temp = 2; break; } } else{ t=0; for(i=0;i<10000;i++){;} } if(P3IN & BIT1) { if(u==0) { Display('5'); // DIsplaying 5 on UART u=1; temp = 5; break; } } else u=0; if(P2IN & BIT1) { if(v==0) { Display('8'); // DIsplaying 8 on UART v=1; temp = 8; break; } } else v=0; if(P2IN & BIT0) { if(x==0) { Display('0'); // DIsplaying 0 on UART x=1; temp = 0; break; } } else x=0; P2OUT &= ~BIT2; // Clearing P2.2 for(i=0;i<10000;i++){;} /*********************** Scanning Column 3 ***********************/ P3OUT |= BIT2; // Setting p3.2 if(P2IN & BIT7) { if(y==0) { Display('3'); // DIsplaying 3 on UART for(i=0;i<10000;i++){;} y=1; temp = 3; break; } } else{ y=0; for(i=0;i<10000;i++){;} } if(P3IN & BIT1) { if(z==0) { Display('6'); // DIsplaying 6 on UART z=1; temp = 6; break; } } else z=0; if(P2IN & BIT1) { if(a==0) { Display('9'); // DIsplaying 9 on UART a=1; temp = 9; break; } } else a=0; if(P2IN & BIT0) { if(b==0) { Display('#'); // DIsplaying # on UART b=1; Dltcode(); flag=1; i=4; break; } } else b=0; P3OUT &= ~BIT2; // Clearing P3.2 for(i=0;i<10000;i++){;} } } void Display(char word) { P1OUT &= ~BIT2; // clear pin CS2 to select chip P1OUT |= BIT7; // set A0 to enable write data __delay_cycles(4000); // Delay before next transmission switch(word) { case 'A': UCA0TXBUF = 0x41; // Sending A to LCD while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(4000); // Delay before next transmission break; case 'B': UCA0TXBUF = 0x42; // Sending B to LCD while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(4000); // Delay before next transmission break; case 'C': UCA0TXBUF = 0x43; // Sending C to LCD while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(4000); // Delay before next transmission break; case 'D': UCA0TXBUF = 0x44; // Sending D to LCD while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(4000); // Delay before next transmission break; case 'E': UCA0TXBUF = 0x45; // Sending E to LCD while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(4000); // Delay before next transmission break; case 'F': UCA0TXBUF = 0x46; // Sending F to LCD while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(4000); // Delay before next transmission break; case 'G': UCA0TXBUF = 0x47; // Sending G to LCD while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(4000); // Delay before next transmission break; case 'H': UCA0TXBUF = 0x48; // Sending H to LCD while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(4000); // Delay before next transmission break; case 'I': UCA0TXBUF = 0x49; // Sending I to LCD while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(4000); // Delay before next transmission break; case 'J': UCA0TXBUF = 0x4A; // Sending J to LCD while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(4000); // Delay before next transmission break; case 'K': UCA0TXBUF = 0x4B; // Sending K to LCD while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(4000); // Delay before next transmission break; case 'L': UCA0TXBUF = 0x4C; // Sending L to LCD while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(4000); // Delay before next transmission break; case 'M': UCA0TXBUF = 0x4D; // Sending M to LCD while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(4000); // Delay before next transmission break; case 'N': UCA0TXBUF = 0x4E; // Sending N to LCD while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(4000); // Delay before next transmission break; case 'O': UCA0TXBUF = 0x4F; // Sending O to LCD while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(4000); // Delay before next transmission break; case 'P': UCA0TXBUF = 0x50; // Sending P to LCD while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(4000); // Delay before next transmission break; case 'Q': UCA0TXBUF = 0x51; // Sending Q to LCD while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(4000); // Delay before next transmission break; case 'R': UCA0TXBUF = 0x52; // Sending R to LCD while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(4000); // Delay before next transmission break; case 'S': UCA0TXBUF = 0x53; // Sending S to LCD while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(4000); // Delay before next transmission break; case 'T': UCA0TXBUF = 0x54; // Sending T to LCD while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(4000); // Delay before next transmission break; case 'U': UCA0TXBUF = 0x55; // Sending U to LCD while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(4000); // Delay before next transmission break; case 'V': UCA0TXBUF = 0x56; // Sending V to LCD while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(4000); // Delay before next transmission break; case 'W': UCA0TXBUF = 0x57; // Sending W to LCD while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(4000); // Delay before next transmission break; case 'X': UCA0TXBUF = 0x58; // Sending X to LCD while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(4000); // Delay before next transmission break; case 'Y': UCA0TXBUF = 0x59; // Sending Y to LCD while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(4000); // Delay before next transmission break; case 'Z': UCA0TXBUF = 0x5A; // Sending Z to LCD while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(4000); // Delay before next transmission break; case '0': UCA0TXBUF = 0x30; // Sending 0 to LCD while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(4000); // Delay before next transmission break; case '1': UCA0TXBUF = 0x31; // Sending 1 to LCD while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(4000); // Delay before next transmission break; case '2': UCA0TXBUF = 0x32; // Sending 2 to LCD while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(4000); // Delay before next transmission break; case '3': UCA0TXBUF = 0x33; // Sending 3 to LCD while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(4000); // Delay before next transmission break; case '4': UCA0TXBUF = 0x34; // Sending 4 to LCD while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(4000); // Delay before next transmission break; case '5': UCA0TXBUF = 0x35; // Sending 5 to LCD while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(4000); // Delay before next transmission break; case '6': UCA0TXBUF = 0x36; // Sending 6 to LCD while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(4000); // Delay before next transmission break; case '7': UCA0TXBUF = 0x37; // Sending 7 to LCD while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(4000); // Delay before next transmission break; case '8': UCA0TXBUF = 0x38; // Sending 8 to LCD while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(4000); // Delay before next transmission break; case '9': UCA0TXBUF = 0x39; // Sending 9 to LCD while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(4000); // Delay before next transmission break; case '?': UCA0TXBUF = 0x3F; // Sending ? to LCD while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(4000); // Delay before next transmission break; case '#': UCA0TXBUF = 0x23; // Sending # to LCD while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(4000); // Delay before next transmission break; case '*': UCA0TXBUF = 0x2A; // Sending * to LCD while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(4000); // Delay before next transmission break; case ' ': UCA0TXBUF = 0x20; // Sending blank to LCD while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(4000); // Delay before next transmission break; case ';': UCA0TXBUF = 0x3B; // Sending ; to LCD while (!(UCA0IFG & UCTXIFG)); // USCI_A0 TX buffer ready? __delay_cycles(4000); // Delay before next transmission break; } P1OUT |= BIT2; // Set the pin CS, Deselecting Chip P1OUT &= ~BIT7; // clear pin A0 to enter command mode Default } void Software_Trim() { unsigned int oldDcoTap = 0xffff; unsigned int newDcoTap = 0xffff; unsigned int newDcoDelta = 0xffff; unsigned int bestDcoDelta = 0xffff; unsigned int csCtl0Copy = 0; unsigned int csCtl1Copy = 0; unsigned int csCtl0Read = 0; unsigned int csCtl1Read = 0; unsigned int dcoFreqTrim = 3; unsigned char endLoop = 0; do { CSCTL0 = 0x100; // DCO Tap = 256 do { CSCTL7 &= ~DCOFFG; // Clear DCO fault flag }while (CSCTL7 & DCOFFG); // Test DCO fault flag __delay_cycles((unsigned int)3000 * MCLK_FREQ_MHZ);// Wait FLL lock status (FLLUNLOCK) to be stable // Suggest to wait 24 cycles of divided FLL reference clock while((CSCTL7 & (FLLUNLOCK0 | FLLUNLOCK1)) && ((CSCTL7 & DCOFFG) == 0)); csCtl0Read = CSCTL0; // Read CSCTL0 csCtl1Read = CSCTL1; // Read CSCTL1 oldDcoTap = newDcoTap; // Record DCOTAP value of last time newDcoTap = csCtl0Read & 0x01ff; // Get DCOTAP value of this time dcoFreqTrim = (csCtl1Read & 0x0070)>>4;// Get DCOFTRIM value if(newDcoTap < 256) // DCOTAP < 256 { newDcoDelta = 256 - newDcoTap; // Delta value between DCPTAP and 256 if((oldDcoTap != 0xffff) && (oldDcoTap >= 256)) // DCOTAP cross 256 endLoop = 1; // Stop while loop else { dcoFreqTrim--; CSCTL1 = (csCtl1Read & (~(DCOFTRIM0+DCOFTRIM1+DCOFTRIM2))) | (dcoFreqTrim<<4); } } else // DCOTAP >= 256 { newDcoDelta = newDcoTap - 256; // Delta value between DCPTAP and 256 if(oldDcoTap < 256) // DCOTAP cross 256 endLoop = 1; // Stop while loop else { dcoFreqTrim++; CSCTL1 = (csCtl1Read & (~(DCOFTRIM0+DCOFTRIM1+DCOFTRIM2))) | (dcoFreqTrim<<4); } } if(newDcoDelta < bestDcoDelta) // Record DCOTAP closest to 256 { csCtl0Copy = csCtl0Read; csCtl1Copy = csCtl1Read; bestDcoDelta = newDcoDelta; } }while(endLoop == 0); // Poll until endLoop == 1 CSCTL0 = csCtl0Copy; // Reload locked DCOTAP CSCTL1 = csCtl1Copy; // Reload locked DCOFTRIM while(CSCTL7 & (FLLUNLOCK0 | FLLUNLOCK1)); // Poll until FLL is locked }