**** Build of configuration Debug for project HID Sensor Fusion_Float **** "C:\\ti\\ccsv5\\utils\\bin\\gmake" -k all 'Building target: HID Sensor Fusion.out' 'Invoking: MSP430 Linker' "C:/ti/ccsv5/tools/compiler/msp430_4.2.1/bin/cl430" -vmspx --abi=eabi --code_model=small --data_model=small -O0 -g --define=__MSP430F5529__ --diag_warning=225 --silicon_errata=CPU21 --silicon_errata=CPU22 --silicon_errata=CPU23 --silicon_errata=CPU40 --printf_support=full -z -m"HID Sensor Fusion.map" --heap_size=160 --stack_size=160 --use_hw_mpy=F5 -i"C:/ti/ccsv5/ccs_base/msp430/include" -i"C:/ti/ccsv5/tools/compiler/msp430_4.2.1/lib" -i"C:/ti/ccsv5/tools/compiler/msp430_4.2.1/include" -i"C:/ti/ccsv5/ccs_base/msp430/lib" --reread_libs --warn_sections --xml_link_info="HID Sensor Fusion_linkInfo.xml" --rom_model -o "HID Sensor Fusion.out" "./DCM_Algorithm/Vector.obj" "./DCM_Algorithm/Matrix.obj" "./DCM_Algorithm/DCM.obj" "./F5xx_F6xx_Core_Lib/HAL_UCS.obj" "./F5xx_F6xx_Core_Lib/HAL_TLV.obj" "./F5xx_F6xx_Core_Lib/HAL_PMM.obj" "./F5xx_F6xx_Core_Lib/HAL_PMAP.obj" "./F5xx_F6xx_Core_Lib/HAL_FLASH.obj" "./MSP-EXP430F5529_HAL/HAL_Wheel.obj" "./MSP-EXP430F5529_HAL/HAL_Dogs102x6.obj" "./MSP-EXP430F5529_HAL/HAL_Buttons.obj" "./MSP-EXP430F5529_HAL/HAL_Board.obj" "./USB_API/USB_CDC_API/UsbCdc.obj" "./USB_API/USB_Common/usb.obj" "./USB_API/USB_Common/dma.obj" "./USB_API/USB_HID_API/UsbHidReq.obj" "./USB_API/USB_HID_API/UsbHid.obj" "./USB_API/USB_MSC_API/UsbMscStateMachine.obj" "./USB_API/USB_MSC_API/UsbMscScsi.obj" "./USB_API/USB_MSC_API/UsbMscReq.obj" "./USB_API/USB_PHDC_API/UsbPHDC.obj" "./USB_config/descriptors.obj" "./USB_config/UsbIsr.obj" "./sensorlib/vector.obj" "./sensorlib/comp_dcm.obj" "./sensorlib/HAL_Cma3000.obj" "./usbEventHandling.obj" "./usbConstructs.obj" "./main.obj" "../MSPMATHLIB_CCS_msp430_small_code_small_data.lib" "../lnk_msp430f5529.cmd" "../msp430USB.cmd" -l"libmath.a" -l"libc.a" warning: automatic library build: using library "C:\ti\ccsv5\tools\compiler\msp430_4.2.1\lib\rts430x_sc_sd_eabi.lib" for the first time, so it must be built. This may take a few minutes. 1 [main] sh 5524 find_fast_cwd: WARNING: Couldn't compute FAST_CWD pointer. Please report this problem to the public mailing list cygwin@cygwin.com cygwin warning: MS-DOS style path detected: C:\SyncFolder\Platform\MSP430\CCS\HID Sensor Fusion_Float\Debug Preferred POSIX equivalent is: /cygdrive/c/SyncFolder/Platform/MSP430/CCS/HID Sensor Fusion_Float/Debug CYGWIN environment variable option "nodosfilewarning" turns off this warning. Consult the user's guide for more details about POSIX paths: http://cygwin.com/cygwin-ug-net/using.html#using-pathnames 1 [main] sh 9044 find_fast_cwd: WARNING: Couldn't compute FAST_CWD pointer. Please report this problem to the public mailing list cygwin@cygwin.com cygwin warning: MS-DOS style path detected: C:\SyncFolder\Platform\MSP430\CCS\HID Sensor Fusion_Float\Debug Preferred POSIX equivalent is: /cygdrive/c/SyncFolder/Platform/MSP430/CCS/HID Sensor Fusion_Float/Debug CYGWIN environment variable option "nodosfilewarning" turns off this warning. Consult the user's guide for more details about POSIX paths: http://cygwin.com/cygwin-ug-net/using.html#using-pathnames 0 [main] sh 1208 find_fast_cwd: WARNING: Couldn't compute FAST_CWD pointer. Please report this problem to the public mailing list cygwin@cygwin.com cygwin warning: MS-DOS style path detected: C:\SyncFolder\Platform\MSP430\CCS\HID Sensor Fusion_Float\Debug Preferred POSIX equivalent is: /cygdrive/c/SyncFolder/Platform/MSP430/CCS/HID Sensor Fusion_Float/Debug CYGWIN environment variable option "nodosfilewarning" turns off this warning. Consult the user's guide for more details about POSIX paths: http://cygwin.com/cygwin-ug-net/using.html#using-pathnames --> error: '*.obj ' not found gmake.exe[1]: *** [library] Error 1 >> ERROR: mklib: gmake error during rts430x_sc_sd_eabi.lib build warning: automatic RTS selection: resolving index library "libc.a" to "C:\ti\ccsv5\tools\compiler\msp430_4.2.1\lib\rts430x_sc_sd_eabi.lib", but "C:\ti\ccsv5\tools\compiler\msp430_4.2.1\lib\rts430x_sc_sd_eabi.lib" was not found error: no input section is linked in warning: entry-point symbol "_c_int00" undefined warning: no suitable entry-point found; setting to 0 error: errors encountered during linking; "HID Sensor Fusion.out" not built >> Compilation failure gmake: *** [HID Sensor Fusion.out] Error 1 gmake: Target `all' not remade because of errors. **** Build Finished ****