/* --COPYRIGHT--,BSD * Copyright (c) 2012, Texas Instruments Incorporated * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * --/COPYRIGHT--*/ //! \file solutions/instaspin_foc/src/proj_lab05b.c //! \brief Adjusting the speed controller //! //! (C) Copyright 2011, Texas Instruments, Inc. //! \defgroup PROJ_LAB05b PROJ_LAB05b //@{ //! \defgroup PROJ_LAB05b_OVERVIEW Project Overview //! //! Adjusting the supplied speed controller //! // ************************************************************************** // the includes // system includes #include #include "main.h" #ifdef FLASH #pragma CODE_SECTION(mainISR,"ramfuncs"); #endif // Include header files used in the main function // ************************************************************************** // the defines #define LED_BLINK_FREQ_Hz 5 // ************************************************************************** // the globals uint_least16_t gCounter_updateGlobals = 0; bool Flag_Latch_softwareUpdate = true; CTRL_Handle ctrlHandle; #ifdef F2802xF #pragma DATA_SECTION(halHandle,"rom_accessed_data"); #endif HAL_Handle halHandle; #ifdef F2802xF #pragma DATA_SECTION(gUserParams,"rom_accessed_data"); #endif USER_Params gUserParams; HAL_PwmData_t gPwmData = {_IQ(0.0), _IQ(0.0), _IQ(0.0)}; HAL_AdcData_t gAdcData; _iq gMaxCurrentSlope = _IQ(0.0); #ifdef FAST_ROM_V1p6 CTRL_Obj *controller_obj; #else #ifdef F2802xF #pragma DATA_SECTION(ctrl,"rom_accessed_data"); #endif CTRL_Obj ctrl; //v1p7 format #endif uint16_t gLEDcnt = 0; volatile MOTOR_Vars_t gMotorVars = MOTOR_Vars_INIT; #ifdef FLASH // Used for running BackGround in flash, and ISR in RAM extern uint16_t *RamfuncsLoadStart, *RamfuncsLoadEnd, *RamfuncsRunStart; #ifdef F2802xF extern uint16_t *econst_start, *econst_end, *econst_ram_load; extern uint16_t *switch_start, *switch_end, *switch_ram_load; #endif #endif #ifdef DRV8301_SPI // Watch window interface to the 8301 SPI DRV_SPI_8301_Vars_t gDrvSpi8301Vars; #endif #ifdef DRV8305_SPI // Watch window interface to the 8305 SPI DRV_SPI_8305_Vars_t gDrvSpi8305Vars; #endif _iq gFlux_pu_to_Wb_sf; _iq gFlux_pu_to_VpHz_sf; _iq gTorque_Ls_Id_Iq_pu_to_Nm_sf; _iq gTorque_Flux_Iq_pu_to_Nm_sf; // ************************************************************************** // the functions void main(void) { uint_least8_t estNumber = 0; #ifdef FAST_ROM_V1p6 uint_least8_t ctrlNumber = 1; #endif // Only used if running from FLASH // Note that the variable FLASH is defined by the project #ifdef FLASH // Copy time critical code and Flash setup code to RAM // The RamfuncsLoadStart, RamfuncsLoadEnd, and RamfuncsRunStart // symbols are created by the linker. Refer to the linker files. memCopy((uint16_t *)&RamfuncsLoadStart,(uint16_t *)&RamfuncsLoadEnd,(uint16_t *)&RamfuncsRunStart); #ifdef F2802xF //copy .econst to unsecure RAM if(*econst_end - *econst_start) { memCopy((uint16_t *)&econst_start,(uint16_t *)&econst_end,(uint16_t *)&econst_ram_load); } //copy .switch ot unsecure RAM if(*switch_end - *switch_start) { memCopy((uint16_t *)&switch_start,(uint16_t *)&switch_end,(uint16_t *)&switch_ram_load); } #endif #endif // initialize the hardware abstraction layer halHandle = HAL_init(&hal,sizeof(hal)); // check for errors in user parameters USER_checkForErrors(&gUserParams); // store user parameter error in global variable gMotorVars.UserErrorCode = USER_getErrorCode(&gUserParams); // do not allow code execution if there is a user parameter error if(gMotorVars.UserErrorCode != USER_ErrorCode_NoError) { for(;;) { gMotorVars.Flag_enableSys = false; } } // initialize the user parameters USER_setParams(&gUserParams); // set the hardware abstraction layer parameters HAL_setParams(halHandle,&gUserParams); // initialize the controller #ifdef FAST_ROM_V1p6 ctrlHandle = CTRL_initCtrl(ctrlNumber, estNumber); //v1p6 format (06xF and 06xM devices) controller_obj = (CTRL_Obj *)ctrlHandle; #else ctrlHandle = CTRL_initCtrl(estNumber,&ctrl,sizeof(ctrl)); //v1p7 format default #endif { CTRL_Version version; // get the version number CTRL_getVersion(ctrlHandle,&version); gMotorVars.CtrlVersion = version; } // set the default controller parameters CTRL_setParams(ctrlHandle,&gUserParams); // setup faults HAL_setupFaults(halHandle); // initialize the interrupt vector table HAL_initIntVectorTable(halHandle); // enable the ADC interrupts HAL_enableAdcInts(halHandle); // enable global interrupts HAL_enableGlobalInts(halHandle); // enable debug interrupts HAL_enableDebugInt(halHandle); // disable the PWM HAL_disablePwm(halHandle); #ifdef DRV8301_SPI // turn on the DRV8301 if present HAL_enableDrv(halHandle); // initialize the DRV8301 interface HAL_setupDrvSpi(halHandle,&gDrvSpi8301Vars); #endif #ifdef DRV8305_SPI // turn on the DRV8305 if present HAL_enableDrv(halHandle); // initialize the DRV8305 interface HAL_setupDrvSpi(halHandle,&gDrvSpi8305Vars); #endif // enable DC bus compensation CTRL_setFlag_enableDcBusComp(ctrlHandle, true); // compute scaling factors for flux and torque calculations gFlux_pu_to_Wb_sf = USER_computeFlux_pu_to_Wb_sf(); gFlux_pu_to_VpHz_sf = USER_computeFlux_pu_to_VpHz_sf(); gTorque_Ls_Id_Iq_pu_to_Nm_sf = USER_computeTorque_Ls_Id_Iq_pu_to_Nm_sf(); gTorque_Flux_Iq_pu_to_Nm_sf = USER_computeTorque_Flux_Iq_pu_to_Nm_sf(); for(;;) { // Waiting for enable system flag to be set while(!(gMotorVars.Flag_enableSys)); // Enable the Library internal PI. Iq is referenced by the speed PI now CTRL_setFlag_enableSpeedCtrl(ctrlHandle, true); // loop while the enable system flag is true while(gMotorVars.Flag_enableSys) { CTRL_Obj *obj = (CTRL_Obj *)ctrlHandle; // increment counters gCounter_updateGlobals++; // enable/disable the use of motor parameters being loaded from user.h CTRL_setFlag_enableUserMotorParams(ctrlHandle,gMotorVars.Flag_enableUserParams); // enable/disable Rs recalibration during motor startup EST_setFlag_enableRsRecalc(obj->estHandle,gMotorVars.Flag_enableRsRecalc); // enable/disable automatic calculation of bias values CTRL_setFlag_enableOffset(ctrlHandle,gMotorVars.Flag_enableOffsetcalc); if(CTRL_isError(ctrlHandle)) { // set the enable controller flag to false CTRL_setFlag_enableCtrl(ctrlHandle,false); // set the enable system flag to false gMotorVars.Flag_enableSys = false; // disable the PWM HAL_disablePwm(halHandle); } else { // update the controller state bool flag_ctrlStateChanged = CTRL_updateState(ctrlHandle); // enable or disable the control CTRL_setFlag_enableCtrl(ctrlHandle, gMotorVars.Flag_Run_Identify); if(flag_ctrlStateChanged) { CTRL_State_e ctrlState = CTRL_getState(ctrlHandle); if(ctrlState == CTRL_State_OffLine) { // enable the PWM HAL_enablePwm(halHandle); } else if(ctrlState == CTRL_State_OnLine) { if(gMotorVars.Flag_enableOffsetcalc == true) { // update the ADC bias values HAL_updateAdcBias(halHandle); } else { // set the current bias HAL_setBias(halHandle,HAL_SensorType_Current,0,_IQ(I_A_offset)); HAL_setBias(halHandle,HAL_SensorType_Current,1,_IQ(I_B_offset)); HAL_setBias(halHandle,HAL_SensorType_Current,2,_IQ(I_C_offset)); // set the voltage bias HAL_setBias(halHandle,HAL_SensorType_Voltage,0,_IQ(V_A_offset)); HAL_setBias(halHandle,HAL_SensorType_Voltage,1,_IQ(V_B_offset)); HAL_setBias(halHandle,HAL_SensorType_Voltage,2,_IQ(V_C_offset)); } // Return the bias value for currents gMotorVars.I_bias.value[0] = HAL_getBias(halHandle,HAL_SensorType_Current,0); gMotorVars.I_bias.value[1] = HAL_getBias(halHandle,HAL_SensorType_Current,1); gMotorVars.I_bias.value[2] = HAL_getBias(halHandle,HAL_SensorType_Current,2); // Return the bias value for voltages gMotorVars.V_bias.value[0] = HAL_getBias(halHandle,HAL_SensorType_Voltage,0); gMotorVars.V_bias.value[1] = HAL_getBias(halHandle,HAL_SensorType_Voltage,1); gMotorVars.V_bias.value[2] = HAL_getBias(halHandle,HAL_SensorType_Voltage,2); // enable the PWM HAL_enablePwm(halHandle); } else if(ctrlState == CTRL_State_Idle) { // disable the PWM HAL_disablePwm(halHandle); gMotorVars.Flag_Run_Identify = false; } if((CTRL_getFlag_enableUserMotorParams(ctrlHandle) == true) && (ctrlState > CTRL_State_Idle) && (gMotorVars.CtrlVersion.minor == 6)) { // call this function to fix 1p6 USER_softwareUpdate1p6(ctrlHandle); } } } if(EST_isMotorIdentified(obj->estHandle)) { // set the current ramp EST_setMaxCurrentSlope_pu(obj->estHandle,gMaxCurrentSlope); gMotorVars.Flag_MotorIdentified = true; // set the speed reference CTRL_setSpd_ref_krpm(ctrlHandle,gMotorVars.SpeedRef_krpm); // set the speed acceleration CTRL_setMaxAccel_pu(ctrlHandle,_IQmpy(MAX_ACCEL_KRPMPS_SF,gMotorVars.MaxAccel_krpmps)); if(Flag_Latch_softwareUpdate) { Flag_Latch_softwareUpdate = false; USER_calcPIgains(ctrlHandle); // initialize the watch window kp and ki current values with pre-calculated values gMotorVars.Kp_Idq = CTRL_getKp(ctrlHandle,CTRL_Type_PID_Id); gMotorVars.Ki_Idq = CTRL_getKi(ctrlHandle,CTRL_Type_PID_Id); // initialize the watch window kp and ki values with pre-calculated values gMotorVars.Kp_spd = CTRL_getKp(ctrlHandle,CTRL_Type_PID_spd); gMotorVars.Ki_spd = CTRL_getKi(ctrlHandle,CTRL_Type_PID_spd); } } else { Flag_Latch_softwareUpdate = true; // the estimator sets the maximum current slope during identification gMaxCurrentSlope = EST_getMaxCurrentSlope_pu(obj->estHandle); } // when appropriate, update the global variables if(gCounter_updateGlobals >= NUM_MAIN_TICKS_FOR_GLOBAL_VARIABLE_UPDATE) { // reset the counter gCounter_updateGlobals = 0; updateGlobalVariables_motor(ctrlHandle); } // update Kp and Ki gains updateKpKiGains(ctrlHandle); // enable/disable the forced angle EST_setFlag_enableForceAngle(obj->estHandle,gMotorVars.Flag_enableForceAngle); // enable or disable power warp CTRL_setFlag_enablePowerWarp(ctrlHandle,gMotorVars.Flag_enablePowerWarp); #ifdef DRV8301_SPI HAL_writeDrvData(halHandle,&gDrvSpi8301Vars); HAL_readDrvData(halHandle,&gDrvSpi8301Vars); #endif #ifdef DRV8305_SPI HAL_writeDrvData(halHandle,&gDrvSpi8305Vars); HAL_readDrvData(halHandle,&gDrvSpi8305Vars); #endif } // end of while(gFlag_enableSys) loop // disable the PWM HAL_disablePwm(halHandle); // set the default controller parameters (Reset the control to re-identify the motor) CTRL_setParams(ctrlHandle,&gUserParams); gMotorVars.Flag_Run_Identify = false; } // end of for(;;) loop } // end of main() function interrupt void mainISR(void) { // toggle status LED if(gLEDcnt++ > (uint_least32_t)(USER_ISR_FREQ_Hz / LED_BLINK_FREQ_Hz)) { HAL_toggleLed(halHandle,(GPIO_Number_e)HAL_Gpio_LED2); gLEDcnt = 0; } // acknowledge the ADC interrupt HAL_acqAdcInt(halHandle,ADC_IntNumber_1); // convert the ADC data HAL_readAdcData(halHandle,&gAdcData); // run the controller CTRL_run(ctrlHandle,halHandle,&gAdcData,&gPwmData); // write the PWM compare values HAL_writePwmData(halHandle,&gPwmData); // setup the controller CTRL_setup(ctrlHandle); return; } // end of mainISR() function void updateGlobalVariables_motor(CTRL_Handle handle) { CTRL_Obj *obj = (CTRL_Obj *)handle; // get the speed estimate gMotorVars.Speed_krpm = EST_getSpeed_krpm(obj->estHandle); // get the real time speed reference coming out of the speed trajectory generator gMotorVars.SpeedTraj_krpm = _IQmpy(CTRL_getSpd_int_ref_pu(handle),EST_get_pu_to_krpm_sf(obj->estHandle)); // get the torque estimate gMotorVars.Torque_Nm = USER_computeTorque_Nm(handle, gTorque_Flux_Iq_pu_to_Nm_sf, gTorque_Ls_Id_Iq_pu_to_Nm_sf); // get the magnetizing current gMotorVars.MagnCurr_A = EST_getIdRated(obj->estHandle); // get the rotor resistance gMotorVars.Rr_Ohm = EST_getRr_Ohm(obj->estHandle); // get the stator resistance gMotorVars.Rs_Ohm = EST_getRs_Ohm(obj->estHandle); // get the stator inductance in the direct coordinate direction gMotorVars.Lsd_H = EST_getLs_d_H(obj->estHandle); // get the stator inductance in the quadrature coordinate direction gMotorVars.Lsq_H = EST_getLs_q_H(obj->estHandle); // get the flux in V/Hz in floating point gMotorVars.Flux_VpHz = EST_getFlux_VpHz(obj->estHandle); // get the flux in Wb in fixed point gMotorVars.Flux_Wb = USER_computeFlux(handle, gFlux_pu_to_Wb_sf); // get the controller state gMotorVars.CtrlState = CTRL_getState(handle); // get the estimator state gMotorVars.EstState = EST_getState(obj->estHandle); // Get the DC buss voltage gMotorVars.VdcBus_kV = _IQmpy(gAdcData.dcBus,_IQ(USER_IQ_FULL_SCALE_VOLTAGE_V/1000.0)); return; } // end of updateGlobalVariables_motor() function void updateKpKiGains(CTRL_Handle handle) { if((gMotorVars.CtrlState == CTRL_State_OnLine) && (gMotorVars.Flag_MotorIdentified == true) && (Flag_Latch_softwareUpdate == false)) { // set the kp and ki speed values from the watch window CTRL_setKp(handle,CTRL_Type_PID_spd,gMotorVars.Kp_spd); CTRL_setKi(handle,CTRL_Type_PID_spd,gMotorVars.Ki_spd); // set the kp and ki current values for Id and Iq from the watch window CTRL_setKp(handle,CTRL_Type_PID_Id,gMotorVars.Kp_Idq); CTRL_setKi(handle,CTRL_Type_PID_Id,gMotorVars.Ki_Idq); CTRL_setKp(handle,CTRL_Type_PID_Iq,gMotorVars.Kp_Idq); CTRL_setKi(handle,CTRL_Type_PID_Iq,gMotorVars.Ki_Idq); } return; } // end of updateKpKiGains() function //@} //defgroup // end of file