//==========================================================================
//					 traction controller test
//					A.Brousalis		Nov 2013
//==========================================================================
//! Based on  PROJ_LAB04A
// **************************************************************************
// 	includes
// **************************************************************************
#include <math.h>
#include "main.h"
// **************************************************************************
//
// **************************************************************************
#define 	TORQUE_MODE
//#define		FULL_MOTOR_ID
#define		PART_MOTOR_ID
//#define		NO_MOTOR_ID



#define LED_BLINK_FREQ_Hz   5
// **************************************************************************
#ifdef FLASH
#pragma CODE_SECTION(mainISR,"ramfuncs");
#endif

// **************************************************************************

// **************************************************************************
static inline bool myDRV_ReadGpio(DRV_Handle handle,const GPIO_Number_e gpioNumber)
{
  DRV_Obj *obj = (DRV_Obj *)handle;

  // set GPIO high
  return( GPIO_read(obj->gpioHandle,gpioNumber));
}

#define 	StartPressed()	(myDRV_ReadGpio(drvHandle,GPIO_Number_9) == 0)
#define 	StopPressed()	(myDRV_ReadGpio(drvHandle,GPIO_Number_7) == 0)

#define 	Led10_ON()		DRV_setGpioHigh(drvHandle,GPIO_Number_12)
#define 	Led10_OFF()		DRV_setGpioLow(drvHandle,GPIO_Number_12)
#define 	Led10_TOG()		DRV_toggleGpio(drvHandle,GPIO_Number_12)

#define 	Led11_ON()		DRV_setGpioHigh(drvHandle,GPIO_Number_15)
#define 	Led11_OFF()		DRV_setGpioLow(drvHandle,GPIO_Number_15)
#define 	Led11_TOG()		DRV_toggleGpio(drvHandle,GPIO_Number_15)

// **************************************************************************
// 		 globals
// **************************************************************************
_iq PotRef_krpm;
_iq TorqueRef;
float vare;

uint_least16_t gCounter_updateGlobals = 0;

bool Flag_Latch_softwareUpdate = true;

CTRL_Handle ctrlHandle;

DRV_Handle drvHandle;

USER_Params gUserParams;

DRV_PwmData_t gPwmData;

DRV_AdcData_t gAdcData;

_iq gMaxCurrentSlope = _IQ(0.0);

#ifdef FAST_ROM_V1p6
CTRL_Obj *controller_obj;
#else
CTRL_Obj ctrl;				//v1p7 format
#endif

ST_Obj st_obj;
ST_Handle stHandle;

uint16_t gLEDcnt = 0;

volatile MOTOR_Vars_t gMotorVars = MOTOR_Vars_INIT;

#ifdef FLASH
// Used for running BackGround in flash, and ISR in RAM
extern uint16_t *RamfuncsLoadStart, *RamfuncsLoadEnd, *RamfuncsRunStart;
#endif


#ifdef DRV8301_SPI
// Watch window interface to the 8301 SPI
DRV_SPI_8301_Vars_t gDrvSpi8301Vars;
#endif


// **************************************************************************
/// the functions
// ************************************************************************** RatedFlux_OL

void main(void)
{
  uint_least8_t estNumber = 0;
  TorqueRef = 0;

#ifdef FAST_ROM_V1p6
  uint_least8_t ctrlNumber = 0;
#endif

  // Only used if running from FLASH
  // Note that the variable FLASH is defined by the project
  #ifdef FLASH
  // Copy time critical code and Flash setup code to RAM
  // The RamfuncsLoadStart, RamfuncsLoadEnd, and RamfuncsRunStart
  // symbols are created by the linker. Refer to the linker files.
  memCopy((uint16_t *)&RamfuncsLoadStart,(uint16_t *)&RamfuncsLoadEnd,(uint16_t *)&RamfuncsRunStart);
  #endif

  // initialize the driver
  drvHandle = DRV_init(&drv,sizeof(drv));


  // initialize the user parameters
  USER_setParams(&gUserParams);


  // set the driver parameters
  DRV_setParams(drvHandle,&gUserParams);


  // initialize the controller
#ifdef FAST_ROM_V1p6
  ctrlHandle = CTRL_initCtrl(ctrlNumber, estNumber);  		//v1p6 format (06xF and 06xM devices)
  controller_obj = (CTRL_Obj *)ctrlHandle;
#else
  ctrlHandle = CTRL_initCtrl(estNumber,&ctrl,sizeof(ctrl));	//v1p7 format default
#endif


  Led11_OFF();

  // set the default controller parameters
  CTRL_setParams(ctrlHandle,&gUserParams);

  // setup faults
  DRV_setupFaults(drvHandle);

  // initialize the interrupt vector table
  DRV_initIntVectorTable(drvHandle);

  // enable the ADC interrupts
  DRV_enableAdcInts(drvHandle);

  // enable global interrupts
  DRV_enableGlobalInts(drvHandle);

  // enable debug interrupts
  DRV_enableDebugInt(drvHandle);

  // disable the PWM
  DRV_disablePwm(drvHandle);

//===========================================================================================
//===========================================================================================
#ifdef DRV8301_SPI
  // turn on the DRV8301 if present
  DRV_enable8301(drvHandle);
  // initialize the DRV8301 interface
  DRV_8301_SpiInterface_init(drvHandle,&gDrvSpi8301Vars);
#endif

  // enable DC bus compensation
  CTRL_setFlag_enableDcBusComp(ctrlHandle, true);

#ifndef TORQUE_MODE
  // initialize the SpinTAC Components
  stHandle = ST_init(&st_obj, sizeof(st_obj));

  // setup the SpinTAC Components
  ST_setupVelCtl(stHandle);
#endif

#ifdef NO_MOTOR_ID

  gMotorVars.Flag_enableOffsetcalc = false;
  gMotorVars.Flag_enableRsRecalc = false;
  gMotorVars.Flag_MotorIdentified = true;

#endif

#ifdef FULL_MOTOR_ID
  gMotorVars.Flag_MotorIdentified = false;
#endif

#ifdef PART_MOTOR_ID
  gMotorVars.Flag_enableOffsetcalc = true;
  gMotorVars.Flag_enableRsRecalc = true;
  gMotorVars.Flag_MotorIdentified = false;
#endif

//  gMotorVars.Flag_enableForceAngle = false;

  for(;;)
  {
	  CTRL_Obj *obj = (CTRL_Obj *)ctrlHandle;
	  ST_Obj *stObj = (ST_Obj *)stHandle;


    // Waiting for enable system flag to be set
	  while(!(gMotorVars.Flag_enableSys))
	      {
	      	if(StartPressed())
	      	{
	      		Led10_ON();
	          	gMotorVars.Flag_enableSys = true;
	          	gMotorVars.Flag_Run_Identify = true;
	          }
	      }
	      
#ifndef FULL_MOTOR_ID
    // Dis-able the Library internal PI.  Iq has no reference now
    //if(gMotorVars.Flag_MotorIdentified	== true)
    // {
    	CTRL_setFlag_enableSpeedCtrl(ctrlHandle, false);
    //}
#endif

    // loop while the enable system flag is true
    while(gMotorVars.Flag_enableSys)
      {
      	
      	// increment counters
      	gCounter_updateGlobals++;
      	
      
#ifdef PART_MOTOR_ID
        CTRL_setFlag_enableUserMotorParams(ctrlHandle,true ) ;										// Use user.h parameters
#endif

#ifdef NO_MOTOR_ID
        CTRL_setFlag_enableUserMotorParams(ctrlHandle,true ) ;										// Use user.h parameters
#endif

      
        if(CTRL_isError(ctrlHandle))
          {
            // set the enable controller flag to false
            CTRL_setFlag_enableCtrl(ctrlHandle,false);

            // set the enable system flag to false
            gMotorVars.Flag_enableSys = false;

            // disable the PWM
            DRV_disablePwm(drvHandle);
          }
        else
          {
            // update the controller state
            bool flag_ctrlStateChanged = CTRL_updateState(ctrlHandle);

            // enable or disable the control
            CTRL_setFlag_enableCtrl(ctrlHandle, gMotorVars.Flag_Run_Identify);

            if(flag_ctrlStateChanged)
              {
                CTRL_State_e ctrlState = CTRL_getState(ctrlHandle);

                if(ctrlState == CTRL_State_OffLine)
                  {
                    // enable the PWM
                    DRV_enablePwm(drvHandle);
                  }
                else if(ctrlState == CTRL_State_OnLine)
                  {
                	Led11_ON();
                    if(gMotorVars.Flag_enableOffsetcalc == true)
                    {
                      // update the ADC bias values
                      DRV_updateAdcBias(drvHandle);
                    }
                    else
                    {
                      // set the current bias
                      DRV_setBias(drvHandle,DRV_SensorType_Current,0,_IQ(I_A_offset));
                      DRV_setBias(drvHandle,DRV_SensorType_Current,1,_IQ(I_B_offset));
                      DRV_setBias(drvHandle,DRV_SensorType_Current,2,_IQ(I_C_offset));

                      // set the voltage bias
                      DRV_setBias(drvHandle,DRV_SensorType_Voltage,0,_IQ(V_A_offset));
                      DRV_setBias(drvHandle,DRV_SensorType_Voltage,1,_IQ(V_B_offset));
                      DRV_setBias(drvHandle,DRV_SensorType_Voltage,2,_IQ(V_C_offset));
                    }

                    // enable the PWM
                    DRV_enablePwm(drvHandle);
                  }
                else if(ctrlState == CTRL_State_Idle)
                  {
                  	Led11_OFF();
                    // disable the PWM
                    DRV_disablePwm(drvHandle);
                    gMotorVars.Flag_Run_Identify = false;
                  }
              }
          }


        if(EST_isMotorIdentified(obj->estHandle))
          {
            // set the current ramp
            EST_setMaxCurrentSlope_pu(obj->estHandle,gMaxCurrentSlope);
            gMotorVars.Flag_MotorIdentified = true;

#ifndef TORQUE_MODE
            // set the speed reference
        	vare = (float) ( (float)((float)PotRef_krpm / 4096) * USER_MOTOR_MAX_SPEED_KRPM);
            gMotorVars.SpeedRef_krpm = _IQ(vare);

            CTRL_setSpd_ref_krpm(ctrlHandle,gMotorVars.SpeedRef_krpm);

            gMotorVars.MaxAccel_krpmps = _IQ(2.0);

            // set the speed acceleration
            CTRL_setMaxAccel_pu(ctrlHandle,_IQmpy(MAX_ACCEL_KRPMPS_SF,gMotorVars.MaxAccel_krpmps));

            // enable the SpinTAC Speed Controller
            STVELCTL_setEnable(stObj->velCtlHandle, true);

            if(EST_getState(obj->estHandle) != EST_State_OnLine)
            {
            	// if the estimator is not running, place SpinTAC into reset
            	STVELCTL_setEnable(stObj->velCtlHandle, false);
            }
#endif


#ifdef TORQUE_MODE
            vare = (float) ( (float)((float)PotRef_krpm / 4096));
            vare *= USER_MOTOR_MAX_CURRENT;
            gMotorVars.IqRef_A = _IQ(vare);
#endif

            if(Flag_Latch_softwareUpdate)
            {
              Flag_Latch_softwareUpdate = false;

#ifdef FAST_ROM_V1p6
              if(CTRL_getFlag_enableUserMotorParams(ctrlHandle) == true)
              {
                  // call this function to fix 1p6
                  softwareUpdate1p6(ctrlHandle);
              }
#endif

              calcPIgains(ctrlHandle);
            }

          }
        else
          {
            Flag_Latch_softwareUpdate = true;

            // the estimator sets the maximum current slope during identification
            gMaxCurrentSlope = EST_getMaxCurrentSlope_pu(obj->estHandle);
          }


        // when appropriate, update the global variables
        if(gCounter_updateGlobals >= NUM_MAIN_TICKS_FOR_GLOBAL_VARIABLE_UPDATE)
          {
            // reset the counter
            gCounter_updateGlobals = 0;

            updateGlobalVariables_motor(ctrlHandle);
          }

      } // end of while(gFlag_enableSys) loop


    // disable the PWM
    DRV_disablePwm(drvHandle);

    // set the default controller parameters (Reset the control to re-identify the motor)
    CTRL_setParams(ctrlHandle,&gUserParams);
  //gMotorVars.Flag_Run_Identify = false;
#ifndef TORQUE_MODE
    // setup the SpinTAC Components
    ST_setupVelCtl(stHandle);
#endif
  } // end of for(;;) loop

} // end of main() function
//===================================================================================
//					RT service routine
//===================================================================================
interrupt void mainISR(void)
{

	static uint16_t stCnt = 0;

  // toggle status LED
  if(gLEDcnt++ > (uint_least32_t)(USER_PWM_FREQ_kHz * 1000 / LED_BLINK_FREQ_Hz)){
    DRV_toggleLed(drvHandle,(GPIO_Number_e)DRV_Gpio_LED2);
    gLEDcnt = 0;

  }

  if(StopPressed())
  {
	  Led10_OFF();
	  Led11_OFF();
      gMotorVars.Flag_enableSys = false;
  }

  // acknowledge the ADC interrupt
  DRV_acqAdcInt(drvHandle,ADC_IntNumber_1);


  // convert the ADC data
  DRV_readAdcData(drvHandle,&gAdcData);


#ifndef   	TORQUE_MODE

  // Run the SpinTAC Components
   if(stCnt++ >= ISR_TICKS_PER_SPINTAC_TICK) {
 	  ST_runVelCtl(stHandle, ctrlHandle);
 	  stCnt = 1;
   }

#endif


  // run the controller
  CTRL_run(ctrlHandle,drvHandle,&gAdcData,&gPwmData);


  // write the PWM compare values
  DRV_writePwmData(drvHandle,&gPwmData);


  // setup the controller
  CTRL_setup(ctrlHandle);


  return;
} // end of mainISR() function


void updateGlobalVariables_motor(CTRL_Handle handle)
{
  CTRL_Obj *obj = (CTRL_Obj *)handle;
  //**************************************************
  union
  {
    int32_t   long_value;
    float_t float_value;
  } interface;


#ifdef TORQUE_MODE
 
  _iq iq_ref = _IQmpy(gMotorVars.IqRef_A,_IQ(1.0/USER_MOTOR_MAX_CURRENT));

  // get the speed estimate
  gMotorVars.Speed_krpm = EST_getSpeed_krpm(obj->estHandle);


  // set the speed reference so that the forced angle rotates in the correct direction
  // for startup.
  if(_IQabs(gMotorVars.Speed_krpm) < _IQ(0.01))
  {
      if(iq_ref < 0)
          CTRL_setSpd_ref_krpm(handle,_IQ(-0.01));
      else if(iq_ref > 0)
          CTRL_setSpd_ref_krpm(handle,_IQ(0.01));
  }

  // Set the Iq reference that use to come out of the PI speed control
   TorqueRef = iq_ref;
   CTRL_setIq_ref_pu(handle, iq_ref);

#endif

  // get the speed estimate
  gMotorVars.Speed_krpm = EST_getSpeed_krpm(obj->estHandle);

  // get the torque estimate
  gMotorVars.Torque_lbin = EST_getTorque_lbin(obj->estHandle);

  // get the magnetizing current
  interface.long_value = EST_getIdRated(obj->estHandle);
  gMotorVars.MagnCurr_A = interface.float_value;

  // get the rotor resistance
  interface.long_value = EST_getRr_Ohm(obj->estHandle);
  gMotorVars.Rr_Ohm = interface.float_value;

  // get the stator resistance
  interface.long_value = EST_getRs_Ohm(obj->estHandle);
  gMotorVars.Rs_Ohm = interface.float_value;

  // get the stator inductance in the direct coordinate direction
  interface.long_value = EST_getLs_d_H(obj->estHandle);
  gMotorVars.Lsd_H = interface.float_value;

  // get the stator inductance in the quadrature coordinate direction
  interface.long_value = EST_getLs_q_H(obj->estHandle);
  gMotorVars.Lsq_H = interface.float_value;

  // get the flux
  interface.long_value = EST_getFlux_VpHz(obj->estHandle);
  gMotorVars.Flux_VpHz = interface.float_value;

  // get the controller state
  gMotorVars.CtrlState = CTRL_getState(handle);

  // get the estimator state
  gMotorVars.EstState = EST_getState(obj->estHandle);

  // enable/disable the forced angle
  EST_setFlag_enableForceAngle(obj->estHandle,gMotorVars.Flag_enableForceAngle);
  
  // enable or disable power warp
  CTRL_setFlag_enableEpl(handle,gMotorVars.Flag_enableEpl);

  // Get the DC buss voltage
  gMotorVars.VdcBus_kV = _IQmpy(gAdcData.dcBus,_IQ(USER_IQ_FULL_SCALE_VOLTAGE_V/1000.0));

#ifdef DRV8301_SPI
  DRV_8301_SpiInterface(drvHandle,&gDrvSpi8301Vars);
#endif

  return;
} // end of updateGlobalVariables_motor() function
//===========================================================================================
//
//===========================================================================================

#ifdef FAST_ROM_V1p6
void softwareUpdate1p6(CTRL_Handle handle)
{

  CTRL_Obj *obj = (CTRL_Obj *)handle;

  float_t fullScaleInductance = USER_IQ_FULL_SCALE_VOLTAGE_V/(USER_IQ_FULL_SCALE_CURRENT_A*USER_VOLTAGE_FILTER_POLE_rps);
  float_t Ls_coarse_max = _IQ30toF(EST_getLs_coarse_max_pu(obj->estHandle));
  int_least8_t lShift = ceil(log(obj->motorParams.Ls_d/(Ls_coarse_max*fullScaleInductance))/log(2.0));
  uint_least8_t Ls_qFmt = 30 - lShift;
  float_t L_max = fullScaleInductance * pow(2.0,lShift);
  _iq Ls_d_pu = _IQ30(obj->motorParams.Ls_d / L_max);
  _iq Ls_q_pu = _IQ30(obj->motorParams.Ls_q / L_max);


  // store the results
  EST_setLs_d_pu(obj->estHandle,Ls_d_pu);
  EST_setLs_q_pu(obj->estHandle,Ls_q_pu);
  EST_setLs_qFmt(obj->estHandle,Ls_qFmt);

  return;
} // end of softwareUpdate1p6() function
#endif

//===========================================================================================
//
//===========================================================================================
void calcPIgains(CTRL_Handle handle)
{
  CTRL_Obj *obj = (CTRL_Obj *)handle;
  float_t fullScaleCurrent = USER_IQ_FULL_SCALE_CURRENT_A;
  float_t fullScaleVoltage = USER_IQ_FULL_SCALE_VOLTAGE_V;
  float_t ctrlPeriod_sec = CTRL_getCtrlPeriod_sec(handle);
  float_t Ls_d;
  float_t Ls_q;
  float_t Rs;
  float_t RoverLs_d;
  float_t RoverLs_q;
  _iq Kp_Id;
  _iq Ki_Id;
  _iq Kp_Iq;
  _iq Ki_Iq;
  _iq Kd;
  union
  {
    int32_t   long_value;
    float_t float_value;
  } interface;

  interface.long_value = EST_getLs_d_H(obj->estHandle);
  Ls_d = interface.float_value;

  interface.long_value = EST_getLs_q_H(obj->estHandle);
  Ls_q = interface.float_value;

  interface.long_value = EST_getRs_Ohm(obj->estHandle);
  Rs = interface.float_value;

  RoverLs_d = Rs/Ls_d;
  Kp_Id = _IQ(Kp_Scale * (0.25*Ls_d*fullScaleCurrent)/(ctrlPeriod_sec*fullScaleVoltage));
  Ki_Id = _IQ(RoverLs_d*ctrlPeriod_sec);

  RoverLs_q = Rs/Ls_q;
  Kp_Iq = _IQ(Kp_Scale * (0.25*Ls_q*fullScaleCurrent)/(ctrlPeriod_sec*fullScaleVoltage));
  Ki_Iq = _IQ(RoverLs_q*ctrlPeriod_sec);

  Kd = _IQ(0.0);

  // set the Id controller gains
  PID_setKi(obj->pidHandle_Id,Ki_Id);
  CTRL_setGains(handle,CTRL_Type_PID_Id,Kp_Id,Ki_Id,Kd);

  // set the Iq controller gains
  PID_setKi(obj->pidHandle_Iq,Ki_Iq);
  CTRL_setGains(handle,CTRL_Type_PID_Iq,Kp_Iq,Ki_Iq,Kd);

  return;
} // end of calcPIgains() function
//@} //defgroup
// end of file
//===========================================================================================
//
//===========================================================================================

void ST_runVelCtl(ST_Handle sthandle, CTRL_Handle handle)
{

    _iq speedFeedback, iqReference;
    ST_Obj *stObj = (ST_Obj *)sthandle;
    CTRL_Obj *ctrlObj = (CTRL_Obj *)handle;

    // Get the mechanical speed in pu
    speedFeedback = EST_getFm_pu(ctrlObj->estHandle);

	// Run the SpinTAC Controller
	// Note that the library internal ramp generator is used to set the speed reference
    STVELCTL_setVelocityReference(stObj->velCtlHandle, TRAJ_getIntValue(ctrlObj->trajHandle_spd));
	STVELCTL_setAccelerationReference(stObj->velCtlHandle, _IQ(0.0));	// Internal ramp generator does not provide Acceleration Reference
	STVELCTL_setVelocityFeedback(stObj->velCtlHandle, speedFeedback);
	STVELCTL_run(stObj->velCtlHandle);

	// select SpinTAC Velocity Controller
	iqReference = STVELCTL_getTorqueReference(stObj->velCtlHandle);

	// Set the Iq reference that came out of SpinTAC Velocity Control
	TorqueRef = iqReference;																	// just for external monitoring
	CTRL_setIq_ref_pu(ctrlHandle, iqReference);
}
//@} //defgroup
// end of file