//***************************************************************************** // // startup_ccs.c - Startup code for use with TI's Code Composer Studio. // // Copyright (c) 2013 Texas Instruments Incorporated. All rights reserved. // Software License Agreement // // Texas Instruments (TI) is supplying this software for use solely and // exclusively on TI's microcontroller products. The software is owned by // TI and/or its suppliers, and is protected under applicable copyright // laws. You may not combine this software with "viral" open-source // software in order to form a larger program. // // THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS. // NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT // NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR // A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY // CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL // DAMAGES, FOR ANY REASON WHATSOEVER. // // This is part of revision 1.0 of the EK-TM4C123GXL Firmware Package. // //***************************************************************************** #include #include "inc/hw_nvic.h" #include "inc/hw_types.h" //***************************************************************************** // // Forward declaration of the default fault handlers. // //***************************************************************************** void ResetISR(void); static void NmiSR(void); static void FaultISR(void); static void IntDefaultHandler(void); //***************************************************************************** // // External declaration for the reset handler that is to be called when the // processor is started // //***************************************************************************** extern void _c_int00(void); //***************************************************************************** // // Linker variable that marks the top of the stack. // //***************************************************************************** extern uint32_t __STACK_TOP; //***************************************************************************** // // External declarations for the interrupt handlers used by the application. // //***************************************************************************** //extern void IntGPIOe(void); extern void ISL29023I2CIntHandler(void); //extern void SysTickIntHandler(void); //extern void UARTStdioIntHandler(void); //extern void RGBBlinkIntHandler(void); //***************************************************************************** // // The vector table. Note that the proper constructs must be placed on this to // ensure that it ends up at physical address 0x0000.0000 or at the start of // the program if located at a start address other than 0. // //***************************************************************************** #pragma DATA_SECTION(g_pfnVectors, ".intvecs") void (* const g_pfnVectors[])(void) = { (void (*)(void))((uint32_t)&__STACK_TOP), // The initial stack pointer ResetISR, // The reset handler NmiSR, // The NMI handler FaultISR, // The hard fault handler IntDefaultHandler, // The MPU fault handler IntDefaultHandler, // The bus fault handler IntDefaultHandler, // The usage fault handler 0, // Reserved 0, // Reserved 0, // Reserved 0, // Reserved IntDefaultHandler, // SVCall handler IntDefaultHandler, // Debug monitor handler 0, // Reserved IntDefaultHandler, // The PendSV handler IntDefaultHandler, // The SysTick handler IntDefaultHandler, // GPIO Port A IntDefaultHandler, // GPIO Port B IntDefaultHandler, // GPIO Port C IntDefaultHandler, // GPIO Port D IntDefaultHandler, // GPIO Port E IntDefaultHandler, // UART0 Rx and Tx IntDefaultHandler, // UART1 Rx and Tx IntDefaultHandler, // SSI0 Rx and Tx IntDefaultHandler, // I2C0 Master and Slave IntDefaultHandler, // PWM Fault IntDefaultHandler, // PWM Generator 0 IntDefaultHandler, // PWM Generator 1 IntDefaultHandler, // PWM Generator 2 IntDefaultHandler, // Quadrature Encoder 0 IntDefaultHandler, // ADC Sequence 0 IntDefaultHandler, // ADC Sequence 1 IntDefaultHandler, // ADC Sequence 2 IntDefaultHandler, // ADC Sequence 3 IntDefaultHandler, // Watchdog timer IntDefaultHandler, // Timer 0 subtimer A IntDefaultHandler, // Timer 0 subtimer B IntDefaultHandler, // Timer 1 subtimer A IntDefaultHandler, // Timer 1 subtimer B IntDefaultHandler, // Timer 2 subtimer A IntDefaultHandler, // Timer 2 subtimer B IntDefaultHandler, // Analog Comparator 0 IntDefaultHandler, // Analog Comparator 1 IntDefaultHandler, // Analog Comparator 2 IntDefaultHandler, // System Control (PLL, OSC, BO) IntDefaultHandler, // FLASH Control IntDefaultHandler, // GPIO Port F IntDefaultHandler, // GPIO Port G IntDefaultHandler, // GPIO Port H IntDefaultHandler, // UART2 Rx and Tx IntDefaultHandler, // SSI1 Rx and Tx IntDefaultHandler, // Timer 3 subtimer A IntDefaultHandler, // Timer 3 subtimer B IntDefaultHandler, // I2C1 Master and Slave IntDefaultHandler, // Quadrature Encoder 1 IntDefaultHandler, // CAN0 IntDefaultHandler, // CAN1 IntDefaultHandler, // CAN2 0, // Reserved IntDefaultHandler, // Hibernate IntDefaultHandler, // USB0 IntDefaultHandler, // PWM Generator 3 IntDefaultHandler, // uDMA Software Transfer IntDefaultHandler, // uDMA Error IntDefaultHandler, // ADC1 Sequence 0 IntDefaultHandler, // ADC1 Sequence 1 IntDefaultHandler, // ADC1 Sequence 2 IntDefaultHandler, // ADC1 Sequence 3 0, // Reserved 0, // Reserved IntDefaultHandler, // GPIO Port J IntDefaultHandler, // GPIO Port K IntDefaultHandler, // GPIO Port L IntDefaultHandler, // SSI2 Rx and Tx IntDefaultHandler, // SSI3 Rx and Tx IntDefaultHandler, // UART3 Rx and Tx IntDefaultHandler, // UART4 Rx and Tx IntDefaultHandler, // UART5 Rx and Tx IntDefaultHandler, // UART6 Rx and Tx IntDefaultHandler, // UART7 Rx and Tx 0, // Reserved 0, // Reserved 0, // Reserved 0, // Reserved IntDefaultHandler, // I2C2 Master and Slave ISL29023I2CIntHandler, // I2C3 Master and Slave IntDefaultHandler, // Timer 4 subtimer A IntDefaultHandler, // Timer 4 subtimer B 0, // Reserved 0, // Reserved 0, // Reserved 0, // Reserved 0, // Reserved 0, // Reserved 0, // Reserved 0, // Reserved 0, // Reserved 0, // Reserved 0, // Reserved 0, // Reserved 0, // Reserved 0, // Reserved 0, // Reserved 0, // Reserved 0, // Reserved 0, // Reserved 0, // Reserved 0, // Reserved IntDefaultHandler, // Timer 5 subtimer A IntDefaultHandler, // Timer 5 subtimer B IntDefaultHandler, // Wide Timer 0 subtimer A IntDefaultHandler, // Wide Timer 0 subtimer B IntDefaultHandler, // Wide Timer 1 subtimer A IntDefaultHandler, // Wide Timer 1 subtimer B IntDefaultHandler, // Wide Timer 2 subtimer A IntDefaultHandler, // Wide Timer 2 subtimer B IntDefaultHandler, // Wide Timer 3 subtimer A IntDefaultHandler, // Wide Timer 3 subtimer B IntDefaultHandler, // Wide Timer 4 subtimer A IntDefaultHandler, // Wide Timer 4 subtimer B IntDefaultHandler, // Wide Timer 5 subtimer A IntDefaultHandler, // Wide Timer 5 subtimer B IntDefaultHandler, // FPU 0, // Reserved 0, // Reserved IntDefaultHandler, // I2C4 Master and Slave IntDefaultHandler, // I2C5 Master and Slave IntDefaultHandler, // GPIO Port M IntDefaultHandler, // GPIO Port N IntDefaultHandler, // Quadrature Encoder 2 0, // Reserved 0, // Reserved IntDefaultHandler, // GPIO Port P (Summary or P0) IntDefaultHandler, // GPIO Port P1 IntDefaultHandler, // GPIO Port P2 IntDefaultHandler, // GPIO Port P3 IntDefaultHandler, // GPIO Port P4 IntDefaultHandler, // GPIO Port P5 IntDefaultHandler, // GPIO Port P6 IntDefaultHandler, // GPIO Port P7 IntDefaultHandler, // GPIO Port Q (Summary or Q0) IntDefaultHandler, // GPIO Port Q1 IntDefaultHandler, // GPIO Port Q2 IntDefaultHandler, // GPIO Port Q3 IntDefaultHandler, // GPIO Port Q4 IntDefaultHandler, // GPIO Port Q5 IntDefaultHandler, // GPIO Port Q6 IntDefaultHandler, // GPIO Port Q7 IntDefaultHandler, // GPIO Port R IntDefaultHandler, // GPIO Port S IntDefaultHandler, // PWM 1 Generator 0 IntDefaultHandler, // PWM 1 Generator 1 IntDefaultHandler, // PWM 1 Generator 2 IntDefaultHandler, // PWM 1 Generator 3 IntDefaultHandler // PWM 1 Fault }; //***************************************************************************** // // This is the code that gets called when the processor first starts execution // following a reset event. Only the absolutely necessary set is performed, // after which the application supplied entry() routine is called. Any fancy // actions (such as making decisions based on the reset cause register, and // resetting the bits in that register) are left solely in the hands of the // application. // //***************************************************************************** void ResetISR(void) { // // Jump to the CCS C initialization routine. This will enable the // floating-point unit as well, so that does not need to be done here. // __asm(" .global _c_int00\n" " b.w _c_int00"); } //***************************************************************************** // // This is the code that gets called when the processor receives a NMI. This // simply enters an infinite loop, preserving the system state for examination // by a debugger. // //***************************************************************************** static void NmiSR(void) { // // Enter an infinite loop. // while(1) { } } //***************************************************************************** // // This is the code that gets called when the processor receives a fault // interrupt. This simply enters an infinite loop, preserving the system state // for examination by a debugger. // //***************************************************************************** static void FaultISR(void) { // // Enter an infinite loop. // while(1) { } } //***************************************************************************** // // This is the code that gets called when the processor receives an unexpected // interrupt. This simply enters an infinite loop, preserving the system state // for examination by a debugger. // //***************************************************************************** static void IntDefaultHandler(void) { // // Go into an infinite loop. // while(1) { } }