//***************************************************************************** #include #include #include "inc/hw_memmap.h" #include "driverlib/gpio.h" #include "driverlib/pin_map.h" #include "driverlib/ssi.h" #include "driverlib/sysctl.h" #include "driverlib/uart.h" #include "utils/uartstdio.h" //***************************************************************************** // Number of bytes to send and receive. // #define NUM_SSI_DATA 3 //***************************************************************************** // This function sets up UART0 to be used for a console to display conversion // void InitConsole(void) { // Enable GPIO port A which is used for UART0 pins. SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA); // // Configure the pin muxing for UART0 functions on port A0 and A1. GPIOPinConfigure(GPIO_PA0_U0RX); GPIOPinConfigure(GPIO_PA1_U0TX); // // Enable UART0 so that we can configure the clock. SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0); // Use the internal 16MHz oscillator as the UART clock source. // UARTClockSourceSet(UART0_BASE, UART_CLOCK_PIOSC); // Select the alternate (UART) function for these pins. GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1); // Initialize the UART for console I/O. UARTStdioConfig(0, 115200, 16000000); } //***************************************************************************** // // Configure SSI0 in master Freescale (SPI) mode. This example will send out // 3 bytes of data, then wait for 3 bytes of data to come in. This will all be // done using the polling method. // //***************************************************************************** int main(void) { uint32_t pui32DataTx[NUM_SSI_DATA]; uint32_t pui32DataRx[NUM_SSI_DATA]; uint32_t ui32Index; double lettura = 0; // // Set the clocking to run directly from the external crystal/oscillator. SysCtlClockSet(SYSCTL_SYSDIV_2 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ); // // Set up the serial console to use for displaying messages. This is // just for this example program and is not needed for SSI operation. // InitConsole(); // // Display the setup on the console. // UARTprintf("SSI ->\n"); UARTprintf(" Mode: SPI\n"); UARTprintf(" Data: 8-bit\n\n"); // // The SSI0 peripheral must be enabled for use. // SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI0); // // For this example SSI0 is used with PortA[5:2]. The actual port and pins // used may be different on your part, consult the data sheet for more // information. GPIO port A needs to be enabled so these pins can be used. // TODO: change this to whichever GPIO port you are using. // SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA); // // Configure the pin muxing for SSI0 functions on port A2, A3, A4, and A5. // This step is not necessary if your part does not support pin muxing. // TODO: change this to select the port/pin you are using. // GPIOPinConfigure(GPIO_PA2_SSI0CLK); GPIOPinConfigure(GPIO_PA3_SSI0FSS); GPIOPinConfigure(GPIO_PA4_SSI0RX); GPIOPinConfigure(GPIO_PA5_SSI0TX); // // Configure the GPIO settings for the SSI pins. This function also gives // control of these pins to the SSI hardware. Consult the data sheet to // see which functions are allocated per pin. // The pins are assigned as follows: // PA5 - SSI0Tx // PA4 - SSI0Rx // PA3 - SSI0Fss // PA2 - SSI0CLK // TODO: change this to select the port/pin you are using. // GPIOPinTypeSSI(GPIO_PORTA_BASE, GPIO_PIN_5 | GPIO_PIN_4 | GPIO_PIN_3 | GPIO_PIN_2); // // Configure and enable the SSI port for SPI master mode. Use SSI0, // system clock supply, idle clock level low and active low clock in // freescale SPI mode, master mode, 1MHz SSI frequency, and 8-bit data. // For SPI mode, you can set the polarity of the SSI clock when the SSI // unit is idle. You can also configure what clock edge you want to // capture data on. Please reference the datasheet for more information on // the different SPI modes. // SSIConfigSetExpClk(SSI0_BASE, SysCtlClockGet(), SSI_FRF_MOTO_MODE_1, SSI_MODE_MASTER, 5000000, 8); // // Enable the SSI0 module. // SSIEnable(SSI0_BASE); // Read any residual data from the SSI port. This makes sure the receive // FIFOs are empty, so we don't read any unwanted junk. This is done here // because the SPI SSI mode is full-duplex, which allows you to send and // receive at the same time. The SSIDataGetNonBlocking function returns // "true" when data was returned, and "false" when no data was returned. // The "non-blocking" function checks if there is any data in the receive // FIFO and does not "hang" if there isn't. // while (1) { while(SSIDataGetNonBlocking(SSI0_BASE, &pui32DataRx[0])) { } // Initialize the data to send. // pui32DataTx[0] = 0; pui32DataTx[1] = 0; pui32DataTx[2] = 0; // Display indication that the SSI is transmitting data. // UARTprintf("Sent:\n "); // // Send 3 bytes of data. // for(ui32Index = 0; ui32Index < NUM_SSI_DATA; ui32Index++) { // // Display the data that SSI is transferring. // UARTprintf("'%c' ", pui32DataTx[ui32Index]); // // Send the data using the "blocking" put function. This function // will wait until there is room in the send FIFO before returning. // This allows you to assure that all the data you send makes it into // the send FIFO. // SSIDataPut(SSI0_BASE, pui32DataTx[ui32Index]); } // // Wait until SSI0 is done transferring all the data in the transmit FIFO. // while(SSIBusy(SSI0_BASE)) { } // // Display indication that the SSI is receiving data. // UARTprintf("\nReceived:\n "); // // Receive 3 bytes of data. // for(ui32Index = 0; ui32Index < NUM_SSI_DATA; ui32Index++) { // // Receive the data using the "blocking" Get function. This function // will wait until there is data in the receive FIFO before returning. // if (ui32Index == 0) { SSIDataGet(SSI0_BASE, &pui32DataRx[0]); // Since we are using 8-bit data, mask off the MSB. // pui32DataRx[0] &= 0x00FF; } else if (ui32Index == 1) { SSIDataGet(SSI0_BASE, &pui32DataRx[1]); pui32DataRx[1] &= 0x00FF; } else { SSIDataGet(SSI0_BASE, &pui32DataRx[2]); pui32DataRx[2] &= 0x00FF; } // // Display the data that SSI0 received. // //UARTprintf("'%x'\n", (pui32DataRx[2] | (pui32DataRx[1] << 8)|(pui32DataRx[0]<<16))); } uint32_t a = (pui32DataRx[2] | (pui32DataRx[1] << 8) | (pui32DataRx[0] << 16)); lettura = a * 0.0000001788; UARTprintf("'%c'\n", lettura); // // Return no errors // //return(0); } }