//***************************************************************************** // // multi_rx.c - Peripheral example demonstrating multiple CAN message // reception. // // Copyright (c) 2010-2015 Texas Instruments Incorporated. All rights reserved. // Software License Agreement // // Redistribution and use in source and binary forms, with or without // modification, are permitted provided that the following conditions // are met: // // Redistributions of source code must retain the above copyright // notice, this list of conditions and the following disclaimer. // // Redistributions in binary form must reproduce the above copyright // notice, this list of conditions and the following disclaimer in the // documentation and/or other materials provided with the // distribution. // // Neither the name of Texas Instruments Incorporated nor the names of // its contributors may be used to endorse or promote products derived // from this software without specific prior written permission. // // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. // // This is part of revision 2.1.1.71 of the Tiva Firmware Development Package. // //***************************************************************************** #include #include #include "inc/hw_can.h" #include "inc/hw_memmap.h" #include "inc/hw_ints.h" #include "driverlib/can.h" #include "driverlib/gpio.h" #include "driverlib/interrupt.h" #include "driverlib/pin_map.h" #include "driverlib/sysctl.h" #include "driverlib/uart.h" #include "utils/uartstdio.h" //***************************************************************************** // //! \addtogroup can_examples_list //!

Multiple CAN RX (multi_rx)

//! //! This example shows how to set up the CAN to receive multiple CAN messages //! using separate message objects for different messages, and using CAN ID //! filtering to control which messages are received. Three message objects //! are set up to receive 3 of the 4 CAN message IDs that are used by the //! multi_tx example. Filtering is used to demonstrate how to receive only //! specific messages, and therefore not receiving all 4 messages from the //! multi_tx example. As messages are received the content of each are printed //! to the serial console. //! //! This example uses the following peripherals and I/O signals. You must //! review these and change as needed for your own board: //! - CAN0 peripheral //! - GPIO port B peripheral (for CAN0 pins) //! - CAN0RX - PB4 //! - CAN0TX - PB5 //! //! The following UART signals are configured only for displaying console //! messages for this example. These are not required for operation of CAN. //! - GPIO port A peripheral (for UART0 pins) //! - UART0RX - PA0 //! - UART0TX - PA1 //! //! This example uses the following interrupt handlers. To use this example //! in your own application you must add these interrupt handlers to your //! vector table. //! - INT_CAN0 - CANIntHandler // //***************************************************************************** //***************************************************************************** // // A counter that keeps track of the number of times the RX interrupt has // occurred, which should match the number of messages that were received. // //***************************************************************************** volatile uint32_t g_ui32MsgCount = 0; unsigned int X[30]; unsigned int uIdx; /*extern void gettingmsg(tCANMsgObject *psCANMsg, uint32_t ui32MsgObj);*/ //***************************************************************************** // // A flag for the interrupt handler to indicate that a message was received. // //***************************************************************************** volatile bool g_bRXFlag1 = 0; //***************************************************************************** // // A flag to indicate that some reception error occurred. // //***************************************************************************** volatile bool g_bErrFlag = 0; //***************************************************************************** // // This function sets up UART0 to be used for a console to display information // as the example is running. tCANMsgObject g_SCANMsgObject2; uint8_t g_pui8Msg[8]={ 03,51, 01, 00, 00, 00, 00, 00}; // //***************************************************************************** void InitConsole(void) { // // Enable GPIO port A which is used for UART0 pins. // TODO: change this to whichever GPIO port you are using. // SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA); // // Configure the pin muxing for UART0 functions on port A0 and A1. // This step is not necessary if your part does not support pin muxing. // TODO: change this to select the port/pin you are using. // GPIOPinConfigure(GPIO_PA0_U0RX); GPIOPinConfigure(GPIO_PA1_U0TX); // // Enable UART0 so that we can configure the clock. // SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0); // // Use the internal 16MHz oscillator as the UART clock source. // UARTClockSourceSet(UART0_BASE, UART_CLOCK_PIOSC); // // Select the alternate (UART) function for these pins. // TODO: change this to select the port/pin you are using. // GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1); // // Initialize the UART for console I/O. // UARTStdioConfig(0, 115200, 16000000); } //***************************************************************************** // // This function prints some information about the CAN message to the // serial port for information purposes only. // //***************************************************************************** void PrintCANMessageInfo(tCANMsgObject *psCANMsg, uint32_t ui32MsgObj) { // // Check to see if there is an indication that some messages were // lost. // if(psCANMsg->ui32Flags & MSG_OBJ_DATA_LOST) { UARTprintf("CAN message loss detected on message object %d\n", ui32MsgObj); } // // Print out the contents of the message that was received. // UARTprintf("Msg Obj=%u ID=0x%05X len=%u data=0x", ui32MsgObj, psCANMsg->ui32MsgID, psCANMsg->ui32MsgLen); for(uIdx = 0; uIdx < psCANMsg->ui32MsgLen; uIdx++) { UARTprintf("%02X ", psCANMsg->pui8MsgData[uIdx]); } UARTprintf("\n"); } void PrintCANMessageInfo1(tCANMsgObject *psCANMsg, uint32_t ui32MsgObj) { UARTprintf("sending msg: Obj=%d ID=0x%05X data=0x", ui32MsgObj, psCANMsg->ui32MsgID); for(uIdx = 0; uIdx < psCANMsg->ui32MsgLen; uIdx++) { UARTprintf("%02X ", psCANMsg->pui8MsgData[uIdx]); } UARTprintf("\n"); } void gettingmsg(tCANMsgObject *psCANMsg, uint32_t ui32MsgObj) { for(uIdx =0; uIdx < psCANMsg->ui32MsgLen; uIdx++) { X[uIdx]=psCANMsg->pui8MsgData[uIdx]; if(X[uIdx]==11) { // initializing msg object 2 for transmission// // data to be transmitted // g_SCANMsgObject2.ui32MsgID = 0x2001; g_SCANMsgObject2.ui32MsgIDMask =0xff; g_SCANMsgObject2.ui32Flags = MSG_OBJ_TX_INT_ENABLE; g_SCANMsgObject2.ui32MsgLen = sizeof(g_pui8Msg); g_SCANMsgObject2.pui8MsgData = g_pui8Msg; CANMessageSet(CAN0_BASE, 2, &g_SCANMsgObject2, MSG_OBJ_TYPE_TX); UARTprintf("%d",X[1]); X[1]=0; UARTprintf("\n"); } } } //***************************************************************************** // // This function is the interrupt handler for the CAN peripheral. It checks // for the cause of the interrupt, and maintains a count of all messages that // have been received. // //***************************************************************************** ; CANIntHandler(void) { uint32_t ui32Status; // // Read the CAN interrupt status to find the cause of the interrupt // ui32Status = CANIntStatus(CAN0_BASE, CAN_INT_STS_CAUSE); // // If the cause is a controller status interrupt, then get the status // if(ui32Status == CAN_INT_INTID_STATUS) { // // Read the controller status. This will return a field of status // error bits that can indicate various errors. Error processing // is not done in this example for simplicity. Refer to the // API documentation for details about the error status bits. // The act of reading this status will clear the interrupt. // ui32Status = CANStatusGet(CAN0_BASE, CAN_STS_CONTROL); // // Set a flag to indicate some errors may have occurred. // g_bErrFlag = 1; } // // Check if the cause is message object 1. // else if(ui32Status == 1) { // // Getting to this point means that the RX interrupt occurred on // message object 1, and the message reception is complete. Clear the // message object interrupt. // CANIntClear(CAN0_BASE, 1); // // Increment a counter to keep track of how many messages have been // received. In a real application this could be used to set flags to // indicate when a message is received. // g_ui32MsgCount++; // // Set flag to indicate received message is pending for this message // object. // g_bRXFlag1 = 1; // // Since a message was received, clear any error flags. // g_bErrFlag = 0; } // // Check if the cause is message object 2. // else { // // Spurious interrupt handling can go here. // } } //***************************************************************************** // // Configure the CAN and enter a loop to receive CAN messages. // //***************************************************************************** int main(void) { #if defined(TARGET_IS_TM4C129_RA0) || \ defined(TARGET_IS_TM4C129_RA1) || \ defined(TARGET_IS_TM4C129_RA2) uint32_t ui32SysClock; #endif tCANMsgObject sCANMessage; uint8_t pui8MsgData[8]; // // Set the clocking to run directly from the external crystal/oscillator. // TODO: The SYSCTL_XTAL_ value must be changed to match the value of the // crystal used on your board. // #if defined(TARGET_IS_TM4C129_RA0) || \ defined(TARGET_IS_TM4C129_RA1) || \ defined(TARGET_IS_TM4C129_RA2) ui32SysClock = SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ | SYSCTL_OSC_MAIN | SYSCTL_USE_OSC) 25000000); #else SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ); #endif // // Set up the serial console to use for displaying messages. This is // just for this example program and is not needed for CAN operation. // InitConsole(); // // For this example CAN0 is used with RX and TX pins on port B4 and B5. // The actual port and pins used may be different on your part, consult // the data sheet for more information. // GPIO port B needs to be enabled so these pins can be used. // TODO: change this to whichever GPIO port you are using // SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB); // // Configure the GPIO pin muxing to select CAN0 functions for these pins. // This step selects which alternate function is available for these pins. // This is necessary if your part supports GPIO pin function muxing. // Consult the data sheet to see which functions are allocated per pin. // TODO: change this to select the port/pin you are using // GPIOPinConfigure(GPIO_PB4_CAN0RX); GPIOPinConfigure(GPIO_PB5_CAN0TX); // // Enable the alternate function on the GPIO pins. The above step selects // which alternate function is available. This step actually enables the // alternate function instead of GPIO for these pins. // TODO: change this to match the port/pin you are using // GPIOPinTypeCAN(GPIO_PORTB_BASE, GPIO_PIN_4 | GPIO_PIN_5); // // The GPIO port and pins have been set up for CAN. The CAN peripheral // must be enabled. // SysCtlPeripheralEnable(SYSCTL_PERIPH_CAN0); // // Initialize the CAN controller // CANInit(CAN0_BASE); // // Set up the bit rate for the CAN bus. This function sets up the CAN // bus timing for a nominal configuration. You can achieve more control // over the CAN bus timing by using the function CANBitTimingSet() instead // of this one, if needed. // In this example, the CAN bus is set to 500 kHz. In the function below, // the call to SysCtlClockGet() or ui32SysClock is used to determine the // clock rate that is used for clocking the CAN peripheral. This can be // replaced with a fixed value if you know the value of the system clock, // saving the extra function call. For some parts, the CAN peripheral is // clocked by a fixed 8 MHz regardless of the system clock in which case // the call to SysCtlClockGet() or ui32SysClock should be replaced with // 8000000. Consult the data sheet for more information about CAN // peripheral clocking. // #if defined(TARGET_IS_TM4C129_RA0) || \ defined(TARGET_IS_TM4C129_RA1) || \ defined(TARGET_IS_TM4C129_RA2) CANBitRateSet(CAN0_BASE, ui32SysClock, 500000); #else CANBitRateSet(CAN0_BASE, SysCtlClockGet(), 500000); #endif // // Enable interrupts on the CAN peripheral. This example uses static // allocation of interrupt handlers which means the name of the handler // is in the vector table of startup code. If you want to use dynamic // allocation of the vector table, then you must also call CANIntRegister() // here. // // CANIntRegister(CAN0_BASE, CANIntHandler); // if using dynamic vectors // CANIntEnable(CAN0_BASE, CAN_INT_MASTER | CAN_INT_ERROR | CAN_INT_STATUS); // // Enable the CAN interrupt on the processor (NVIC). // IntEnable(INT_CAN0); // // Enable the CAN for operation. // CANEnable(CAN0_BASE); // // Initialize a message object to receive CAN messages with ID 0x1001. // The expected ID must be set along with the mask to indicate that all // bits in the ID must match. // sCANMessage.ui32MsgID = 0x1001; sCANMessage.ui32MsgIDMask = 10; sCANMessage.ui32Flags = (MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER | MSG_OBJ_EXTENDED_ID); sCANMessage.ui32MsgLen = 8; // // Now load the message object into the CAN peripheral message object 1. // Once loaded the CAN will receive any messages with this CAN ID into // this message object, and an interrupt will occur. // CANMessageSet(CAN0_BASE, 1, &sCANMessage, MSG_OBJ_TYPE_RX); // // Change the ID to 0x2001, and load into message object 2 which will be // used for receiving any CAN messages with this ID. Since only the CAN // ID field changes, we don't need to reload all the other fields. // for(;;) { // // If the flag for message object 1 is set, that means that the RX // interrupt occurred and there is a message ready to be read from // this CAN message object. // if(g_bRXFlag1) { // // Reuse the same message object that was used earlier to configure // the CAN for receiving messages. A buffer for storing the // received data must also be provided, so set the buffer pointer // within the message object. This same buffer is used for all // messages in this example, but your application could set a // different buffer each time a message is read in order to store // different messages in different buffers. // sCANMessage.pui8MsgData = pui8MsgData; // // Read the message from the CAN. Message object number 1 is used // (which is not the same thing as CAN ID). The interrupt clearing // flag is not set because this interrupt was already cleared in // the interrupt handler. // CANMessageGet(CAN0_BASE, 1, &sCANMessage, 0); // // Clear the pending message flag so that the interrupt handler can // set it again when the next message arrives. // g_bRXFlag1 = 0; // // Print information about the message just received. // PrintCANMessageInfo(&sCANMessage, 1); gettingmsg(&sCANMessage, 1); // PrintCANMessageInfo1(&g_SCANMsgObject2, 2); } } // // Check for message received on message object 2. If so then // read message and print information. // }