/** @file sys_main.c 
*   @brief Application main file
*   @date 11-Dec-2018
*   @version 04.07.01
*
*   This file contains an empty main function,
*   which can be used for the application.
*/

/* 
* Copyright (C) 2009-2018 Texas Instruments Incorporated - www.ti.com 
* 
* 
*  Redistribution and use in source and binary forms, with or without 
*  modification, are permitted provided that the following conditions 
*  are met:
*
*    Redistributions of source code must retain the above copyright 
*    notice, this list of conditions and the following disclaimer.
*
*    Redistributions in binary form must reproduce the above copyright
*    notice, this list of conditions and the following disclaimer in the 
*    documentation and/or other materials provided with the   
*    distribution.
*
*    Neither the name of Texas Instruments Incorporated nor the names of
*    its contributors may be used to endorse or promote products derived
*    from this software without specific prior written permission.
*
*  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
*  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
*  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
*  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
*  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
*  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
*  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
*  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
*  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
*  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
*  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*/


/* USER CODE BEGIN (0) */
/* USER CODE END */

/* Include Files */

#include "sys_common.h"

/* USER CODE BEGIN (1) */
/* USER CODE END */

/** @fn void main(void)
*   @brief Application main function
*   @note This function is empty by default.
*
*   This function is called after startup.
*   The user can use this function to implement the application.
*/

/* USER CODE BEGIN (2) */
#include "ti_fee.h"

#include "bl_flash.h"
#include "F021.h"

extern unsigned int apiLoadStart;
extern unsigned int apiLoadSize;
extern unsigned int apiRunStart;

uint16 u16JobResult,Status;
Std_ReturnType oResult=E_OK;
unsigned char read_data[100]={0};

uint8 SpecialRamBlock[100];

unsigned char pattern;
uint16 u16writecounter;

unsigned int  FeeVirtualSectorNumber;
unsigned char VsState, u8EEPIndex;
unsigned char u8VirtualSector;
uint8 Test_Recovery;
uint8 Test_Cancel;


void delay(void)
{
    unsigned int dummycnt=0x0000FFU;
    do
    {
        dummycnt--;
    }
    while(dummycnt>0);
}
/* USER CODE END */

int main(void)
{
/* USER CODE BEGIN (3) */
    uint32_t status, i;

    unsigned int BlockNumber;
    unsigned int BlockOffset, Length;
    unsigned char *Read_Ptr=read_data;

    unsigned int loop;

    memcpy(&apiRunStart, &apiLoadStart, (uint32)&apiLoadSize);

    uint32_t Success[] = {0xbd0400ea, 0x12345678,
                          0x5a5a5a5a, 0x37373737,
                          0x19191919, 0x28282828,
                          0xabababab, 0xcdcdcdcd,
                          0x38b50546, 0x0c46062d,
                          0x05d0082d, 0x03d00e2d,
                          0x18bf0520, 0x08d11020,
                          0x00f034fa, 0x03480460};

    for(i=0; i<1; i++){
        status = Fapi_BlockErase(0x80000, 8);

        //make sure "Fapi_AutoEccGeneration" is used in Flash API call, bl_flash.c
        status = Fapi_BlockProgram(0x80000, (unsigned long)&Success, 8);
    }

    /* Initialize RAM array.*/
    for(loop=0;loop<100;loop++)SpecialRamBlock[loop] = loop;

    /* Initialize FEE. This will create Virtual sectors, initialize global variables etc.*/
    TI_Fee_Init();
    do
    {
        TI_Fee_MainFunction();
        delay();
        Status=TI_Fee_GetStatus(0 );
    }
    while(Status!= IDLE);

    /* Write the block into EEP Asynchronously. Block size is configured in ti_fee_cfg.c file. Default Block size is
       8 bytes */
    BlockNumber=0x1;
    TI_Fee_WriteAsync(BlockNumber, &SpecialRamBlock[0]);
    do
    {
        TI_Fee_MainFunction();
        delay();
        Status=TI_Fee_GetStatus(0);
    }
    while(Status!=IDLE);


    /* Write the block into EEP Synchronously. Write will not happen since data is same. */
    TI_Fee_WriteSync(BlockNumber, &SpecialRamBlock[0]);

    /* Read the block with unknown length */
     BlockOffset = 0;
     Length = 0xFFFF;
     oResult=TI_Fee_Read(BlockNumber,BlockOffset,Read_Ptr,Length);
     do
     {
         TI_Fee_MainFunction();
         delay();
         Status=TI_Fee_GetStatus(0);
     }
    while(Status!=IDLE);

    /* Invalidate a written block  */
    TI_Fee_InvalidateBlock(BlockNumber);
    do
    {
        TI_Fee_MainFunction();
        delay();
        Status=TI_Fee_GetStatus(0);
    }
    while(Status!=IDLE);

    /* Format bank 7 */
    TI_Fee_Format(0xA5A5A5A5U);



/* USER CODE END */

    return 0;
}


/* USER CODE BEGIN (4) */
/* USER CODE END */