/** @file sys_main.c * @brief Application main file * @date 05-Oct-2016 * @version 04.06.00 * * This file contains an empty main function, * which can be used for the application. */ /* * Copyright (C) 2009-2016 Texas Instruments Incorporated - www.ti.com * * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the * distribution. * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * */ /* USER CODE BEGIN (0) */ /* USER CODE END */ /* Include Files */ #include "sys_common.h" /* USER CODE BEGIN (1) */ /* USER CODE END */ /** @fn void main(void) * @brief Application main function * @note This function is empty by default. * * This function is called after startup. * The user can use this function to implement the application. */ /* USER CODE BEGIN (2) */ #include "F021.h" #include "gio.h" #include "het.h" #include "sci.h" #include "cpy_tbl.h" #include "ti_fee.h" #include "ti_fee_Types.h" extern COPY_TABLE _flash_ctbl; #define WRITE 1 void delay(void) { unsigned int dummycnt=0x0000FFU; do { dummycnt--; }while(dummycnt>0); } uint16 u16JobResult,Status; Std_ReturnType oResult=E_OK; unsigned char read_data[100]={0}; uint8 SpecialRamBlock[100]; unsigned char pattern; uint16 u16writecounter; unsigned int FeeVirtualSectorNumber; unsigned char VsState, u8EEPIndex; unsigned char u8VirtualSector; uint8 Test_Recovery; uint8 Test_Cancel; /* USER CODE END */ int main(void) { /* USER CODE BEGIN (3) */ Fapi_StatusType f021_Res; Fapi_FlashStatusWordType f021_State; uint32_t *f021_Address; uint8 *ReadAdd , ReadData; uint32_t ReadBuff[8] = { 0 } ; Std_ReturnType StatusReturn ; uint16 flag = 0 ; uint8_t Data[]= { }; unsigned int BlockNumber; unsigned int BlockOffset, Length; unsigned char *Read_Ptr=read_data; unsigned int loop; /* Initialize RAM array.*/ for(loop=0;loop<10;loop++)SpecialRamBlock[loop] = loop; sciInit(); gioSetDirection( hetPORT1 , 0xffffffff ); copy_in(&_flash_ctbl); f021_Res = Fapi_initializeFlashBanks(160); if (f021_Res != Fapi_Status_Success) { sciSend(scilinREG , 38 ,(uint8 *)"Unable to initialize EEPROM support!"); return; } else { sciSend(scilinREG , 29,(uint8 *) "EEPROM support initialized..."); } sciSend(scilinREG , 2,"\r\n"); // f021_Res = Fapi_setActiveFlashBank(Fapi_FlashBank7); //f021_Res = Fapi_enableEepromBankSectors( 0x0000000f , 0x00000000); if (f021_Res != Fapi_Status_Success) { sciSend(scilinREG , 28,(uint8 *)"Unable to activate flash bank!"); return; } sciSend(scilinREG , 2,"\r\n"); while ( FAPI_CHECK_FSM_READY_BUSY != Fapi_Status_FsmReady) ; //f021_Res = Fapi_enableMainBankSectors(0xFFFF); f021_Res = Fapi_enableEepromBankSectors( 0x0000000f , 0x00000000); if (f021_Res != Fapi_Status_Success) { sciSend(scilinREG , 26,(uint8 *)"Unable to enable sectors!"); return; } sciSend(scilinREG , 2,"\r\n"); while(1) { while ( FAPI_CHECK_FSM_READY_BUSY != Fapi_Status_FsmReady); Fapi_issueAsyncCommandWithAddress(Fapi_EraseSector, (uint32 *) 0xf0200002); f021_Address = (uint32 *) 0xf0200002; f021_State.au32StatusWord[3] = 0; // prepare function answer // Fapi_disableAutoEccCalculation(); //Fapi_disableAutoEccCalculation(); f021_Res = Fapi_doBlankCheck(f021_Address, 2, &f021_State); if (f021_Res == Fapi_Status_Success) sciSend(scilinREG , 8,(uint8 *)"sucess\r\n"); else sciSend(scilinREG , 9,(uint8 *)"unsucess\r\n"); while ( FAPI_CHECK_FSM_READY_BUSY != Fapi_Status_FsmReady); f021_Address = (uint32 *) 0xf0200002; if(WRITE) { if( flag == 0 ) { Data[0] = 0x11;//,0x56,0x57,0x08,0x09,0x10,0x11,0x12,0x13,0x14}; Data[1] = 0x22; Data[2] = 0x33; Data[3] = 0x44; Data[4] = 0x55; flag = 1 ; } else { Data[0] = 0x66;//,0x56,0x57,0x08,0x09,0x10,0x11,0x12,0x13,0x14}; Data[1] = 0x77; Data[2] = 0x88; Data[3] = 0x99; Data[4] = 0x00; flag = 0 ; } f021_Res = Fapi_issueProgrammingCommand(f021_Address,Data,5,0,0,Fapi_DataOnly); } else { uint8_t Data[]={0x00};//,0x56,0x57,0x08,0x09,0x10,0x11,0x12,0x13,0x14}; f021_Res = Fapi_issueProgrammingCommand(f021_Address,Data,5,0,0,Fapi_DataOnly); } if ( f021_Res != Fapi_Status_Success ){ sciSend(scilinREG , 26,(uint8 *)"Unable to write!"); return; } while ( FAPI_CHECK_FSM_READY_BUSY != Fapi_Status_FsmReady); // Fapi_doMarginRead( f021_Address , ReadBuff , 1 , Fapi_NormalRead ); ReadAdd = (uint8 *) 0xf0200002; Fapi_doMarginReadByByte( ReadAdd , &ReadData , 1 , Fapi_NormalRead ); gioSetBit( hetPORT1 , 0 , 1); gioSetBit( hetPORT1 , 5 , 1); gioSetBit( hetPORT1 , 25 , 1); // } /* USER CODE END */ return 0; } /* USER CODE BEGIN (4) */ /* USER CODE END */