//***************************************************************************** // // Digitalpot.c - Example demonstrating how to configure SSI2 in TI master mode. // // Copyright (c) 2010-2017 Texas Instruments Incorporated. All rights reserved. // Software License Agreement // // This is part of revision 2.1.4.178 of the Tiva Firmware Development Package. // //***************************************************************************** #include #include #include "inc/hw_gpio.h" #include "inc/hw_ints.h" #include "inc/hw_nvic.h" #include "inc/hw_memmap.h" #include "inc/hw_types.h" #include "driverlib/debug.h" #include "driverlib/fpu.h" #include "driverlib/gpio.h" #include "driverlib/interrupt.h" #include "driverlib/pin_map.h" #include "driverlib/rom.h" #include "driverlib/pwm.h" #include "driverlib/sysctl.h" #include "driverlib/systick.h" #include "driverlib/uart.h" #include "utils/uartstdio.h" #include "driverlib/adc.h" #include "driverlib/timer.h" #include "math.h" #include "driverlib/ssi.h" #include "driverlib/qei.h" //***************************************************************************** // //! \addtogroup ssi_examples_list //!

TI Master (ti_master)

//! //! This example shows how to configure the SSI0 as TI Master. The code will //! send three characters on the master Tx then poll the receive FIFO until //! 3 characters are received on the master Rx. //! //! This example uses the following peripherals and I/O signals. You must //! review these and change as needed for your own board: //! - SSI2 peripheral //! - GPIO Port B peripheral (for SSI2 pins) //! - SSI2Clk - PB4 //! - SSI2Fss - PB5 //! - SSI2Rx - PB6 //! - SSI2Tx - PB7 //! //! The following UART signals are configured only for displaying console //! messages for this example. These are not required for operation of I2C0. //! - UART0 peripheral //! - GPIO Port A peripheral (for UART0 pins) //! - UART0RX - PA0 //! - UART0TX - PA1 //! //! This example uses the following interrupt handlers. To use this example //! in your own application you must add these interrupt handlers to your //! vector table. //! - None. // //***************************************************************************** // DigitalPot Command Byte for Digital Pot Reading and writing. // //***************************************************************************** #define COMMAND_WRITE 0x40 #define COMMAND_READ 0x4C //***************************************************************************** // // Transmit FIFO and Receive FIFO // //***************************************************************************** uint32_t pui32DataTx; uint32_t pui32DataRx; //***************************************************************************** // // This Function is used to Enable the all peripheral clocks. // A,B,C,D,E and F //***************************************************************************** void InitModules(void) { SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA); SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB); SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOC); SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD); SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE); SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF); } //***************************************************************************** // // This function sets up UART0 to be used for a console to display information // as the example is running. // //***************************************************************************** void InitConsole(void) { // // Enable UART0 so that we can configure the clock. // SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0); // // Configure the pin muxing for UART0 functions on port A0 and A1. // This step is not necessary if your part does not support pin muxing. // TODO: change this to select the port/pin you are using. // GPIOPinConfigure(GPIO_PA0_U0RX); GPIOPinConfigure(GPIO_PA1_U0TX); // // Use the internal 16MHz oscillator as the UART clock source. // UARTClockSourceSet(UART0_BASE, UART_CLOCK_PIOSC); // // Select the alternate (UART) function for these pins. // TODO: change this to select the port/pin you are using. // GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1); // // Initialize the UART for console I/O. // UARTStdioConfig(0, 115200, 16000000); } //***************************************************************************** // // Configure SSI2 in Master TI mode. This example will send out 10 bytes of // data, then wait for 3 bytes of data to come in. This will all be done using // the interrupt method. // //***************************************************************************** void InitSSI2(void) { // // The SSI0 peripheral must be enabled for use. // SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI2); // // // Configure the pin muxing for SSI2 functions on port A2, A3, A4, and A5. // This step is not necessary if your part does not support pin muxing. // TODO: change this to select the port/pin you are using. // GPIOPinConfigure(GPIO_PB4_SSI2CLK); // GPIOPinConfigure(GPIO_PB5_SSI2FSS); GPIOPinConfigure(GPIO_PB6_SSI2RX); GPIOPinConfigure(GPIO_PB7_SSI2TX); // // Configure the GPIO settings for the SSI pins. This function also gives // control of these pins to the SSI hardware. Consult the data sheet to // see which functions are allocated per pin. // The pins are assigned as follows: // PB7 - SSI0Tx // PB6 - SSI0Rx // PB5 - SSI0Fss // PB4 - SSI0CLK // TODO: change this to select the port/pin you are using. // GPIOPinTypeSSI(GPIO_PORTB_BASE,GPIO_PIN_7|GPIO_PIN_6|GPIO_PIN_4); // // Configure PB2,PE0,PF0,PA6 pins for digital pot slave select // GPIOPinTypeGPIOOutput(GPIO_PORTB_BASE,GPIO_PIN_2); GPIOPinTypeGPIOOutput(GPIO_PORTE_BASE,GPIO_PIN_0); GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE,GPIO_PIN_0); GPIOPinTypeGPIOOutput(GPIO_PORTA_BASE,GPIO_PIN_6); // // Unlock the PF0 pin // HWREG(GPIO_PORTF_BASE + GPIO_O_LOCK) = GPIO_LOCK_KEY; HWREG(GPIO_PORTF_BASE + GPIO_O_CR) |= 0x01; HWREG(GPIO_PORTF_BASE + GPIO_O_AFSEL) |= 0x400; HWREG(GPIO_PORTF_BASE + GPIO_O_DEN) |= 0x01; HWREG(GPIO_PORTF_BASE + GPIO_O_LOCK) = 0; // // Configure and enable the SSI port for TI master mode. Use SSI2, system // clock supply, master mode, 1MHz SSI frequency, and 8-bit data. // SSIConfigSetExpClk(SSI2_BASE, SysCtlClockGet(),SSI_FRF_MOTO_MODE_0,SSI_MODE_MASTER,50000, 16); // // Enable SSI2 module // SSIEnable(SSI2_BASE); // // Make Chip select pins as High // GPIOPinWrite(GPIO_PORTB_BASE,GPIO_PIN_2,GPIO_PIN_2); GPIOPinWrite(GPIO_PORTE_BASE,GPIO_PIN_0,GPIO_PIN_0); GPIOPinWrite(GPIO_PORTF_BASE,GPIO_PIN_0,GPIO_PIN_0); GPIOPinWrite(GPIO_PORTA_BASE,GPIO_PIN_6,GPIO_PIN_6); // // Read any residual data from the SSI port. This makes sure the receive // FIFOs are empty, so we don't read any unwanted junk. This is done here // because the TI SSI mode is full-duplex, which allows you to send and // receive at the same time. The SSIDataGetNonBlocking function returns // "true" when data was returned, and "false" when no data was returned. // The "non-blocking" function checks if there is any data in the receive // FIFO and does not "hang" if there isn't. // while(SSIDataGetNonBlocking(SSI2_BASE, &pui32DataRx)) { } } //***************************************************************************** // // This function is used to send 16 bit data over SSI2 bus // //***************************************************************************** bool SSI2_MCP41HV51_Write (uint32_t ulDataTx,uint32_t channel) { uint32_t validity = false; pui32DataTx = 0x4200 | (ulDataTx & 0xff); // pui32DataTx = ulDataTx; switch(channel) { case 1: GPIOPinWrite(GPIO_PORTB_BASE,GPIO_PIN_2,~GPIO_PIN_2); SysCtlDelay(100); // SSIDataPut(SSI2_BASE, 0x0000); SSIDataPut(SSI2_BASE, pui32DataTx); while(SSIBusy(SSI2_BASE)); GPIOPinWrite(GPIO_PORTB_BASE,GPIO_PIN_2,GPIO_PIN_2); SysCtlDelay(100); validity = true; break; case 2: GPIOPinWrite(GPIO_PORTE_BASE,GPIO_PIN_0,~GPIO_PIN_0); SysCtlDelay(100); SSIDataPut(SSI2_BASE, pui32DataTx); while(SSIBusy(SSI2_BASE)); GPIOPinWrite(GPIO_PORTE_BASE,GPIO_PIN_0,GPIO_PIN_0); SysCtlDelay(100); validity = true; break; case 3: GPIOPinWrite(GPIO_PORTF_BASE,GPIO_PIN_0,~GPIO_PIN_0); SysCtlDelay(100); SSIDataPut(SSI2_BASE, pui32DataTx); while(SSIBusy(SSI2_BASE)); GPIOPinWrite(GPIO_PORTF_BASE,GPIO_PIN_0,GPIO_PIN_0); SysCtlDelay(100); validity = true; break; case 4: GPIOPinWrite(GPIO_PORTA_BASE,GPIO_PIN_6,~GPIO_PIN_6); SysCtlDelay(100); SSIDataPut(SSI2_BASE, pui32DataTx); while(SSIBusy(SSI2_BASE)); GPIOPinWrite(GPIO_PORTA_BASE,GPIO_PIN_6,GPIO_PIN_6); SysCtlDelay(100); validity = true; break; default:GPIOPinWrite(GPIO_PORTB_BASE,GPIO_PIN_2,GPIO_PIN_2); GPIOPinWrite(GPIO_PORTE_BASE,GPIO_PIN_0,GPIO_PIN_0); GPIOPinWrite(GPIO_PORTF_BASE,GPIO_PIN_0,GPIO_PIN_0); GPIOPinWrite(GPIO_PORTA_BASE,GPIO_PIN_6,GPIO_PIN_6); validity = false; } return validity; } //***************************************************************************** // // Main function entry starts here // //***************************************************************************** int main(void) { uint32_t Rx_Data[10] = {0}; uint32_t count = 0; // // Set the clocking to run directly from the external crystal/oscillator. // TODO: The SYSCTL_XTAL_ value must be changed to match the value of the // crystal on your board. // SysCtlClockSet(SYSCTL_SYSDIV_4 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ); // // Set up the serial console to use for displaying messages. // InitModules(); InitConsole(); InitSSI2(); SSI2_MCP41HV51_Write(0x00,1); SysCtlDelay(10000); SSI2_MCP41HV51_Write(0xff,1); SysCtlDelay(10000); while(1) { // // // // Receive command the data from UART to control the Digital pot // // // while(UARTCharsAvail(UART0_BASE)) // { // Rx_Data[count] = UARTCharGetNonBlocking(UART0_BASE); // // if( Rx_Data[count] == '@') // { // uint32_t Channel = Rx_Data[0] - 48; // uint32_t Data = ((Rx_Data[2] - 48) * 100) + ((Rx_Data[3] - 48) * 10) + (Rx_Data[4] - 48); // SSI2_MCP41HV51_Write(Data,Channel); // count = 0; // } // else // { // count++; // } // } SSI2_MCP41HV51_Write(0x80,1); SysCtlDelay(10000); // SSI2_MCP41HV51_Write(0x10,2); // SysCtlDelay(100); // // SSI2_MCP41HV51_Write(0x20,3); // SysCtlDelay(100); // // SSI2_MCP41HV51_Write(0x30,4); // SysCtlDelay(100); } }