U-Boot SPL 2023.04-dirty (Aug 14 2026 - 17:08:13 +0530) SYSFW ABI: 3.1 (firmware rev 0x0009 '9.2.7--v09.02.07 (Kool Koala)') am62a_init: board_init_f done SPL initial stack usage: 17064 bytes am62a_init: spl_boot_device: devstat = 0x243 bootmedia = 0x8 bootindex = 0 Trying to boot from MMC2 am62a_init: spl_boot_device: devstat = 0x243 bootmedia = 0x8 bootindex = 0 Authentication passed am62a_init: spl_boot_device: devstat = 0x243 bootmedia = 0x8 bootindex = 0 Authentication passed am62a_init: spl_boot_device: devstat = 0x243 bootmedia = 0x8 bootindex = 0 Authentication passed am62a_init: spl_boot_device: devstat = 0x243 bootmedia = 0x8 bootindex = 0 Authentication passed am62a_init: spl_boot_device: devstat = 0x243 bootmedia = 0x8 bootindex = 0 Authentication passed Starting ATF on ARM64 core... NOTICE: BL31: v2.10.0(release):v2.10.0-367-g00f1ec6b87-dirty NOTICE: BL31: Built : 16:09:05, Feb 9 2024 U-Boot SPL 2023.04-dirty (Aug 14 2026 - 17:08:01 +0530) SYSFW ABI: 3.1 (firmware rev 0x0009 '9.2.7--v09.02.07 (Kool Koala)') am62a_init: board_init_f done am62a_init: spl_boot_device: devstat = 0x243 bootmedia = 0x8 bootindex = 0 Trying to boot from MMC2 am62a_init: spl_boot_device: devstat = 0x243 bootmedia = 0x8 bootindex = 0 Authentication passed am62a_init: spl_boot_device: devstat = 0x243 bootmedia = 0x8 bootindex = 0 Authentication passed U-Boot 2023.04-dirty (Aug 14 2026 - 17:08:01 +0530) SoC: AM62AX SR1.0 HS-FS Model: Texas Instruments AM62A7 SK DRAM: 2 GiB (effective 4 GiB) Core: 58 devices, 28 uclasses, devicetree: separate MMC: mmc@fa10000: 0, mmc@fa00000: 1 Loading Environment from nowhere... OK In: serial@2800000 Out: serial@2800000 Err: serial@2800000 Net: Could not get PHY for ethernet@8000000port@1: addr 0 am65_cpsw_nuss_port ethernet@8000000port@1: phy_connect() failed No ethernet found. Hit any key to stop autoboot: 0 switch to partitions #0, OK mmc1 is current device SD/MMC found on device 1 Failed to load 'boot.scr' 675 bytes read in 23 ms (28.3 KiB/s) Loaded env from uEnv.txt Importing environment from mmc1 ... ## Error: "main_cpsw0_qsgmii_phyinit" not defined 19376640 bytes read in 827 ms (22.3 MiB/s) 58214 bytes read in 27 ms (2.1 MiB/s) Working FDT set to 88000000 3441 bytes read in 25 ms (133.8 KiB/s) ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Working FDT set to 88000000 Loading Device Tree to 000000008feee000, end 000000008fffffff ... OK Working FDT set to 8feee000 Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034] [ 0.000000] Linux version 6.1.80-ti-g2e423244f8c0 (oe-user@oe-host) (aarch64-oe-linux-gcc (GCC) 11.4.0, GNU ld (GNU Binutils) 2.38.20220708) #1 SMP PREEMPT Wed Mar 20 14:43:33 UTC 2024 [ 0.000000] Machine model: Texas Instruments AM62A7 SK [ 0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '') [ 0.000000] printk: bootconsole [ns16550a0] enabled [ 0.000000] efi: UEFI not found. [ 0.000000] Reserved memory: created CMA memory pool at 0x00000000c0000000, size 576 MiB [ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x0000000099800000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node c7x-dma-memory@99800000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x0000000099900000, size 30 MiB [ 0.000000] OF: reserved mem: initialized node c7x-memory@99900000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009b800000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@9b800000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009b900000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@9b900000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009c800000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@9c800000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009c900000, size 30 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@9c900000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 32 MiB [ 0.000000] OF: reserved mem: initialized node edgeai-dma-memory@a1000000, compatible id shared-dma-pool [ 0.000000] OF: reserved mem: initialized node edgeai_shared-memories, compatible id dma-heap-carveout [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000ae000000, size 288 MiB [ 0.000000] OF: reserved mem: initialized node edgeai-core-heap-memory@ae000000, compatible id shared-dma-pool [ 0.000000] Zone ranges: [ 0.000000] DMA [mem 0x0000000080000000-0x00000000ffffffff] [ 0.000000] DMA32 empty [ 0.000000] Normal [mem 0x0000000100000000-0x00000008ffffffff] [ 0.000000] Movable zone start for each node [ 0.000000] Early memory node ranges [ 0.000000] node 0: [mem 0x0000000080000000-0x00000000997fffff] [ 0.000000] node 0: [mem 0x0000000099800000-0x000000009b7fefff] [ 0.000000] node 0: [mem 0x000000009b800000-0x000000009e6fffff] [ 0.000000] node 0: [mem 0x000000009e700000-0x000000009e77ffff] [ 0.000000] node 0: [mem 0x000000009e780000-0x00000000a2ffffff] [ 0.000000] node 0: [mem 0x00000000a3000000-0x00000000adffffff] [ 0.000000] node 0: [mem 0x00000000ae000000-0x00000000bfffffff] [ 0.000000] node 0: [mem 0x00000000c0000000-0x00000000ffffffff] [ 0.000000] node 0: [mem 0x0000000880000000-0x00000008ffffffff] [ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000008ffffffff] [ 0.000000] On node 0, zone DMA: 1 pages in unavailable ranges [ 0.000000] psci: probing for conduit method from DT. [ 0.000000] psci: PSCIv1.1 detected in firmware. [ 0.000000] psci: Using standard PSCI v0.2 function IDs [ 0.000000] psci: Trusted OS migration not required [ 0.000000] psci: SMC Calling Convention v1.4 [ 0.000000] percpu: Embedded 20 pages/cpu s41064 r8192 d32664 u81920 [ 0.000000] Detected VIPT I-cache on CPU0 [ 0.000000] CPU features: detected: GIC system register CPU interface [ 0.000000] CPU features: detected: ARM erratum 845719 [ 0.000000] alternatives: applying boot alternatives [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 1032191 [ 0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 mtdparts=spi-nand0:512k(ospi_nand.tiboot3),2m(ospi_nand.tispl),4m(ospi_nand.u-boot),256k(ospi_nand.env),256k(ospi_nand.env.backup),98048k@32m(ospi_nand.rootfs),256k@130816k(ospi_nand.phypattern) root=PARTUUID=076c4a2a-02 rw rootfstype=ext4 rootwait [ 0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes, linear) [ 0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes, linear) [ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off [ 0.000000] software IO TLB: area num 4. [ 0.000000] software IO TLB: mapped [mem 0x00000000fbfff000-0x00000000fffff000] (64MB) [ 0.000000] Memory: 2808820K/4194300K available (11712K kernel code, 1258K rwdata, 3812K rodata, 1984K init, 438K bss, 795656K reserved, 589824K cma-reserved) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1 [ 0.000000] rcu: Preemptible hierarchical RCU implementation. [ 0.000000] rcu: RCU event tracing is enabled. [ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4. [ 0.000000] Trampoline variant of Tasks RCU enabled. [ 0.000000] Tracing variant of Tasks RCU enabled. [ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies. [ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4 [ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0 [ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode [ 0.000000] GICv3: 256 SPIs implemented [ 0.000000] GICv3: 0 Extended SPIs implemented [ 0.000000] Root IRQ handler: gic_handle_irq [ 0.000000] GICv3: GICv3 features: 16 PPIs [ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001880000 [ 0.000000] ITS [mem 0x01820000-0x0182ffff] [ 0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS [ 0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19 [ 0.000000] ITS@0x0000000001820000: allocated 524288 Devices @880800000 (flat, esz 8, psz 64K, shr 0) [ 0.000000] ITS: using cache flushing for cmd queue [ 0.000000] GICv3: using LPI property table @0x0000000880040000 [ 0.000000] GIC: using cache flushing for LPI property table [ 0.000000] GICv3: CPU0: using allocated LPI pending table @0x0000000880050000 [ 0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention. [ 0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys). [ 0.000000] clocksource: arch_sys_counter: mask: 0x3ffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns [ 0.000001] sched_clock: 58 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns [ 0.008505] Console: colour dummy device 80x25 [ 0.013093] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000) [ 0.023775] pid_max: default: 32768 minimum: 301 [ 0.028540] LSM: Security Framework initializing [ 0.033360] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes, linear) [ 0.040940] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes, linear) [ 0.050389] cblist_init_generic: Setting adjustable number of callback queues. [ 0.057819] cblist_init_generic: Setting shift to 2 and lim to 1. [ 0.064110] cblist_init_generic: Setting adjustable number of callback queues. [ 0.071506] cblist_init_generic: Setting shift to 2 and lim to 1. [ 0.077876] rcu: Hierarchical SRCU implementation. [ 0.082784] rcu: Max phase no-delay instances is 1000. [ 0.088341] Platform MSI: msi-controller@1820000 domain created [ 0.094594] PCI/MSI: /bus@f0000/interrupt-controller@1800000/msi-controller@1820000 domain created [ 0.103996] EFI services will not be available. [ 0.108849] smp: Bringing up secondary CPUs ... [ 0.114054] Detected VIPT I-cache on CPU1 [ 0.114140] GICv3: CPU1: found redistributor 1 region 0:0x00000000018a0000 [ 0.114156] GICv3: CPU1: using allocated LPI pending table @0x0000000880060000 [ 0.114201] CPU1: Booted secondary processor 0x0000000001 [0x410fd034] [ 0.114810] Detected VIPT I-cache on CPU2 [ 0.114873] GICv3: CPU2: found redistributor 2 region 0:0x00000000018c0000 [ 0.114887] GICv3: CPU2: using allocated LPI pending table @0x0000000880070000 [ 0.114916] CPU2: Booted secondary processor 0x0000000002 [0x410fd034] [ 0.115456] Detected VIPT I-cache on CPU3 [ 0.115523] GICv3: CPU3: found redistributor 3 region 0:0x00000000018e0000 [ 0.115537] GICv3: CPU3: using allocated LPI pending table @0x0000000880080000 [ 0.115563] CPU3: Booted secondary processor 0x0000000003 [0x410fd034] [ 0.115627] smp: Brought up 1 node, 4 CPUs [ 0.195363] SMP: Total of 4 processors activated. [ 0.200177] CPU features: detected: 32-bit EL0 Support [ 0.205446] CPU features: detected: CRC32 instructions [ 0.210752] CPU: All CPU(s) started at EL2 [ 0.214949] alternatives: applying system-wide alternatives [ 0.222106] devtmpfs: initialized [ 0.233628] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns [ 0.243618] futex hash table entries: 1024 (order: 4, 65536 bytes, linear) [ 0.267215] pinctrl core: initialized pinctrl subsystem [ 0.271646] Unable to handle kernel NULL pointer dereference at virtual address 00000000000000c0 [ 0.272574] Internal error: Oops - Undefined instruction: 0000000002000000 [#1] PREEMPT SMP [ 0.281544] Mem abort info: [ 0.290075] Modules linked in: [ 0.292918] ESR = 0x0000000096000004 [ 0.292920] [ 0.292926] CPU: 0 PID: 1 Comm: swapper/0 Not tainted 6.1.80-ti-g2e423244f8c0 #1 [ 0.296033] EC = 0x25: DABT (current EL), IL = 32 bits [ 0.299855] Hardware name: Texas Instruments AM62A7 SK (DT) [ 0.301366] SET = 0, FnV = 0 [ 0.308921] pstate: 600000c5 (nZCv daIF -PAN -UAO -TCO -DIT -SSBS BTYPE=--) [ 0.314340] EA = 0, S1PTW = 0 [ 0.320028] pc : irq_enter_rcu+0x38/0x70 [ 0.323139] FSC = 0x04: level 0 translation fault [ 0.330248] lr : el1_interrupt+0x28/0x70 [ 0.333448] Data abort info: [ 0.337447] sp : ffff80000932b920 [ 0.342423] ISV = 0, ISS = 0x00000004 [ 0.346422] x29: ffff80000932b920 [ 0.349356] CM = 0, WnR = 0 [ 0.352734] x28: ffff000800108000 [ 0.356644] [00000000000000c0] user address but active_mm is swapper [ 0.360021] x27: 000000000000003b [ 0.376467] x26: 0000000000000000 x25: ffff800009285028 x24: ffff80000932bb97 [ 0.383766] x23: 0000000060000005 x22: ffff8000080af9c4 x21: ffff80000932bab0 [ 0.391064] x20: ffff80000853f0c0 x19: ffff80000932b960 x18: ffffffffffffffff [ 0.398362] x17: 000000000000001c x16: 000000001b881694 x15: ffff80008932ba27 [ 0.405660] x14: 0000000000000000 x13: 6d65747379736275 x12: 73206c7274636e69 [ 0.412958] x11: 702064657a696c61 x10: 6974696e69203a65 x9 : 7274636e69702064 [ 0.420256] x8 : 657a696c61697469 x7 : 205d353132373632 x6 : 322e30202020205b [ 0.427554] x5 : 0000000000000000 x4 : 0000000000000000 x3 : 00000000ffffffff [ 0.434852] x2 : 0000000000000040 x1 : 0000000000b10000 x0 : ffff000800108000 [ 0.442151] Call trace: [ 0.444644] irq_enter_rcu+0x38/0x70 [ 0.448296] el1_interrupt+0x28/0x70 [ 0.451948] el1h_64_irq_handler+0x18/0x2c [ 0.456134] el1h_64_irq+0x64/0x68 [ 0.459608] console_emit_next_record.constprop.0+0x190/0x28c [ 0.465484] console_unlock+0x18c/0x21c [ 0.469403] vprintk_emit+0x1b4/0x2c4 [ 0.473144] vprintk_default+0x38/0x4c [ 0.476974] vprintk+0xa4/0xc0 [ 0.480093] _printk+0x60/0x8c [ 0.483212] pinctrl_init+0x20/0xc4 [ 0.486777] do_one_initcall+0x54/0x1d0 [ 0.490694] kernel_init_freeable+0x218/0x284 [ 0.495145] kernel_init+0x24/0x130 [ 0.498710] ret_from_fork+0x10/0x20 [ 0.502364] Code: 12183c00 7140401f 540041e0 52a01621 (d5387b00) [ 0.508591] ---[ end trace 0000000000000000 ]--- [ 0.513307] Kernel panic - not syncing: Oops - Undefined instruction: Fatal exception in interrupt [ 0.522464] SMP: stopping secondary CPUs [ 1.601998] SMP: failed to stop secondary CPUs 0,3 [ 1.606894] ---[ end Kernel panic - not syncing: Oops - Undefined instruction: Fatal exception in interrupt ]---