U-Boot SPL 2015.07 (Jan 28 2016 - 19:28:18) Entering am33xx_spl_board_init func inside read_eeprom inside ti_i2c_eeprom_am_get func trace 1 ### Use AM335x_SK V1.2 setting ### trace 2 after read_eeprom!!! trace 3 trace 5 after i2c_probe after MPU voltage tps65217_reg_write tps65217_voltage_update do_setup_dpll mpu_vdd DEFLS1 DEFLS2 trace 7 boot device reading args spl_load_image_fat_os: error reading image args, err - -1 reading u-boot.img reading u-boot.img U-Boot 2015.07 (Jan 28 2016 - 19:28:18 +0530) Watchdog enabled I2C: ready DRAM: 256 MiB NAND: 0 MiB MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1 reading uboot.env ** Unable to read "uboot.env" from mmc0:1 ** Using default environment inside ti_i2c_eeprom_am_get func trace 1 ### Use AM335x_SK V1.2 setting ### trace 2 Net: Net Initialization Skipped No ethernet found. Hit any key to stop autoboot: 0 switch to partitions #0, OK mmc0 is current device SD/MMC found on device 0 reading boot.scr ** Unable to read file boot.scr ** reading uEnv.txt ** Unable to read file uEnv.txt ** syntax error switch to partitions #0, OK mmc0 is current device SD/MMC found on device 0 2649704 bytes read in 230 ms (11 MiB/s) 32572 bytes read in 60 ms (529.3 KiB/s) Kernel image @ 0x82000000 [ 0x000000 - 0x286e68 ] ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Loading Device Tree to 8ef26000, end 8ef30f3b ... OK Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Initializing cgroup subsys cpuset [ 0.000000] Initializing cgroup subsys cpu [ 0.000000] Initializing cgroup subsys cpuacct [ 0.000000] Linux version 4.1.13-g8dc6617 (administrator@MYTSP00128) (gcc version 4.9.3 20150413 (prerelease) (Linaro GCC 4.9-20156 [ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] Machine model: TI AM335x EVM-SK [ 0.000000] cma: Reserved 24 MiB at 0x8d000000 [ 0.000000] Memory policy: Data cache writeback [ 0.000000] CPU: All CPU(s) started in SVC mode. [ 0.000000] AM335X ES2.1 (neon ) [ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 64960 [ 0.000000] Kernel command line: console=ttyO0,115200n8 root=PARTUUID=00000000-02 rw rootfstype=ext4 rootwait [ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes) [ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes) [ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes) [ 0.000000] Memory: 227384K/262144K available (5087K kernel code, 196K rwdata, 1672K rodata, 236K init, 210K bss, 10184K reserved,) [ 0.000000] Virtual kernel memory layout: [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB) [ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB) [ 0.000000] vmalloc : 0xd0800000 - 0xff000000 ( 744 MB) [ 0.000000] lowmem : 0xc0000000 - 0xd0000000 ( 256 MB) [ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB) [ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB) [ 0.000000] .text : 0xc0008000 - 0xc06a207c (6761 kB) [ 0.000000] .init : 0xc06a3000 - 0xc06de000 ( 236 kB) [ 0.000000] .data : 0xc06de000 - 0xc070f0a8 ( 197 kB) [ 0.000000] .bss : 0xc0712000 - 0xc07469e0 ( 211 kB) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1 [ 0.000000] Preemptible hierarchical RCU implementation. [ 0.000000] Additional per-CPU info printed with stalls. [ 0.000000] NR_IRQS:16 nr_irqs:16 16 [ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts [ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz [ 0.000016] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns [ 0.000043] clocksource timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns [ 0.000058] OMAP clocksource: timer1 at 24000000 Hz [ 0.000276] Console: colour dummy device 80x30 [ 0.000305] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0' [ 0.000313] This ensures that you still see kernel messages. Please [ 0.000320] update your kernel commandline. [ 0.000342] Calibrating delay loop... 597.60 BogoMIPS (lpj=2988032) [ 0.118930] pid_max: default: 32768 minimum: 301 [ 0.119050] Security Framework initialized [ 0.119117] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes) [ 0.119131] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes) [ 0.119992] Initializing cgroup subsys blkio [ 0.120022] Initializing cgroup subsys memory [ 0.120072] Initializing cgroup subsys devices [ 0.120091] Initializing cgroup subsys freezer [ 0.120109] Initializing cgroup subsys perf_event [ 0.120143] CPU: Testing write buffer coherency: ok [ 0.120597] Setting up static identity map for 0x80008200 - 0x80008270 [ 0.122457] devtmpfs: initialized [ 0.135095] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3 [ 0.147000] omap_hwmod: tptc0 using broken dt data from edma [ 0.147151] omap_hwmod: tptc1 using broken dt data from edma [ 0.147281] omap_hwmod: tptc2 using broken dt data from edma [ 0.152228] omap_hwmod: debugss: _wait_target_disable failed [ 0.209030] clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns [ 0.211718] pinctrl core: initialized pinctrl subsystem [ 0.212286] regulator_register: register [ 0.213365] NET: Registered protocol family 16 [ 0.216199] DMA: preallocated 256 KiB pool for atomic coherent allocations [ 0.238934] cpuidle: using governor ladder [ 0.268920] cpuidle: using governor menu [ 0.273655] OMAP GPIO hardware version 0.1 [ 0.284483] No ATAGs? [ 0.284522] hw-breakpoint: debug architecture 0x4 unsupported. [ 0.328355] edma-dma-engine edma-dma-engine.0: TI EDMA DMA engine driver [ 0.328858] reg_fixed_voltage_probe: entered [ 0.328874] of_get_fixed_voltage_config: fixed vtg extract [ 0.329080] reg_fixed_voltage_probe: if config->enabled_at_boot [ 0.329088] reg_fixed_voltage_probe: gpio low [ 0.329100] regulator_register: register [ 0.329513] reg_fixed_voltage_probe: entered [ 0.329525] of_get_fixed_voltage_config: fixed vtg extract [ 0.329566] reg_fixed_voltage_probe: else [ 0.329574] reg_fixed_voltage_probe: gpio high [ 0.329582] cfg.ena_gpio_flags [2] [ 0.329590] regulator_register: register [ 0.329919] reg_fixed_voltage_probe: entered [ 0.329931] of_get_fixed_voltage_config: fixed vtg extract [ 0.330036] reg_fixed_voltage_probe: else [ 0.330044] reg_fixed_voltage_probe: gpio high [ 0.330051] cfg.ena_gpio_flags [2] [ 0.330059] regulator_register: register [ 0.330264] regulator_ena_gpio_request: gpio enable func [ 0.330279] gpio_request_one: gpiolib_legacy.c [ 0.330363] gpio_request_one: gpio output [ 0.330379] regulator_ena_gpio_request: after gpio_request_one config->ena_gpio_flags [2] [ 0.331316] SCSI subsystem initialized [ 0.331751] omap_i2c 44e0b000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c0_pins, de [ 0.331946] pps_core: LinuxPPS API ver. 1 registered [ 0.331958] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti [ 0.332000] PTP clock support registered [ 0.333067] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400 [ 0.334622] Switched to clocksource timer1 [ 0.348014] NET: Registered protocol family 2 [ 0.349047] TCP established hash table entries: 2048 (order: 1, 8192 bytes) [ 0.349096] TCP bind hash table entries: 2048 (order: 1, 8192 bytes) [ 0.349133] TCP: Hash tables configured (established 2048 bind 2048) [ 0.349238] UDP hash table entries: 256 (order: 0, 4096 bytes) [ 0.349264] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes) [ 0.349465] NET: Registered protocol family 1 [ 0.349922] RPC: Registered named UNIX socket transport module. [ 0.349941] RPC: Registered udp transport module. [ 0.349950] RPC: Registered tcp transport module. [ 0.349958] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.350757] CPU PMU: Failed to parse /pmu/interrupt-affinity[0] [ 0.350810] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available [ 0.353319] futex hash table entries: 256 (order: -1, 3072 bytes) [ 0.353433] audit: initializing netlink subsys (disabled) [ 0.353521] audit: type=2000 audit(0.330:1): initialized [ 0.363333] VFS: Disk quotas dquot_6.6.0 [ 0.363607] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes) [ 0.366559] NFS: Registering the id_resolver key type [ 0.366649] Key type id_resolver registered [ 0.366660] Key type id_legacy registered [ 0.366751] jffs2: version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc. [ 0.369597] io scheduler noop registered [ 0.369628] io scheduler deadline registered [ 0.369700] io scheduler cfq registered (default) [ 0.370977] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568 [ 0.372367] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle [ 0.373080] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled [ 0.378022] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 155, base_baud = 3000000) is a 8250 [ 1.103670] console [ttyS0] enabled [ 1.108389] [drm] Initialized drm 1.1.0 20060810 [ 1.126234] brd: module loaded [ 1.135876] loop: module loaded [ 1.139479] mtdoops: mtd device (mtddev=name/number) must be supplied [ 1.150542] mousedev: PS/2 mouse device common for all mice [ 1.156504] i2c /dev entries driver [ 1.161173] omap_hsmmc 48060000.mmc: Got CD GPIO [ 1.166857] mmc_regulator_set_ocr: entered4 [ 1.171156] mmc_regulator_set_ocr: regulator_not enabled [ 1.176680] mmc_regulator_set_ocr: enabled true [ 1.181319] mmc_regulator_set_ocr: returning!!! [ 1.185989] __mmc_set_signal_voltage: entered1 [ 1.190543] mmc_regulator_set_ocr: entered4 [ 1.194850] mmc_regulator_set_ocr: returning!!! [ 1.236318] mmc_regulator_set_ocr: entered4 [ 1.240615] mmc_regulator_set_ocr: regulator_not enabled [ 1.250409] mmc0: mmc_attach_sdio: mmc_attach_sdio [ 1.255262] mmc0: mmc_send_io_op_cond: entering mmc_send_io_op_cond [ 1.263003] mmc_send_io_op_cond: break 1 [ 1.267061] mmc_send_io_op_cond: after for [ 1.271261] mmc_send_io_op_cond: rocr..!!! [ 1.275480] mmc0: mmc_attach_sdio: error mmc_send_io_op_cond [ 1.324634] mmc_regulator_set_ocr: enabled true [ 1.329273] mmc_regulator_set_ocr: returning!!! [ 1.333914] __mmc_set_signal_voltage: entered1 [ 1.338503] __mmc_set_signal_voltage: entered1 [ 1.343077] mmc_regulator_set_ocr: entered4 [ 1.347405] mmc_regulator_set_ocr: returning!!! [ 1.376048] mmc0: host does not support reading read-only switch, assuming write-enable [ 1.385358] remoteproc0: wkup_m3 is available [ 1.390016] mmc0: new high speed SDHC card at address e624 [ 1.395589] remoteproc0: Note: remoteproc is still under development and considered experimental. [ 1.404590] remoteproc0: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed. [ 1.415552] mmcblk0: mmc0:e624 SU04G 3.69 GiB [ 1.421076] remoteproc0: Direct firmware load for am335x-pm-firmware.elf failed with error -2 [ 1.430000] mmcblk0: p1 p2 [ 1.434083] oprofile: using arm/armv7 [ 1.439262] Initializing XFRM netlink socket [ 1.444749] remoteproc0: Falling back to user helper [ 1.451910] NET: Registered protocol family 17 [ 1.456464] mmc1: mmc_attach_sdio: mmc_attach_sdio [ 1.461279] mmc1: mmc_send_io_op_cond: entering mmc_send_io_op_cond [ 1.468086] NET: Registered protocol family 15 [ 1.472696] Key type dns_resolver registered [ 1.477382] omap_voltage_late_init: Voltage driver support not added [ 1.484305] cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517 [ 1.493195] cpu cpu0: cpu0 clock notifier not ready, retry [ 1.498786] mmc_send_io_op_cond: break 1 [ 1.502815] mmc_send_io_op_cond: after for [ 1.507433] ThumbEE CPU extension supported. [ 1.511753] Registering SWP/SWPB emulation handler [ 1.516642] mmc_send_io_op_cond: rocr..!!! [ 1.520848] mmc1: mmc_attach_sdio: error mmc_send_io_op_cond [ 1.529658] tps65217-pmic tps65217-pmic: tps65217_regulator_probe function [ 1.536830] regulator_register: register [ 1.542385] mmc_regulator_set_ocr: entered4 [ 1.546751] mmc_regulator_set_ocr: regulator disable [ 1.551836] mmc_regulator_set_ocr: enabled false [ 1.556687] mmc_regulator_set_ocr: returning!!! [ 1.562227] regulator_register: register [ 1.568207] regulator_register: register [ 1.573379] regulator_register: register [ 1.578582] regulator_register: register [ 1.583725] regulator_register: register [ 1.588910] regulator_register: register [ 1.595797] tps65217 0-0024: TPS65217 ID 0xe version 1.2 [ 1.601166] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz [ 1.607952] cpu cpu0: of_pm_voltdm_notifier_register: Fail calculating voltage latency[950000<->1100000]:-22 [ 1.618335] cpu cpu0: of_pm_voltdm_notifier_register: Fail calculating voltage latency[950000<->1100000]:-22 [ 1.628665] hctosys: unable to open rtc device (rtc0) [ 1.638273] Entering regulator_init_complete [ 1.642600] wlan-en-regulator: i'm here :'( [ 1.646957] wlan-en-regulator: disabling [ 1.650906] vbat: i'm here :'( [ 1.653971] vbat: disabling [ 1.688230] EXT4-fs (mmcblk0p2): recovery complete [ 1.693088] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null) [ 1.701381] VFS: Mounted root (ext4 filesystem) on device 179:2. [ 1.713463] devtmpfs: mounted [ 1.716919] Freeing unused kernel memory: 236K (c06a3000 - c06de000) INIT: version 2.88 booting Error opening /dev/fb0: No such file or directory Starting udev [ 2.800356] udevd[79]: starting version 182 [ 3.187626] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec [ 3.287630] omap_rtc 44e3e000.rtc: rtc core: registered 44e3e000.rtc as rtc0 [ 3.627306] omap_rng 48310000.rng: OMAP Random Number Generator ver. 20 [ 3.690405] cryptodev: disagrees about version of symbol module_layout [ 4.012043] EXT4-fs (mmcblk0p2): re-mounted. Opts: data=ordered [ 4.366862] PM: bootloader does not support rtc-only! [ 4.454304] remoteproc0: powering up wkup_m3 [ 4.476460] remoteproc0: Booting fw image am335x-pm-firmware.elf, size 219803 [ 4.484034] remoteproc0: remote processor wkup_m3 is now up [ 4.484071] wkup_m3_ipc 44e11324.wkup_m3_ipc: CM3 Firmware Version = 0x191 bootlogd: cannot allocate pseudo tty: No such file or directory Starting random number generator daemon. udevadm settle - timeout of 3 seconds reached, the event queue contains: /sys/devices/platform/ocp/48060000.mmc/mmc_host/mmc0/mmc0:e624/block/mmcblk0/mmcblk0p1 (680) /sys/devices/platform/ocp/48060000.mmc/mmc_host/mmc0/mmc0:e624/block/mmcblk0/mmcblk0p2 (681) [ 6.653602] random: dd urandom read with 110 bits of entropy available [ 6.944186] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck. ALSA: Restoring mixer settings... /usr/sbin/alsactl: load_state:1729: No soundcards found... Sat Jan 9 00:07:57 UTC 2016 INIT: Entering runlevel: 5 Configuring network interfaces... ifconfig: SIOCGIFFLAGS: No such device done. Starting system message bus: dbus. UIM SYSFS Node Not Found Initializing the graphics driver ... PVR:(Error): OpenServices: Cannot open device driver /dev/omapdrm_pvr. [140, /pvr_bridge_u.c] PVR:(Error): PVRSRVInitSrvConnect: PVRSRVConnect failed [2572, /bridged_pvr_glue.c] PVR:(Error): SrvInit: PVRSRVInitSrvConnect failed (4) [37, /srvinit.c] PVR:(Error): main: SrvInit failed (4) [49, /pvrsrvinit.c] Starting Dropbear SSH server: [ 9.676754] NET: Registered protocol family 10 dropbear. Starting telnet daemon. [ 9.806612] random: nonblocking pool is initialized Starting rpcbind daemon...done. starting statd: done Starting syslogd/klogd: done Starting thttpd. Starting Lighttpd Web Server: lighttpd. 2016-01-09 00:07:59: (/home/gtbldadm/processor-sdk-linux-fido-build/build-CORTEX_1/arago-tmp-external-linaro-toolchain/work/cortexa8h / /etc/rc5.d/S97matrix-gui-2.0: line 37: /sys/class/graphics/fbcon/cursor_blink: No such file or directory Starting Matrix GUI application. Enabling thermal zones... /etc/rc5.d/S98thermal-zone-init: line 7: /sys/class/thermal/thermal_zone*/mode: No such file or directory *************************************************************** *************************************************************** NOTICE: This file system contains the following GPLv3 packages: autoconf binutils cpp-symlinks cpp g++-symlinks g++ gcc-symlinks gcc gdb gdbserver gstreamer1.0-libav libgmp10 libmpc3 libmpfr4 make If you do not wish to distribute GPLv3 components please remove the above packages prior to distribution. This can be done using the opkg remove command. i.e.: opkg remove Where is the name printed in the list above NOTE: If the package is a dependency of another package you will be notified of the dependent packages. You should use the --force-removal-of-dependent-packages option to also remove the dependent packages as well *************************************************************** *************************************************************** _____ _____ _ _ | _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_ | | _| .'| . | . | | __| _| . | | | -_| _| _| |__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_| |___| |___| Arago Project http://arago-project.org am335x-evm /dev/ttyO0 Arago 2015.12 am335x-evm /dev/ttyO0 am335x-evm login: root root@am335x-evm:~# ifconfig -a lo Link encap:Local Loopback inet addr:127.0.0.1 Mask:255.0.0.0 inet6 addr: ::1/128 Scope:Host UP LOOPBACK RUNNING MTU:65536 Metric:1 RX packets:10 errors:0 dropped:0 overruns:0 frame:0 TX packets:10 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:0 RX bytes:700 (700.0 B) TX bytes:700 (700.0 B) root@am335x-evm:~# cat /sys/kernel/debug/gpio GPIOs 0-31, platform/44e07000.gpio, gpio: gpio-6 (cd ) in lo IRQ GPIOs 32-63, platform/4804c000.gpio, gpio: gpio-61 (wlan-en-regulator ) out hi GPIOs 64-95, platform/481ac000.gpio, gpio: GPIOs 96-127, platform/481ae000.gpio, gpio: root@am335x-evm:~#