In my project using CC26X2R1 ,SCLK LF source sometimes I planned to use XOSC and if the external crystal is not present then I use RCOSC .
MY confusion is After Boot Up sequence ,any switching from RCOSC to XOSC happen? when if use SCLK source is XOSC(external 32.768kHz low frequency) configured in ccfg.c (SET_CCFG_MODE_CONF_SCLK_LF_OPTION is 0x2) ?