Part Number: CC1352P
Other Parts Discussed in Thread: Z-STACK
Hello Ryan
BR,
Randy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CC1352P
Other Parts Discussed in Thread: Z-STACK
Hello Ryan
BR,
Randy
Hello Randy,
As you've observed, a ZDO_MGMT_LEAVE_REQ does not remove all device information (keys, binding and association/routing/neighbor table entries, etc). Instead, the ZNP waits until ZDO_LeaveCnf (status == ZSuccess) or ZDO_LeaveInd to call ZDApp_LeaveUpdate, which will not happen while the device is offline. You could try using ZDO_SEC_DEVICE_REMOVE, ZDO_REMOVE_LINK_KEY, and/or ZDO_EXT_SEC_APS_REMOVE_REQ commands from your gateway to manually force removal of this information locally, or you can modify the ZNP code to alter it's behavior towards your intended goal. The other option, as YiKai suggested, is to wait until the device comes back online to retry. You will just want to make sure that the gateway's device database stays in sync with the ZNP's stored network information, otherwise the misalignment will cause issues when attempting to send device commands.
Regards,
Ryan
Hi Ryan,
Just taking over as Randy will come in later today: if we would change the ZNP behavior not to wait for the leave confirmation and, in case the deleted device would send further messages, it will automatically get a "Remove" back as its ID is not the module's database anymore?
If yes, then we would not need to wait for it to come back and then delete again.
Regards
Peter
Hi Peter,
Unfortunately, so long as the device has the NWK key it will be able to continue communicating on the network. The APS key is removed so it would not be able to further process APS packets involving key handling. So you would need to either update the NWK key using APS encrypted requests (would have to be unicasted to each device on the network and confirm reception with an APS ACK) or wait for the device to come back online and trust that it leaves when requested. These security concerns are partly why Install Codes were introduced to Zigbee 3.0.
Regards,
Ryan