This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2650: How to disable the external flash for the CC2650

Part Number: CC2650
Other Parts Discussed in Thread: CC2640

Hi,

I am working on trying to characterize the current consumption of the CC2650 using its launchpad. I have been following a TI guide titled "Measuring CC13xx and CC26xx current consumption". Within this guide is the following:

The standby current I was measuring was around 8uA average so it seems like I should get my expected standby current (around 1.2uA) if I can disable this external flash. I searched in the SDK and found "ext_flash.c" and "ext_flash.h" in C:\ti\simplelink\ble_sdk_2_02_06_07\src\examples\util\bim_extflash\cc2640\board.

I add these to my simple_peripheral project and attempt to call the open and close functions in the SimplePeripheral_init function. The code compiles and runs but I do not get any advertisements and the current that I measure is a steady ~3.6mA. As soon as I comment out the two function calls, the example works fine and I can see advertisements. Are these the correct files that I need to disable the flash? I am unsure if I am using the wrong ext_flash files or if my implementation of the function calls is wrong. Any help or recommendations would be appreciated.


Thanks!

Josh