Part Number: TIDC-CC2650STK-SENSORTAG
Other Parts Discussed in Thread: CC2650, HDC1000, CC2650STK
Hi! Apologies if this is a repeat,, but I couldn;t find the same problem in any other thread...
I have a stack of sensortag-2 devices I bought back in 2015, and an urgent requirement to monitor temperature and humidity on an experiment that needs to be run next week. The sensortag devices would be ideal for this. I dug them out and replaced the batteries, and made sure the TI sensortag app was on my phone, and was delighted to find on searching for them with the app that they connected!
I was somewhat less delighted to find that the ambient temperature and humidity reported by all of the devices was wildly inaccurate - from -36 deg. C to +123 deg C, and RH from 0 to 90% (in the same 21 deg. RH 40% environment). For reference, the values reported by light-meter, motion-sensor etc appear more-or-less reasonable, and behave the way one might expect (ie lux goes to zero if you hide the device under an upended mug etc)
I also tried one completely un-used device I found still in its box. Exact same problem.
Has anyone any idea why the temperature and humidity sensors are behaving the way they are? Or what I can do to fix it by next Monday? Do the sensors degrade with time? Do they require some kind of reset or recalibration? If so, how is that achieved?
Thanks for any and all suggestions!
Jeremy Johnson