Part Number: ADS7960
I have met some trouble when i set the function mode of ADS7960SDBT. According to the datasheet,
as my understanding, if i want the device work in auto-1 mode,i need firstly send [0010 1000 0100 0000 ]into sdi
to set the model control registers to make it work in auto-1 mode (2*Vref), and then send [1000 0000 0000 0000]
to enter autp-1 programming register,
finally send [0000 1111 1111 1111] to choose all the twelve channels.
But the device put out lots of nonsense ones and zeros, the first 4 number is not increasing from 0000 to 1100
i wonder the problems caused by my misunderstanding of the modes control method.
I also cannot understand the use of reset state in tabel 2 in page 36 of the datasheet. and after setting suceessful ,what number should i send next to make it work continuely