This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2115A-Q1: Operating free-air temperature

Part Number: TPS2115A-Q1


Hi Team,

Let me ask two quick questions.
1. Could you tell me the background why this device's operation range is limited up to 85C?
2. What kind of list will be estimated if the device will use in 100C ambient condition?

My customer is interested in TPS2115-Q1 for ORing or low voltage power rail but their developing board is mounted very hot area in system.
Actually, load current is not so much, estimated less than 100mA but max ambient would be over 100C around the board.
This condition is violate abs max of this device at  "Operating free-air temperature".

Regards,

Takashi Onawa