what is the resistor and capacitor value for output 0.85V and 0.9V from TPS65400?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
what is the resistor and capacitor value for output 0.85V and 0.9V from TPS65400?
Hi Michael!
You can set Vref as 0.85V and 0.9V by programming. By this way, you can connect Vout pin to Vfb pin directly.
Besides the Vfb divider, there are other resistor and capacitor in the converter. Such as compensation parameters Rcomp and Ccomp, the output capacitor.
These parameters are all determined by switching frequency, Input voltage.
Could you please clarify your requirements?
Shuai
Hi Michael!
Vref can be programmed individually, from 0.6V-1.87V.
Suggested parameters:
L=0.68uH, Rcomp=10kohm, Ccomp=15nF, Cout=2*22uF(10V).
Shuai
There is a writing error. Not 0.68uH, 6.8uH.
You can search in www.we-online.com/.../start.php
If you have a lot of other questions, you can summary these together. I will reply a summary answer.
\
PG can be used to enable CE of second device. You need to pull up PG to VDD with a resistor.

based on Figure 8-13 from TPS65400 datasheet. there are Rc, Cc and Croll. so the Cc is 15nf? Rc is the 10K? what about the Croll?
what is the function of 0ohm on the TPS65400 EVAL board between CB and capacitors?
does I2C programmer need I2CALERT signal? if not can i leave I2CALERT pin open?
Keep the position for that if customer want to slow down the turn on/off slew rate.
the TPS65400 datasheet states that the external programmer needs to connect CE of TPS65400 (datasheet Page 24). the Evaluation board doesn't connect the CE over J13. can you please advise?
the TPS65400 datasheet states that the external programmer needs to connect CE of TPS65400 (datasheet Page 24). the Evaluation board doesn't connect the CE over J13. can you please advise?
does I2C programmer need I2CALERT signal? if not can i leave I2CALERT pin open?
Because EVM board is not external. In EVM, it need to supply VIN. Then CE will be high because the internal pullup current. After these being done, the device can be programmed.
It need I2CALERT , this likes a watch dog to feedback the error state.