Other Parts Discussed in Thread: SIMPLELINK-CC13XX-CC26XX-SDK, TIMAC
Hi!
Following the suggestions in this thread I'm in the process of upgrading from TI SDK 3.40 to 6.10.
I'm facing multiple undefined symbols, a total of 334 symbols, see build output below. Can anyone please help me out?
Edit: Suspecting there could be a missing library somewhere in the setup. While upgrading I changed COM_TI_SIMPLELINK_CC13X2_26X2_SDK_LIBRARIES to COM_TI_SIMPLELINK_CC13XX_CC26XX_SDK_LIBRARIES, yet I don't find it defined somewhere? What is the target for COM_TI_SIMPLELINK_CC13XX_CC26XX_SDK_LIBRARIES and COM_TI_SIMPLELINK_CC13XX_CC26XX_SDK_LIBRARY_PATH?
Building target: ""
Invoking: ARM Linker
Flags: --cmd_file="C:/Work/radio/defines/defines.opts" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me -O2 --opt_for_speed=1 --preinclude="C:/Work/radio/components/system/radioconfig/inc/features.h" --define=Board_EXCLUDE_NVS_EXTERNAL_FLASH --define=DeviceFamily_CC26X2 --define=CCFG_FORCE_VDDR_HH=0 --define=SET_CCFG_BL_CONFIG_BL_LEVEL=0x00 --define=SET_CCFG_BL_CONFIG_BL_ENABLE=0xC5 --define=SET_CCFG_BL_CONFIG_BL_PIN_NUMBER=0x13 --define=SET_CCFG_BL_CONFIG_BOOTLOADER_ENABLE=0xC5 --c99 --plain_char=unsigned --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --embedded_constants=on --unaligned_access=on --enum_type=packed --wchar_t=16 --abi=eabi --common=on --fp_reassoc=off --sat_reassoc=off --asm_directory="C:/Users/c-marmei/workspace_v9/radio/radio_cc2652" --list_directory="C:/Users/c-marmei/workspace_v9/radio/radio_cc2652/obj" --temp_directory="C:/Users/c-marmei/workspace_v9/radio/radio_cc2652" -z -m"radio.map" -i"C:/ti/ccs930/ccs/tools/compiler/ti-cgt-arm_18.12.4.LTS/lib" --reread_libs --define=TWO_PAGE_NV --diag_wrap=off --display_error_number --warn_sections --mapfile_contents=sym_defs --xml_link_info="radio_linkInfo.xml" --rom_model --unused_section_elimination=on
"C:/ti/ccs930/ccs/tools/compiler/ti-cgt-arm_18.12.4.LTS/bin/armcl" -@"C:/Users/c-marmei/workspace_v9/radio/radio_cc2652/ccsLinker.opt" -o "radio.out"
<Linking>
undefined first referenced
symbol in file
--------- ----------------
FHAPI_SFDRxCb
FHAPI_completeRxCb
FHAPI_completeTxCb
FHAPI_getBitCount
FHAPI_getRemDT
FHAPI_getTxChHoppingFunc
FHAPI_getTxParams
FHAPI_getTxParams_old
FHAPI_reset
FHAPI_sendData
FHAPI_setStateCb
...