Part Number: BQ51051B
Other Parts Discussed in Thread: BQ51003, BQ51013B, BQ25170
Hi team while trying to calculate the R1 value i am getting this below error. can you please provide the proper calculations for the divider network

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Bill in my requirement is temperature ranges for NTC resistor is 0deg to 49deg please give the resistor values for below network & NTC Thermistors is 10Kohms 3% Beta value 3435K 1%

Hi
The 49C hot limit is going to be a problem. Circuit can be adjusted using external resistors but was designed for a higher hot temp and may not be able to meet the above requirements. Still looking at it.
Is another NTC an option?
Hi Bill thanks for your response
1.please suggest if you have any NTC part and the Bheta value for this requirement and share the resistor values.
2.Also for the same requirement consider temperature ranges for NTC resistor is 0deg to 60deg please give the resistor values for below network & NTC Thermistors is 10Kohms 3% Beta value 3435K 1%
Hi
With NTC Thermistors 10Kohms Beta value 3435K and R1-200 ohms range is 0C to 62C.
Some other values to consider:
1.) 0C to 50C -- Beta = 5500k with R1=800 and R3=60k
2.) 0C to 50C -- Beta = 5000k with R1=400 and R3=72k
3.) 0C to 55C -- Beta = 4500k with R1=600 and R3=95.5k
4.) 0C to 57C -- Beta = 4000k with R1=350 and R3=160k
Hi BIll thanks for your inputs in BQ5105xB datasheet i am seeing below data is it okay to go with the higher beta values since timing parameters depends on this, And NTC more than 4500 beta value not available

Yes OK to go with higher Beta Value, timing will not be a problem. Also keep the value of C3 in parallel with the NTC thermistor low, 1000pf is large enough unless environment is noisy.
Another approach to this problem is a two IC solution using the BQ51013B or BQ51003, 5V supply and BQ25170 battery charger. The BQ25170 TS input is designed to support the lower battery operating range (0C to 45C)