This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652P: how to start coordinator for cc2652P in Z tool ?

Part Number: CC2652P

Hi,

 how to start Zigbee network in CC2652P via Z tool?, please share steps to start zigbee coordinator.

 

  • Hi Praveen,

    Make sure to start by loading the LAUNCHXL-CC1352P-2 ZNP project.  UART settings should be 115200 baud with no flow control.

    Regards,
    Ryan

  • Hi,

     I follow the above link steps but i could not add my devices in coordinator. please help me out I could not find the error

    Start Time: 8/18/2022 11:12:35 AM

    <RX>11:13:01.42 COM4 SYS_OSAL_NV_WRITE_SRSP (0x6109)
    Status: SUCCESS (0x0)

    <TX>11:13:01.41 COM4 SYS_OSAL_NV_WRITE (0x2109)
    Id: 0x0003
    Offset: 0x00
    Len: 0x01
    Value: . (0x03)

    <TX>11:13:06.2 COM4 SYS_RESET (0x4100)
    Type: 0x00 (HARD RESET) (0x0)

    <RX>11:13:08.45 COM4 SYS_RESET_RESPONSE (0x4180)
    Reason: 0x00
    TransportRev: 0x02
    Product: 0x01
    MajorRel: 0x02
    MinorRel: 0x07
    HwRev: 0x01

    <TX>11:13:37 COM4 SYS_OSAL_NV_WRITE (0x2109)
    Id: 0x0087
    Offset: 0x00
    Len: 0x01
    Value: . (0x00)

    <RX>11:13:37.01 COM4 SYS_OSAL_NV_WRITE_SRSP (0x6109)
    Status: SUCCESS (0x0)

    <TX>11:14:03.42 COM4 APP_CNF_BDB_SET_CHANNEL (0x2F08)
    isPrimary: TRUE (0x1)
    Channel: CHNL_0x00002000 (0x2000)

    <RX>11:14:03.42 COM4 APP_CNF_BDB_SET_CHANNEL_SRSP (0x6F08)
    Status: SUCCESS (0x0)

    <TX>11:14:11.13 COM4 APP_CNF_BDB_SET_CHANNEL (0x2F08)
    isPrimary: FALSE (0x0)
    Channel: NONE (0x0)

    <RX>11:14:11.13 COM4 APP_CNF_BDB_SET_CHANNEL_SRSP (0x6F08)
    Status: SUCCESS (0x0)

    <TX>11:14:31.99 COM4 APP_CNF_BDB_START_COMMISSIONING (0x2F05)
    CommissioningMode: (0x04) Network Formation (0x4)

    <RX>11:14:34.95 COM4 APP_CNF_BDB_START_COMMISSIONING_SRSP (0x6F05)
    Status: SUCCESS (0x0)

    <RX>11:14:34.95 COM4 APP_CNF_BDB_COMMISSIONING_NOTIFICATION (0x4F80)
    Status: 1 (0x1)
    Commissioning Mode: 0x02 (Formation) (0x2)
    Commissioning Mode: 0x04 (Network Formation) (0x4)

    <RX>11:14:35.16 COM4 ZDO_STATE_CHANGE_IND (0x45C0)
    State: 8 (0x8)

    <RX>11:14:35.73 COM4 ZDO_STATE_CHANGE_IND (0x45C0)
    State: 9 (0x9)

    <RX>11:14:35.73 COM4 APP_CNF_BDB_COMMISSIONING_NOTIFICATION (0x4F80)
    Status: 0x00 (Success) (0x0)
    Commissioning Mode: 0x02 (Formation) (0x2)
    Commissioning Mode: 0 (0x0)

    <TX>11:15:22.55 COM4 UTIL_GET_DEVICE_INFO (0x2700)

    <RX>11:15:22.55 COM4 UTIL_GET_DEVICE_INFO_RESPONSE (0x6700)
    Status: SUCCESS (0x0)
    IEEEAddr: 0x00124B0025791D78
    ShortAddress: 0x0000
    DeviceType: COORDINATOR, ROUTER, END_DEVICE (0x7)
    DeviceState: DEV_ZB_COORD (0x9)
    NumAssocDevices: 0x00
    AssocDevicesList

    <TX>11:15:44.36 COM4 SYS_OSAL_NV_WRITE (0x2109)
    Id: 0x008F
    Offset: 0x00
    Len: 0x01
    Value: . (0x01)

    <RX>11:15:44.37 COM4 SYS_OSAL_NV_WRITE_SRSP (0x6109)
    Status: SUCCESS (0x0)

    <TX>11:16:36.66 COM4 APP_CNF_BDB_START_COMMISSIONING (0x2F05)
    CommissioningMode: (0x02) Network Steering (0x2)

    <RX>11:16:36.66 COM4 APP_CNF_BDB_START_COMMISSIONING_SRSP (0x6F05)
    Status: SUCCESS (0x0)

    <RX>11:16:36.67 COM4 ZDO_MGMT_PERMIT_JOIN_RSP (0x45B6)
    SrcAddr: 0x0000
    Status: ZDP_SUCCESS (0x0)

    <RX>11:16:36.67 COM4 APP_CNF_BDB_COMMISSIONING_NOTIFICATION (0x4F80)
    Status: 0x00 (Success) (0x0)
    Commissioning Mode: 0x01 (Network Steering) (0x1)
    Commissioning Mode: 0 (0x0)

    <RX>11:16:36.67 COM4 APP_CNF_BDB_COMMISSIONING_NOTIFICATION (0x4F80)
    Status: 0x02 (No Network) (0x2)
    Commissioning Mode: 0x01 (Network Steering) (0x1)
    Commissioning Mode: 0 (0x0)

  • Do you use second device to act as end device or router to join coordinator?

  • second device act as end device

  • I don't see you do channel setup for end device in your log. Do you set channel on your end device?

  • where the place of end device channel setup in above log?

    I just follow the  steps in Page sunmaysky.blogspot.com/.../use-ztool-z-stack-30-znp-to-set-up.html

  • Read the post carefully and you will see.

  • Devices are added but couldn't control from the AF Data Request in Ztool . It display Invalid parameter

    <TX>02:25:00.1 COM4 AF_DATA_REQUEST (0x2401)
    DstAddr: 0x2B98
    DestEndpoint: 0x01
    SrcEndpoint: 0x07
    ClusterID: 0x0006
    TransID: 0x01
    Options: 0x02
    Radius: 0x07
    Len: 0x03
    Data: ... (0x01, 0x01, 0x00)

    <RX>02:25:00.11 COM4 AF_DATA_REQUEST_SRSP (0x6401)
    Status: afStatus_INVALID_PARAMETER (0x2) 

  • Try to use AF_DATA_REQUEST_EXT instead of AF_DATA_REQUEST.

  • How to get DstPanID from end devices

  • You can use UTIL_GET_NV_INFO to get PANID

  • Added device (on/off module)

    <RX>02:58:39.08 COM4 ZDO_MGMT_LQI_RSP (0x45B1)
    SrcAddr: 0x0000
    Status: ZDP_SUCCESS (0x0)
    NeighborTableEntries: 0x02
    StartIndex: 0x00
    NeighborLqiListCount: 0x02
    NeighborLqiList:
    ExtendedPanID: 0x00124B0025791D78
    ExtendedAddress: 0x086BD7FFFE5B6851
    NetworkAddress: 0x2B98
    Reserved_7_Relationship_6_4_RxOnWhenIdle_3_2_DeviceType_1_0: 0x15
    Reserved_7_2_PermitJoining_1_0: 0x02
    Depth: 0x01
    RxLQI: 0xF3

    i sent the request from AF_DATA_REQUEST_EXT its also invalid parameter

    <TX>02:59:05.81 COM4 AF_DATA_REQUEST_EXT (0x2402)
    DstAddrMode: 0x03 (ADDRESS_64_BIT) (0x3)
    DstAddr: Qh[...k. (0x51, 0x68, 0x5B, 0xFE, 0xFF, 0xD7, 0x6B, 0x08)
    DstEndPoint: 0x01
    DstPanId: 0x0000
    SrcEndpoint: 0x07
    ClusterID: 0x0006
    TransID: 0x01
    Options: 0x02
    Radius: 0x07
    Len: 0x0003
    Data: ... (0x01, 0x01, 0x01)

    <RX>02:59:05.82 COM4 AF_DATA_REQUEST_EXT_SRSP (0x6402)
    Status: afStatus_INVALID_PARAMETER (0x2)

  • Do you use AF_REGISTER to register endpoint on your coordinator and device?

  • devices are controlled but couldn't get feedback from device .so, I manually bind with coordinator using ZDO_BIND_REQ option no feedback from the device

  • I suggest you to use sniffer to check what happens over the air.

  • If the ZED is not polling often enough then the ZC message is timing out due to NWK_INDIRECT_MSG_TIMEOUT (default 7 seconds)

    Regards,
    Ryan