Other Parts Discussed in Thread: DRV632, DRV603
Hi team,
Here're 2 questions from the customer may need your help:
1) Regarding the UVP pin of DRV632PWR which is to prevent chip POP:

Below diagram is an application diagram of the demo board used to test the UVP pin. With no MCU in hardware mode, can the UVP pin be left floating and not connected to any device?

2) What frequency does the DRV632PWR operate at? For example, the PVDD, PVSS pins of DEMO are all connected to ground through a 1 UF capacitor, and the CN.CP pin is also connected to a 1 UF capacitor. What is the operating frequency?
If they want to adjust this frequency, is it ok to just adjust the capacity of the CN.CP pin?
Could you help check this case? Thanks.
Best Regards,
Cherry