Part Number: UCC256403
Other Parts Discussed in Thread: UCC25600,
Good morning,
1. How simple is it to limit the maximum switching frequency to 300kHz? This is not mentioned in the datasheet.
2. How simple is it to limit the minimum switching frequency to keep it away from the capacitive area of the gain curve?
2. How do I simply set it up to only have burst mode at no-load to prevent the output voltage from running away?
This is not clear from the datasheet.
3. Can I disable the high voltage start-up by providing the BLK pin with 5V from an auxiliary power supply?
4. Just a comment: the UCC25600 is a much simpler device to use and works very well.
I know you will say that the UCC256403 gives much better transient response.
Thank you.