Other Parts Discussed in Thread: CC2533, CC2530, REMOTI, CC2430, CC2510
Hello everybody!
I am new to IAR and CC2533 RF4CE Basic Development Kit (Actually, I am on a training period and I have to test a remote).
In the forum, someone else had a similiar problem to mine but I need a different file.
I have just downloaded the last version of IAR (v8.10), and I had to convert files (it was in an older version).
When I rebuild the workspace, I have get the following errors:
Fatal Error[e72]: Segment PDATA_Z must be defined in a segment definition option (-Z, -b or -P)
Error while running Linker
I use the rsa_cc2530-CC2530F64.
Apparently, rsa_cc2530.d51 doesn't exist (the errror is located in rsa_cc2530.map).
Otherwise, I use also ti_51ew_cc2530f64.xcl.
Please, can anybody help me??
Ps: if ever you need further information, don't hesitate.