Part Number: CC2652P
Other Parts Discussed in Thread: Z-STACK, SYSCONFIG
Hi
We need help again.
My project is based on "zed sampleapp". I would like to add two standart attributes:
- ATTRID_BASIC_MANUFACTURER_NAME
- ATTRID_BASIC_MODEL_IDENTIFIER
What I do:
1.Run syscfg
2.Entered "RF Stacks" -> "Z-Stack".
3.Inside "Zigbee Application Endpoint Configure ZCL settings" -> "Mandatory Clusters" -> "Optional Attributes" added "ManufacturerName" and "Modelidentifier" into parameter "Basic Server Attributes".
4.In my code added
uint8 sampleApp_Basic_ManufacturerName[]= {4, 'N','a','m','e'};
uint8 sampleApp_Basic_ModelIdentifier[] = {5, 'M','o','d','e','l'};
5.Send request
FE0F240136E50801000002001E051003000500FF (ATTRID_BASIC_MODEL_IDENTIFIER 0x0005)
Get response
FE 1A 4481 0000 0000 36E5 08 01 00 CC 00 D2BCD600 00 06 1803010500C1 36E5 1D 67
1803010500C1
0xC1 = ZCL_STATUS_SOFTWARE_FAILURE
I found out under debugger there is no CallBack. Why? Should standart request have my own CallBackHandler?
May be in syscfg something should be added...
Thanks