Part Number: CC2652P7
Other Parts Discussed in Thread: CC2652P, , SYSCONFIG
Hi,
I'm using SmartRF Studio 7 and xds110 simulator to test CC2652P launchpad. I select proprietary mode, and there are 3 typical settings. I want to increase the TX power to 20dbm, but none of setting allow me to enable high output power PA, thus only 5dbm can be triggered. I noticed that from data sheet and other document, if I change GPIOs configuration and some code of register, there should have some ways to let proprietary 2.4g working on 20dbm tx power, but I do not know the exact way. So can anyone help me do that specifically? I really want to test the range increase when the tx power is 20dbm.
Thanks!