Part Number: LP-CC1352P7
Good day,
Commercial motion sensor not successfully binding to Coordinator. I am using a Sonoff SNZB-03 sensor as ED and LP-CC1352P7-4 as Coordinator. I am running the stock-standard "zc_zone" software example from the TI resource Explorer package (listed under the CC1352P7-4 Launchpad device. Which is listed under the SimpleLink CC13xx CC26xx SDK 7.10.01.24) on the Launchpad. Both devices are running Zigbee 3.
It appears that the Coordinator starts and creates a network. I then do Trip-To-Pair by manual button-press on ZC and ZED side.
The Motion sensor announces itself (Device Announcement) but then an END Device Timeout Request is sent by the ED.
The ED then sends a Zone Enroll Request, followed by a Zone Status Change Notification.
The coordinator then sends an End Device Timeout Response, Success
Then finally the coordinator sends a Default Response (0x0b) command with status = "Unsupported Cluster Command"
I am attaching a wireshark trace. I would appreciate some input on this.
Best regardsPIR1.zip