Part Number: TPS62811-Q1
Other Parts Discussed in Thread: TPS22919
Tool/software:
Hi, there~
I manage to use TPS628112 and a HSW IC TPS22919 to achieve track function, that is according to TPS628112's SS/TR pin function.
Add external voltage on this pin and make sure external voltage slightly bigger than internal reference voltage (0.6V).
It doesn't work well, so I make a little test, chang 4.7k resistor to 470ohm resistor,that expect DSP_1.8V output follow outside voltage tightly, and output 0.25V.
no it doesn't. The picture shows DSP_3.3V_SW output and DSP_1.8V output, DSP_1.8V rises up first (internal refernce ?) and down to external reference.
Why does this happen? How can I achieve two power IC rise in same slope?