Other Parts Discussed in Thread: DRV8462
Tool/software:
Hi,
We are designing custom motor driver board using DRV8462DDWR IC,
Regarding VREF connection, Used Voltage divider circuit using Two 10K Resistor.(as per Development board and Typical application circuit)
1. Is that okay for driving the stepper motor?
2. Based on the Motor Capacity is it required to change the divider voltage?
3. How to check the functionality of the MANUAL_VREF in the DRV8462VEVM development board. and what jumper modifications required? (J6 to be removed and Put it to the J7)
Kindly suggest if any other modifications required in the Hardware or GUI setting.
Regards