Part Number: TPS566247
Tool/software:
Hello , I f I creat ea new design on the above part specifying: Vin 4.5-5.5V, U out =3.3V Iout=2.5A, Ta =70C once teh WEBENCH opens design it pops the following info:
"The TPS566247 can support the large duty operation, please contact e2e.ti.com/.../196 forum for application help."
The duty cyclke of 3.3/4.5=0.733 does not look like extremally large, the data sheet mentions Large Duty Operation
by dropping switching frequency but for Vin/Vout<1.6 and I am having 4.5/3.3=1.51. Though it says dropping of switching frequency happends in order to extend Ton ( probably above minimum of 50ns sp[ecified in teh dat asheet) So at 600kHz we talking about times of 1.17us and 426ns far away from Toff, Ton minimum specified in the data sheet.
1) will switching frequency change in my design?
2) what is the reason for it ?
3) why I am getting the WEBENCH info related to large duty cycle
4) Is there anything else I shoudl be awaro of related to this info what can affect operation of this controller?
Kind Regards
Sebastian