Tool/software:
Dear,
I would like to know what is the accuracy of the TLV770 simulation model available on the website and if I can use is to cover all possible operative condition of my project.
In particular:
1) I need to add a long cable with inductive parasitic and I would simulate the load step response;
2) I would check the behavior at -40°C and +125°C
Is the SBVMA03.ZIP (64 KB) - PSpice Model reliable for this simulations?
Best regards,
Fulvio