Tool/software:
Hello
tl;dr: I am trying to figure out, if its ok to replace ceramic decoupling capacitors with capacitors of lesser size and voltage rating in a DC power system
I have developed my first power system with two linear regulators(LM27762 and TLV67), which have ceramic decoupling capacitors on Input and Output:

I used several references as guidelines for the schematic and the parts(BOM)
ADS1261 EVM for LM27762
TLV67EVM for TLV67
We can manufacture our pcbs inhouse and for the first prototype I want to replace some capacitors from the references with capacitors we already have in stock.
But I am unsure, what effect(if any) this will have on the prototype, when diverging from the references.
I know that several parameters influence the actual capacity of a ceramic capacitor:
- rated voltage
- size
- nominal capacity
- tolerance
- acutal supply voltage
- temperatur coefficient (X5R,X7R,...)
- frequency of ripple?
Example:
Replacing
4.7 uF +-10% 25V 0805
with
4.7 uF +- 10% 16V 0603 capacitors
Questions I have:
- What will happen when I replace the input and output Decoulping capacitors
- Will the behaviour of my system change?
- Can I ignore the change? It is DC power and not AC.
- How big is the influence of each parameter?
So if anyone has some adivce and can help me, this would be much appreciated. If you have any questions feel free to ask.
Thank you in advance for your time
Regards
Johannes