i am trying to find some examples for bit bang slave i2c driver on CC2540. Any suggestions ???
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ravi,
Unfortuanately we do not have any example code for I2C slave bit banging implementation for CC2540. It should be possible to implement (especially if CC2540 will be only slave device), but please notice that it will be quite CPU cycle consuming. Thus it might be not possible to run any other tasks during I2C activity.
http://www.ti.com/tool/RemoTi has I2C driver for CC2530. I know CC2540 and CC2530 chips only at a high level. I believe CC2530 I2C deriver will work for CC2540. Please try and let us know if you are able to compile and make it work on CC2540/CC2541.5342.i2c.zip
http://www.ti.com/tool/RemoTi has I2C driver for CC2530. I know CC2540 and CC2530 chips only at a high level. I believe CC2530 I2C deriver will work for CC2540. Please try and let us know if you are able to compile and make it work on CC2540/CC2541.
Works great with CC2540 with minor mods.
/**************************************************************************************************
Filename: hal_i2c.c
Revised: $Date: 2010-06-28 17:37:07 -0700 (Mon, 28 Jun 2010) $
Revision: $Revision: 22837 $
Description: I2C driver implementation.
Copyright 2006 - 2010 Texas Instruments Incorporated. All rights reserved.
IMPORTANT: Your use of this Software is limited to those specific rights
granted under the terms of a software license agreement between the user
who downloaded the software, his/her employer (which must be your employer)
and Texas Instruments Incorporated (the "License"). You may not use this
Software unless you agree to abide by the terms of the License. The License
limits your use, and you acknowledge, that the Software may not be modified,
copied or distributed unless embedded on a Texas Instruments microcontroller
or used solely and exclusively in conjunction with a Texas Instruments radio
frequency transceiver, which is integrated into your product. Other than for
the foregoing purpose, you may not use, reproduce, copy, prepare derivative
works of, modify, distribute, perform, display or sell this Software and/or
its documentation for any purpose.
YOU FURTHER ACKNOWLEDGE AND AGREE THAT THE SOFTWARE AND DOCUMENTATION ARE
PROVIDED �AS IS� WITHOUT WARRANTY OF ANY KIND, EITHER EXPRESS OR IMPLIED,
INCLUDING WITHOUT LIMITATION, ANY WARRANTY OF MERCHANTABILITY, TITLE,
NON-INFRINGEMENT AND FITNESS FOR A PARTICULAR PURPOSE. IN NO EVENT SHALL
TEXAS INSTRUMENTS OR ITS LICENSORS BE LIABLE OR OBLIGATED UNDER CONTRACT,
NEGLIGENCE, STRICT LIABILITY, CONTRIBUTION, BREACH OF WARRANTY, OR OTHER
LEGAL EQUITABLE THEORY ANY DIRECT OR INDIRECT DAMAGES OR EXPENSES
INCLUDING BUT NOT LIMITED TO ANY INCIDENTAL, SPECIAL, INDIRECT, PUNITIVE
OR CONSEQUENTIAL DAMAGES, LOST PROFITS OR LOST DATA, COST OF PROCUREMENT
OF SUBSTITUTE GOODS, TECHNOLOGY, SERVICES, OR ANY CLAIMS BY THIRD PARTIES
(INCLUDING BUT NOT LIMITED TO ANY DEFENSE THEREOF), OR OTHER SIMILAR COSTS.
Should you have any questions regarding your right to use this Software,
contact Texas Instruments Incorporated at www.TI.com.
**************************************************************************************************/
/**************************************************************************************************
This file contains the I2C interface to off-chip serial EEPROM. While
much of the driver is generic, certain portions are specific to the
Atmel part AT24C1024. For example, the 17th address bit occurs in the
device address byte where one of the address pins should be. Different
1 Mb parts use a different bit location. This could be abstracted at
a later time if this is the only difference among these parts.
**************************************************************************************************/
#include "ioCC2540.h"
#include "bcomdef.h"
#include "hal_i2c.h"
#define STATIC static
#if !defined HAL_I2C_RETRY_CNT
#define HAL_I2C_RETRY_CNT 3
#endif
// the default cofiguration below uses P1.6 for SDA and P0.0 for SCL.
// change these as needed.
#ifndef OCM_CLK_PORT
#define OCM_CLK_PORT 0
#endif
#ifndef OCM_DATA_PORT
#define OCM_DATA_PORT 0 //port to use for i2c
#endif
#ifndef OCM_CLK_PIN
#define OCM_CLK_PIN 1 //assigned SCL P0_1 for PCF85162
#endif
#ifndef OCM_DATA_PIN
#define OCM_DATA_PIN 0 //assigned SDA P0_0 for PCF85162
#endif
// General I/O definitions
#define IO_GIO 0 // General purpose I/O
#define IO_PER 1 // Peripheral function
#define IO_IN 0 // Input pin
#define IO_OUT 1 // Output pin
#define IO_PUD 0 // Pullup/pulldn input
#define IO_TRI 1 // Tri-state input
#define IO_PUP 0 // Pull-up input pin
#define IO_PDN 1 // Pull-down input pin
#define OCM_ADDRESS (0x70) // PCF85162 LCD driver address
#define OCM_READ (0x01) // No read commands for PCF85162
#define OCM_WRITE (0x00) // Only write commands for PCF85162
#define SMB_ACK (0)
#define SMB_NAK (1)
#define SEND_STOP (0)
#define NOSEND_STOP (1)
#define SEND_START (0)
#define NOSEND_START (1)
// device specific as to where the 17th address bit goes...
// ************************* MACROS ************************************
#undef P
/* I/O PORT CONFIGURATION */
#define CAT1(x,y) x##y // Concatenates 2 strings
#define CAT2(x,y) CAT1(x,y) // Forces evaluation of CAT1
// OCM port I/O defintions
// Builds I/O port name: PNAME(1,DIR) ==> P1DIR
#define PNAME(y,z) CAT2(P,CAT2(y,z))
// Builds I/O bit name: BNAME(1,2) ==> P1_2
#define BNAME(port,pin) CAT2(CAT2(P,port),CAT2(_,pin))
// OCM port I/O defintions
#define OCM_SCL BNAME(OCM_CLK_PORT, OCM_CLK_PIN) //assigned SCL P0_1 for PCF85162
#define OCM_SDA BNAME(OCM_DATA_PORT, OCM_DATA_PIN) //assigned SDA P0_0 for PCF85162
// port direction
#define IO_DIR_PORT_PIN(port, pin, dir) \
{\
if ( dir == IO_OUT ) \
PNAME(port,DIR) |= (1<<(pin)); \
else \
PNAME(port,DIR) &= ~(1<<(pin)); \
}
// set pin to go high by making input
#define OCM_DATA_HIGH()\
{ \
IO_DIR_PORT_PIN(OCM_DATA_PORT, OCM_DATA_PIN, IO_IN); \
}
// set pin to go low by sinking
#define OCM_DATA_LOW() \
{ \
IO_DIR_PORT_PIN(OCM_DATA_PORT, OCM_DATA_PIN, IO_OUT); \
OCM_SDA = 0;\
}
// config pin as i/o or peripheral
#define IO_FUNC_PORT_PIN(port, pin, func) \
{ \
if( port < 2 ) \
{ \
if ( func == IO_PER ) \
PNAME(port,SEL) |= (1<<(pin)); \
else \
PNAME(port,SEL) &= ~(1<<(pin)); \
} \
else \
{ \
if ( func == IO_PER ) \
P2SEL |= (1<<(pin>>1)); \
else \
P2SEL &= ~(1<<(pin>>1)); \
} \
}
// set i2c tristate
#define IO_IMODE_PORT_PIN(port, pin, mode) \
{ \
if ( mode == IO_TRI ) \
PNAME(port,INP) |= (1<<(pin)); \
else \
PNAME(port,INP) &= ~(1<<(pin)); \
}
// set pin as pulled up or pulled down
#define IO_PUD_PORT(port, dir) \
{ \
if ( dir == IO_PDN ) \
P2INP |= (1<<(port+5)); \
else \
P2INP &= ~(1<<(port+5)); \
}
STATIC void hali2cSend( uint8 *buffer, uint16 len, uint8 sendStart, uint8 sendStop );
STATIC _Bool hali2cSendByte( uint8 dByte );
STATIC void hali2cWrite( bool dBit );
STATIC void hali2cClock( bool dir );
STATIC void hali2cStart( void );
STATIC void hali2cStop( void );
STATIC void hali2cReceive( uint8 address, uint8 *buffer, uint16 len );
STATIC uint8 hali2cReceiveByte( void );
STATIC _Bool hali2cRead( void );
STATIC void hali2cSendDeviceAddress(uint8 address);
STATIC __near_func void hali2cWait( uint8 );
STATIC uint8 s_xmemIsInit;
/*********************************************************************
* @fn HalI2CInit
* @brief Initializes two-wire serial I/O bus
* @param void
* @return void
*/
void HalI2CInit( void )
{
if (!s_xmemIsInit) {
s_xmemIsInit = 1;
// Set port pins as inputs
IO_DIR_PORT_PIN( OCM_CLK_PORT, OCM_CLK_PIN, IO_IN );
IO_DIR_PORT_PIN( OCM_DATA_PORT, OCM_DATA_PIN, IO_IN );
// Set for general I/O operation
IO_FUNC_PORT_PIN( OCM_CLK_PORT, OCM_CLK_PIN, IO_GIO );
IO_FUNC_PORT_PIN( OCM_DATA_PORT, OCM_DATA_PIN, IO_GIO );
// Initializations below are irrelevant to CC2540
// // Set I/O mode for pull-up/pull-down
// IO_IMODE_PORT_PIN( OCM_CLK_PORT, OCM_CLK_PIN, IO_PUD );
// IO_IMODE_PORT_PIN( OCM_DATA_PORT, OCM_DATA_PIN, IO_PUD );
//
// // Set pins to pull-up
// IO_PUD_PORT( OCM_CLK_PORT, IO_PUP );
// IO_PUD_PORT( OCM_DATA_PORT, IO_PUP );
}
}
int8 HalI2CReceive(uint8 address, uint8 *buf, uint16 len)
{
hali2cReceive(address, buf, len);
return 0;
}
int8 HalI2CSend(uint8 address, uint8 *buf, uint16 len)
{
// begin the write sequence with the address byte
hali2cSendDeviceAddress(address);
hali2cSend(buf, len, NOSEND_START, SEND_STOP);
return 0;
}
/*********************************************************************
* @fn hali2cSend
* @brief Sends buffer contents to SM-Bus device
* @param buffer - ptr to buffered data to send
* @param len - number of bytes in buffer
* @param sendStart - whether or not to send start condition.
* @param sendStop - whether or not to send stop condition.
* @return void
*/
STATIC void hali2cSend( uint8 *buffer, uint16 len, uint8 sendStart, uint8 sendStop )
{
uint16 i;
uint8 retry = HAL_I2C_RETRY_CNT;
if (!len) {
return;
}
if (sendStart == SEND_START) {
hali2cStart();
}
for ( i = 0; i < len; i++ )
{
do {
if ( hali2cSendByte( buffer[i] ) ) // takes care of ack polling
{
break;
}
} while ( --retry );
}
if (sendStop == SEND_STOP) {
hali2cStop();
}
}
/*********************************************************************
* @fn hali2cSendByte
* @brief Serialize and send one byte to SM-Bus device
* @param dByte - data byte to send
* @return ACK status - 0=none, 1=received
*/
STATIC _Bool hali2cSendByte( uint8 dByte )
{
uint8 i;
for ( i = 0; i < 8; i++ )
{
// Send the MSB
hali2cWrite( dByte & 0x80 );
// Next bit into MSB
dByte <<= 1;
}
// need clock low so if the SDA transitions on the next statement the
// slave doesn't stop. Also give opportunity for slave to set SDA
hali2cClock( 0 );
OCM_DATA_HIGH(); // set to input to receive ack...
hali2cClock( 1 );
hali2cWait(1);
return ( !OCM_SDA ); // Return ACK status
}
/*********************************************************************
* @fn hali2cWrite
* @brief Send one bit to SM-Bus device
* @param dBit - data bit to clock onto SM-Bus
* @return void
*/
STATIC void hali2cWrite( bool dBit )
{
hali2cClock( 0 );
hali2cWait(1);
if ( dBit )
{
OCM_DATA_HIGH();
}
else
{
OCM_DATA_LOW();
}
hali2cClock(1);
hali2cWait(1);
}
/*********************************************************************
* @fn hali2cClock
* @brief Clocks the SM-Bus. If a negative edge is going out, the
* I/O pin is set as an output and driven low. If a positive
* edge is going out, the pin is set as an input and the pin
* pull-up drives the line high. This way, the slave device
* can hold the node low if longer setup time is desired.
* @param dir - clock line direction
* @return void
*/
STATIC void hali2cClock( bool dir )
{
if ( dir )
{
IO_DIR_PORT_PIN( OCM_CLK_PORT, OCM_CLK_PIN, IO_IN );
while(!OCM_SCL) /* Wait until clock is high */
hali2cWait(1);
}
else
{
IO_DIR_PORT_PIN( OCM_CLK_PORT, OCM_CLK_PIN, IO_OUT );
OCM_SCL = 0;
}
hali2cWait(1);
}
/*********************************************************************
* @fn hali2cStart
* @brief Initiates SM-Bus communication. Makes sure that both the
* clock and data lines of the SM-Bus are high. Then the data
* line is set high and clock line is set low to start I/O.
* @param void
* @return void
*/
STATIC void hali2cStart( void )
{
uint8 retry = HAL_I2C_RETRY_CNT;
// set SCL to input but with pull-up. if slave is pulling down it will stay down.
hali2cClock(1);
do {
// wait for slave to release clock line...
if (OCM_SCL) // wait until the line is high...
{
break;
}
hali2cWait(1);
} while ( --retry );
// SCL low to set SDA high so the transition will be correct.
hali2cClock(0);
OCM_DATA_HIGH(); // SDA high
hali2cClock(1); // set up for transition
hali2cWait(1);
OCM_DATA_LOW(); // start
hali2cWait(1);
hali2cClock( 0 );
}
/*********************************************************************
* @fn hali2cStop
* @brief Terminates SM-Bus communication. Waits unitl the data line
* is low and the clock line is high. Then sets the data line
* high, keeping the clock line high to stop I/O.
* @param void
* @return void
*/
STATIC void hali2cStop( void )
{
// Wait for clock high and data low
hali2cClock(0);
OCM_DATA_LOW(); // force low with SCL low
hali2cWait(1);
hali2cClock( 1 );
OCM_DATA_HIGH(); // stop condition
hali2cWait(1);
}
/*********************************************************************
* @fn hali2cWait
* @brief Wastes a an amount of time.
* @param count: down count in busy-wait
* @return void
*/
STATIC __near_func void hali2cWait( uint8 count )
{
while ( count-- );
}
/*********************************************************************
* @fn hali2cReceiveByte
* @brief Read the 8 data bits.
* @param void
* @return character read
*/
STATIC uint8 hali2cReceiveByte()
{
int8 i, rval = 0;
for (i=7; i>=0; --i) {
if (hali2cRead()) {
rval |= 1<<i;
}
}
return rval;
}
/**************************************************************************************************
**************************************************************************************************/
/*********************************************************************
* @fn hali2cReceive
* @brief reads data into a buffer
* @param address: linear address on part from which to read
* @param buffer: target array for read characters
* @param len: max number of characters to read
* @return void
*/
STATIC void hali2cReceive( uint8 address, uint8 *buffer, uint16 len )
{
//uint8 ch;
uint16 i;
if (!len) {
return;
}
hali2cSendDeviceAddress(address);
//ch = OCM_ADDRESS_BYTE(0, OCM_READ);
//hali2cSend(&ch, 1, SEND_START, NOSEND_STOP);
for ( i = 0; i < len-1; i++ )
{
// SCL may be high. set SCL low. If SDA goes high when input
// mode is set the slave won't see a STOP
hali2cClock(0);
OCM_DATA_HIGH();
buffer[i] = hali2cReceiveByte();
hali2cWrite(SMB_ACK); // write leaves SCL high
}
// condition SDA one more time...
hali2cClock(0);
OCM_DATA_HIGH();
buffer[i] = hali2cReceiveByte();
hali2cWrite(SMB_NAK);
hali2cStop();
}
/*********************************************************************
* @fn hali2cRead
* @brief Toggle the clock line to let the slave set the data line.
* Then read the data line.
* @param void
* @return TRUE if bit read is 1 else FALSE
*/
STATIC _Bool hali2cRead( void )
{
// SCL low to let slave set SDA. SCL high for SDA
// valid and then get bit
hali2cClock( 0 );
hali2cWait(1);
hali2cClock( 1 );
hali2cWait(1);
return OCM_SDA;
}
/*********************************************************************
* @fn hali2cSendDeviceAddress
* @brief Send onlythe device address. Do ack polling
*
* @param void
* @return none
*/
STATIC void hali2cSendDeviceAddress(uint8 address)
{
uint8 retry = HAL_I2C_RETRY_CNT;
do {
hali2cStart();
if (hali2cSendByte(address)) // do ack polling...
{
break;
}
} while ( --retry );
}