Part Number: TMS320F28027F
Other Parts Discussed in Thread: TMS320F28027, , TMDSCNCD28027, CONTROLSUITE
I am planning on buying http://www.ti.com/tool/tmdscncd28027f which has TMS320F28027F on it. I checked the datasheets and it is pin compatible with TMS320F28027 with only difference being the FOC block in ROM.
Although I am 90% sure, I just need confirmation that the control CARD will work with 100 pin base station and I can program/debug it.
(Docking-Stn USB-EMU R3 which works with TMDSCNCD28027 (TMS320F28027 control CARD))
I was not able to find controller to 100 pin connector mapping schematic for the control CARD. As the two ICs differ only in software, is it safe to assume that the control CARD mapping is
exactly identical ?