This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2500: CC2500 packet retransmitting

Part Number: CC2500


Hello !

I wish to know if there is a way to retransmit the same content of the TxFifo without re-filling it. In other words I need to transmit the same 64 bytes block two times identical, avoiding waste of time and power due to refilling the TxFifo with the same data of the previous packet.

Obviously if I set the Packet_Lenght = 64, fill the TxFifo with 64 bytes  and give the strobe Tx command everything works fine and I can repeat this sequence how many times I need.

I wish to :

1st time: set the Packet_Lenght = 64, fill the TxFifo with 64 bytes  and give the strobe Tx command

2nd time: give the strobe Tx command (or a simple sequence of commands) to retransmit the same packet of the 1st time

Do you think it's possible ?

Many thanks

Giuseppe