Part Number: CC2530
Other Parts Discussed in Thread: Z-STACK
One question from customer side:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CC2530
Other Parts Discussed in Thread: Z-STACK
One question from customer side:
Hi,
Can you provide the sniffer log itself (not just a screenshot)?
It's probably due to different security settings used between the devices.
As we have newer releases for Z-Stack, I'd recommend updating the firmware on the router. Can you try with Z-Stack 3.0.2?
Regards,
Toby
Hi Toby,
thanks for feedback. The customers' feedback as below:
/////////////////////////////////////////////////
1.附件是log文件。其实TI自己可以搞个3.0再搞个2.5.1a版本,用固定密钥方式, 就能复现这个问题并定位原因,只单看log估计还是无法理解为何两者不能入网兼容.
2.现在我们碰到的问题就是新模块用3.0协议栈, 需要跟之前老的2.5.1.a版本兼容,新版本和老版本如何通讯得了?
3.关键还是要知道老版本为什么无法和新版本通讯,我们需要如何修改3.0版本, 这部分它代码没开源我们无法发现问题.
4. 参考附件, 有一个是2.5.1a的可以入网,另一个是3.0不能跟2.5.1.a版本协议栈入网兼容, 为什么? 需要确定,固定密钥情况下,两个版本若不能兼容通讯, 我是否可以关掉3.0版本的某些特性,来达到使用新栈软件又能兼容2.5.1.a版本通讯?
/////////////////aaa.psdbbb.psd
regards,
Steven
yk,
Thanks for feedback. Sorry, per customers' comments, the TC_Link proposal is tried but has no help before (noted in E2EChina website).
regards,
Steven
Please see the difference in encryption of the Transport Key message between aaa.psd and bbb.psd.
When you look at a packet in detail, the upper right lock icon will show you they key which the packet is encrypted with.
In aaa.psd (with Zigbee 3.0 coordinator), the Transport Key message is encrypted at the APS layer using the default global TC link key "ZigBeeAlliance09"(5A:69:67:42:65:65:41:6C:6C:69:61:6E:63:65:30:39). The 2.5.1a joining device is probably unable to decrypt this packet.
In bbb.psd (with 2.5.1a coordinator), the Transport Key message is encrypted at the NWK layer using some NWK key. This 2.5.1a joining device seems to know this key, since it's able to decrypt the command and then broadcast the Device Announce.
Thank Toby.
So it since the keys are different. What / how does the customer do to make them communicate successfully?
thanks.
Make sure the following conditions are meet in Z-Stack 2.5.1a device.
1. Set the following values in ZGlobals.c
uint8 zgPreConfigKeys = FALSE;// TRUE;
uint8 zgUseDefaultTCLK = TRUE; // FALSE
2. Set -DSECURE=1 in f8wconfig.cfg.
3. Make sure the following define isn't changed in nwk_globals.h
#define DEFAULT_TC_LINK_KEY { 0x5a, 0x69, 0x67, 0x42, 0x65, 0x65, 0x41, 0x6c,\
0x6c, 0x69, 0x61, 0x6e, 0x63, 0x65, 0x30, 0x39 }