Part Number: CC2640R2F
Other Parts Discussed in Thread: BLE-STACK
I just added new task to perform ADCBuf converting on project_zero.
I did't do anything more on the original project.
While new task working fine, GAP-Role or projectZero task seems not working correctly.
During ADC converting starts and showing log well, I cannot find BLE-Service list in mobile APP (TI-SensorTag) anymore.
It shows just name of main service ('Project Zero').
I cannot step into service item to see button-service, led-service and so on.
I found that GAP-Role enters connection state but never get 'ATT_MTU_UPDATED_EVENT'.
Can't I use ADC Buffer with BLE Service?
Please anyone give me a piece of advice!
Here is my code of new task.
-----------------------------------------------------------------------------------------------------------
#define ADC_SAMPLE_COUNT 8
// My own data block
typedef struct {
uint16_t buff1[ADC_SAMPLE_COUNT];
uint16_t buff2[ADC_SAMPLE_COUNT];
uint32_t mvolt[ADC_SAMPLE_COUNT]; // micro volts
ADCBuf_Handle handle;
ADCBuf_Conversion conversion; // continuous conversion
} MY_ADC_t;
static MY_ADC_t my_adc = {0,};
static void initMyADC(void);
static void ADC_callback( ADCBuf_Handle handle,
ADCBuf_Conversion *conversion,
void *buff,
uint32_t channel);
static void tmpTaskFunc(UArg arg0, UArg arg1)
{
initMyADC();
while(1){
Log_Info0("TmpTaskFunc is Running");
taskSleepMilisec(1000); // macro function. sleep for 1 sec
}
}
static void initMyADC(void)
{
ADCBuf_Params params;
ADCBuf_Handle handle;
ADCBuf_Conversion *conversion;
ADCBuf_init();
// Configure the conversion struct
conversion = &my_adc.conversion;
conversion->arg = NULL;
conversion->adcChannel = Board_ADCBUF0CHANNEL0;
conversion->sampleBuffer = my_adc.buff1;
conversion->sampleBufferTwo = my_adc.buff2;
conversion->samplesRequestedCount = ADC_SAMPLE_COUNT;
// ADC Buffer Open
ADCBuf_Params_init(¶ms);
params.callbackFxn = ADC_callback;
params.recurrenceMode = ADCBuf_RECURRENCE_MODE_CONTINUOUS;
params.returnMode = ADCBuf_RETURN_MODE_CALLBACK;
params.samplingFrequency = 20; // 20 hz
handle = ADCBuf_open(Board_ADCBUF0, ¶ms);
assert(handle);
my_adc.handle = handle; // keep it for later use
{
// Start converting
int_fast16_t res = ADCBuf_convert(handle, conversion, 1);
assert(res == ADCBuf_STATUS_SUCCESS);
}
}
static void ADC_callback( ADCBuf_Handle handle,
ADCBuf_Conversion *conversion,
void *buff,
uint32_t channel)
{
int_fast16_t status;
// Adjust raw ADC values
status = ADCBuf_adjustRawValues(handle, buff, ADC_SAMPLE_COUNT, channel);
if (status NEQ ADCBuf_STATUS_SUCCESS){
Log_warn1("ADC adjust Raw failed. status=0x%02x", status);
goto exit;
}
// Convert adjusted ADC-values to microVolts
status = ADCBuf_convertAdjustedToMicroVolts(handle,
channel,
buff,
my_adc.mvolt,
ADC_SAMPLE_COUNT);
if (status NEQ ADCBuf_STATUS_SUCCESS) {
Log_warn1("ADC converting to microVolts failed. status=0x%02x", status);
goto exit;
}
// OK, just print log
Log_Info0("ADC_callback() - OK");
exit:
return;
}