Part Number: TIDA-01352
Other Parts Discussed in Thread: TX7332, , LM5030, TIDA-00181, LMZ34202, LMZ34002, LM3411
Hi,
Our system will have 64 channels and need TX7332.
Each TX7332 need 5 supply rails such as:
1. 1.8V Fixed supply rail
2. 5.0V Fixed supply rail
3. -5.0V Fixed supply rail
4. 100V Fixed supply rail
5. -100V Fixed supply rail
We intend to design the power board for TX7332 with V_input = 15V.
Q1: Push-Pull transformer 750343547 has V_input = 24V (following datasheet). is it ok if we use V_input for it = 15?
Q2: How to choose the value of the resistor and capacitor connected to the Compensation (COMP) pin of LM5030?
Q3: Can we configure the PWM of LM5030 to change the output?
The below figure with input: 15V and output 100V I had. Any problem if we use this schematic?