Part Number: LMR33610
Hello team,
I have a question about inductor value for LMR33610.
Looking at table 2 on datasheet for 5Vout with 1400kHz, 2.2uH is recommended.
However calculating inductor value with using equation 4 with assuming 24Vin, 0.3A max current output, it is calculated as about 31uH.
If assuming 1A max output instead, the inductor value still 10uH.
Should we use 2.2uH as suggested in table 2 for 24Vin, 5Vout, 0.3A out, 1400kHz fsw?
Also could you please let me know Isc spec for the device?
When selecting inductor I think high side current limit value should be referenced. However there is no spec information in datasheet.
Best regards,