Part Number: CC2652P
Tool/software: Code Composer Studio
Hi, I use CC2652P. I have a question about watchdog.
Here is my code:
void watchdogCallback(uintptr_t watchdogHandle)
{
/*
* If the Watchdog Non-Maskable Interrupt (NMI) is called,
* loop until the device resets. Some devices will invoke
* this callback upon watchdog expiration while others will
* reset. See the device specific watchdog driver documentation
* for your device.
*/
printf("watchdogCallback!\n");
//HWREG(WDT_BASE + WDT_O_ICR) = 0xFFFFFFFF;
SysCtrlSystemReset();
}
void watchdog_init(void)
{
Watchdog_Params params;
Watchdog_init();
Watchdog_Params_init(¶ms);
params.callbackFxn = (Watchdog_Callback) watchdogCallback;
params.debugStallMode = Watchdog_DEBUG_STALL_ON;
params.resetMode = Watchdog_RESET_ON;
Watchdog_open(CONFIG_WATCHDOG_0, ¶ms);
}
When enters watchdog callback, I want to reset the target immediately. So I use SysCtrlSystemReset() in callback. But CPU just stops in SysCtrlSystemReset(), and keeps until another watchdog period to trigger a warm reset.
In my application code, SysCtrlSystemReset() works fine.
So, my question is why SysCtrlSystemReset() doesn't work in watchdog callback?
Are there any other cases where SysCtrlSystemReset() dosen't work?