Part Number: LAUNCHXL-CC26X2R1
Hello,
While experimenting with the TI-Thread Thermostat and Temperature Sensor example projects on the LaunchXL-CC26X2R1 platform, the thermostat CoAP appears to stop receiving updated temperature readings from the temp. sensor.
Once both devices have joined the network, the thermostat will stop receiving Temp change events from the CoAP. Once the network is established, the CUI is updated a total of 40 times before it stops updating.
Using a 3rd board with the CLI project, I can request the temperature from the thermostat (thermostat/temperature), but it is the stale value shown on the CUI.
Could someone share some insight into this problem?
I am using the following:
SDK: 4.30.0.54
CCS: 10.0.0.00010
Thank you,