Hello,
In SmartRF Studio 7 my XDS110 is found in the List of Connected Devices.
My controller CC2652R is found.
When I try to open the Device Control Panel the following error occurs:
It seems that the XDS110 is trying to upload some firmware but this is not happening for some reason.
My previous program with a LED is still running but is getting reset a few (2x?) times.
When I upload through "Flash Programmer 2" in 4-pin JTAG everything goes correctly.
Is SmartRF Studio trying to upload through 2-pin JTAG?
Looking forward to some reactions.